AM263x MCU+ SDK  08.03.00
GPIO LED Blink

Introduction

This example configures a GPIO pin connected to an LED on the EVM in output mode. The application toggles the LED on/off for 10 seconds and exits.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263x-cc, am263x-lp
Example folder examples/drivers/gpio/gpio_led_blink/

Steps to Run the Example

AM263X-CC

  • Watch out for LED LD13 on the CC to blink which is controlled by GPIO0_1.

AM263X-LP

  • Watch out for LED DS2 on the LP to blink which is controlled by GPIO0_26.

See Also

GPIO

Sample Output

Shown below is a sample output when the application is run,

GPIO LED Blink Test Started ...
LED will Blink for 10 seconds ...
GPIO LED Blink Test Passed!!
All tests have passed!!