Introduction
EPWM HR UpDown
This example modifies the MEP control registers to show edge displacement for high-resolution period with ePWM in Up-Down count mode due to the HRPWM control extension of the respective ePWM module.
Block Diagram for EPWM HR UpDown example
External Connections
- Pin can be connected to high resolution oscilloscope (1 GHz) to observe the edge displacement.
AM263X-CC
When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)
- Capture waveform on HSEC Pin 49, 51 for epwm0
- Capture waveform on HSEC Pin 53, 55 for epwm1
- Capture waveform on HSEC Pin 50, 52 for epwm2
- Capture waveform on HSEC Pin 54, 56 for epwm3
- Capture waveform on HSEC Pin 57, 59 for epwm4
AM263X-LP
This example is not supported on AM263X-LP
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am263x-cc |
Example folder | examples/drivers/epwm/epwm_hr_updown |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
See Also
EPWM
Sample Output
Shown below is a sample output when the application is run,
EPWM High Resolution Up Down Test Started ...
EPWM High Resolution Up Down Test Passed!!
All tests have passed!!
EPWM HR UpDown waveform