|
AM263Px MCU+ SDK
11.01.00
|
|
Go to the documentation of this file.
78 typedef struct Dp83826_Cfg_s
107 const void *pVersion);
114 const uint32_t extCfgSize,
Definition: phy_common.h:283
uint8_t EthPhyDrv_Handle[ETHPHYDRV_MAX_OBJ_SIZE]
Definition: phy_common.h:302
bool Dp83826_isPhyDevSupported(EthPhyDrv_Handle hPhy, const void *pVersion)
bool Dp83826_isMacModeSupported(EthPhyDrv_Handle hPhy, Phy_Mii mii)
Phy_Mii
Definition: phy_common.h:220
void Dp83826_bind(EthPhyDrv_Handle *hPhy, uint8_t phyAddr, Phy_RegAccessCb_t *pRegAccessCb)
void Dp83826_printRegs(EthPhyDrv_Handle hPhy)
dp83826 PHY configuration parameters.
Definition: dp83826.h:79
void Dp83826_initCfg(Dp83826_Cfg *cfg)
Initialize dp83826 PHY specific config params.
int32_t Dp83826_config(EthPhyDrv_Handle hPhy, const void *pExtCfg, const uint32_t extCfgSize, Phy_Mii mii, bool loopbackEn)