AM263Px MCU+ SDK  11.01.00
TaskP.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2018-2023 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef TASKP_H
34 #define TASKP_H
35 
36 #ifdef __cplusplus
37 extern "C" {
38 #endif
39 
40 #include <stdint.h>
41 #include <kernel/dpl/SystemP.h>
42 #if defined(__ARM_ARCH_7R__)
43 #include <kernel/dpl/MpuP_armv7.h>
44 #endif
45 
58 typedef void (*TaskP_FxnMain)(void *args);
59 
63 #define TaskP_PRIORITY_LOWEST (0u)
64 
68 #define TaskP_PRIORITY_HIGHEST (31u)
69 
73 #define TaskP_LOAD_UPDATE_WINDOW_MSEC (500u)
74 
75 
79 typedef struct {
80 
81  const char *name;
82  uint64_t runTime;
83  uint64_t totalTime;
84  uint32_t cpuLoad;
86 } TaskP_Load;
87 
92 #if defined (OS_FREERTOS) || defined (OS_FREERTOS_SMP) || defined (OS_FREERTOS_MPU)
93 
94 #include <FreeRTOS.h>
95 #include <task.h>
96 
97 typedef struct TaskP_Object_ {
98 
99  StaticTask_t taskTcb;
100  TaskHandle_t taskHndl;
101  uint32_t lastRunTime;
102  uint64_t accRunTime;
103 
104 } TaskP_Object;
105 
106 #elif defined (OS_SAFERTOS)
107 
108 #include <SafeRTOS.h>
109 #include <task.h>
110 
111 typedef struct TaskP_Object_ {
112 
113  xTCB taskTcb;
114  portTaskHandleType taskHndl;
115  uint32_t lastRunTime;
116  uint64_t accRunTime;
117 
118 } TaskP_Object;
119 
120 #elif defined (OS_NORTOS)
121 
125 typedef struct TaskP_Object_ {
126 
127  uint32_t rsv;
128 
129 } TaskP_Object;
130 
131 #else
132 
133 #error "Define OS_FREERTOS or OS_FREERTOS_SMP or OS_FREERTOS_MPU or OS_SAFERTOS or OS_NORTOS"
134 
135 #endif
136 
140 typedef struct TaskP_Params_ {
141 
142  const char *name;
143  uint32_t stackSize;
144  uint8_t *stack;
145  uint32_t priority;
146  void *args;
148  uintptr_t coreAffinity;
150 } TaskP_Params;
151 
152 #if defined(__ARM_ARCH_7R__)
153 
158 typedef struct TaskP_MpuRegionConfig_ {
159  uint32_t baseAddr;
160  uint32_t sizeBytes;
170  MpuP_RegionAttrs attrs;
171 } TaskP_MpuRegionConfig;
172 
178 typedef struct TaskP_ParamsRestricted_ {
179  TaskP_Params params;
180  TaskP_MpuRegionConfig regionConfig[7U];
181  // TODO: Replace with below after TaskP refactor to include FreeRTOS headers and structs directly.
182  // TaskP_MpuRegionConfig regionConfig[portNUM_CONFIGURABLE_REGIONS]; /**< MPU region configurations */
183 } TaskP_ParamsRestricted;
184 #endif
185 
194 
206 int32_t TaskP_construct(TaskP_Object *obj, const TaskP_Params *params);
207 
208 #if defined(__ARM_ARCH_7R__)
209 
218 void TaskP_ParamsRestricted_init(TaskP_ParamsRestricted *params);
219 
230 int32_t TaskP_constructRestricted(TaskP_Object *obj, const TaskP_ParamsRestricted *params);
231 #endif
232 
238 void TaskP_destruct(TaskP_Object *obj);
239 
240 
248 void* TaskP_getHndl(TaskP_Object *obj);
249 
253 void TaskP_yield(void);
254 
265 void TaskP_exit(void);
266 
273 void TaskP_loadGet(TaskP_Object *obj, TaskP_Load *taskLoad);
274 
286 
293 
294 
301 
304 #ifdef __cplusplus
305 }
306 #endif
307 
308 #endif /* TASKP_H */
TaskP_FxnMain
void(* TaskP_FxnMain)(void *args)
Entry point to the task.
Definition: TaskP.h:58
TaskP_Params
Opaque task object used with the task APIs.
Definition: TaskP.h:140
args
void * args
Definition: hsmclient_msg.h:4
TaskP_Load
Task load statistics.
Definition: TaskP.h:79
SystemP.h
TaskP_Load::name
const char * name
Definition: TaskP.h:81
TaskP_loadResetAll
void TaskP_loadResetAll(void)
Reset task load statistics.
TaskP_Params::args
void * args
Definition: TaskP.h:146
TaskP_Params::name
const char * name
Definition: TaskP.h:142
TaskP_loadUpdateAll
void TaskP_loadUpdateAll(void)
Updated task load statistics.
TaskP_Params::taskMain
TaskP_FxnMain taskMain
Definition: TaskP.h:147
TaskP_exit
void TaskP_exit(void)
Exit current task.
MpuP_armv7.h
TaskP_yield
void TaskP_yield(void)
Yield current task.
TaskP_Params::stackSize
uint32_t stackSize
Definition: TaskP.h:143
TaskP_getHndl
void * TaskP_getHndl(TaskP_Object *obj)
Return OS defined task handle.
TaskP_Load::cpuLoad
uint32_t cpuLoad
Definition: TaskP.h:84
TaskP_Params::priority
uint32_t priority
Definition: TaskP.h:145
TaskP_construct
int32_t TaskP_construct(TaskP_Object *obj, const TaskP_Params *params)
Create a task object.
TaskP_loadGetTotalCpuLoad
uint32_t TaskP_loadGetTotalCpuLoad(void)
Get total CPU load including all task and ISR execution time.
TaskP_Load::runTime
uint64_t runTime
Definition: TaskP.h:82
TaskP_loadGet
void TaskP_loadGet(TaskP_Object *obj, TaskP_Load *taskLoad)
Get task load.
MpuP_RegionAttrs
Attribute's to apply for a MPU region.
Definition: MpuP_armv7.h:115
TaskP_Params::coreAffinity
uintptr_t coreAffinity
Definition: TaskP.h:148
TaskP_Load::totalTime
uint64_t totalTime
Definition: TaskP.h:83
TaskP_Params::stack
uint8_t * stack
Definition: TaskP.h:144
TaskP_Params_init
void TaskP_Params_init(TaskP_Params *params)
Set default values to TaskP_Params.
TaskP_destruct
void TaskP_destruct(TaskP_Object *obj)
Cleanup, delete, destruct a task object.