AM263Px MCU+ SDK  11.01.00
Security Related Tools

Signing Scripts

  • To run these scripts, one needs openssl installed as mentioned here, OpenSSL
  • Signing scripts are a collection of scripts needed to sign ROM images (image booted by ROM - mostly the SBL) and application images (image booted by the SBL)

Signing SBL

  • The RBL requires the boot image (mostly SBL), to be signed always, even if we are not using secure boot.

For SBL images, the script /source/security/security_common/tools/boot/signing/mcu_rom_image_gen.py.

For HS-FS devices:

cd ${SDK_INSTALL_PATH}/source/security/security_common/tools/boot/signing
$(PYTHON) mcu_rom_image_gen.py --image-bin <path-to-the-binary> --core R5 --swrv 1 --loadaddr $(SBL_RUN_ADDRESS) --sign-key <signing-key-configured-in-devconfig> --out-image <output-image-name> --debug $(DEBUG_OPTION)

For HS-SE devices:

cd ${SDK_INSTALL_PATH}/source/security/security_common/tools/boot/signing
$(PYTHON) mcu_rom_image_gen.py --sbl-enc --enc-key <encryption-key-configured-in-devconfig> --image-bin <path-to-the-binary> --core R5 --swrv 1 --loadaddr $(SBL_RUN_ADDRESS) --sign-key <signing-key-configured-in-devconfig> --kd-salt <path-to-key-derivation-salt> --out-image <output-image-name> --debug $(DEBUG_OPTION)

Here, we deep dive into the extension supported in SBL and HSM Runtime (TIFS-MCU) certificate by ROM. To get access to the HSM Runtime code and ability to build it for HS-SE device, please contact your TI representative to get access to the TIFS-MCU package from MySecureSW.

Boot Information OID (1.3.6.1.4.1.294.1.1)

bootInfo ::= SEQUENCE {
cert_type: INTEGER, -- identifies the certificate type
boot_core: INTEGER, -- identifies the boot core
core_opts: INTEGER, -- Core Options
load_addr: OCTET STRING, -- Global address image destination
image_size: INTEGER, -- Image size in bytes
}

The Boot Information Object identifier provides information about the image which is being loaded. This information is mandatory and needs to be present else the image boot will fail.

Elements of the extension:

Certificate Type: The certificate type defines the type of the image which is being loaded by the Boot-ROM.

These are the supported values:

  • 0x1 R5 SBL Boot Image
  • 0x2 HSM Runtime (TIFS-MCU) Image

Boot core: The boot core identifies the core on which the image will be executing.

These are the supported values:

  • 0x0 HSM Core
  • 0x10 R5 Core

Core Options: The core options are documented in the table below.

These are the supported values:

  • 0x0 Lock Step Mode
  • Non-Zero Dual Core Mode
Note
Currently, configuring this option is not supported with Signing scripts. This feature will be added in future releases.

Core options are applicable only for the R5 SBL Images.

Load Address: The load address will be address in the system where the image will be loaded. This is applicable for both SBL and TIFS-MCU (HSMRt) images.

Image Size: This is the size in bytes of the R5 SBL or HSM Runtime Image to which the certificate has been attached.

Image Integrity OID (1.3.6.1.4.1.294.1.2)

imageIntegrity ::= SEQUENCE {
sha_type: OID, -- Identifies the SHA type
hash: OCTET STRING -- The SHA of the boot image
}

If the X.509 certificate provides the image integrity boot extension, the Boot-ROM will perform the SHA-512 on the entire image and will verify the computed hash with the hash provided in the boot extension. In the case of a mismatch the boot will fail.

Elements of the extension:

SHA Type: The Boot-ROM only supports SHA-512.

The following values are supported:

2.16.840.1.101.3.4.2.3 SHA-512 Object Identifier

Please refer to the Section 2.4 of the RFC-5754 for the SHA-512 Object Identifier.

Hash: This is SHA-512 hash which is calculated over the image (R5 SBL/HSM Runtime)

R5 SBL Image:

  • HS-SE Device: Image Integrity is mandatory
  • HS-FS Device: Image Integrity is optional

HSM Runtime Image:

  • HS-SE Device: Image Integrity is mandatory
  • HS-FS Device: Image Integrity is mandatory

Software Revision OID (1.3.6.1.4.1.294.1.3)

softwareRevision ::= SEQUENCE {
revision: INTEGER -- Software revision
}

The information in the software revision is used to indicate the version of the image which is being loaded.

Elements of the extension:

revision: This is the version number. This will be matched to the EFUSE programmed version to indicate if the image loading should be done or not. This is applicable only for SE devices.

EFUSE Revision Certificate Revision Description
0 0 Ignore the revision checking. Images will always be loaded
0 >0 Device does not mandate revision checking. Images will be loaded
>0 0 EFUSE Version > Certificate Version. Image will never be loaded.
>0 >0 Image will be loaded only if the Certificate revision >= EFUSE revision

The following fields in efuse ROM help support the above feature:

  • SWRV_SBL- This is used to perform the revision checking while loading the R5 SBL
  • SWRV_HSM- This is used to perform the revision checking while loading the HSM Runtime

For more information, about how to fuse in these values, please refer to OTP Keywriter Documentation available on MySecureSW.

Image Encryption OID (1.3.6.1.4.1.294.1.4)

imageEncryption ::= SEQUENCE {
iv: OCTET STRING -- The initialization vector
rs: OCTET STRING -- Random string
iter: INTEGER -- Iteration count
salt: OCTET STRING -- encryption salt value
}

The Boot-ROM only supports AES-CBC mode with 256bit keys. The information in the image encryption object identifier is used to decrypt the image.

Elements of the extension:

IV: The initialization vector is used during the AES-CBC decryption procedure. The initialization vector needs to be 16bytes.

rs: This is the random string which is 32bytes long and is appended by the script at the end of the image. The Boot-ROM will decrypt the image and will perform a random string comparison to determine if the decryption was successful.

iter: Iteration Count which is used to determine if the HKDF needs to be performed and key derivation needs to be done. If the iteration count is 0 then the key from the e-fuse is used as is for the decryption. If the iteration count is non-zero then the Boot-ROM will perform the HKDF key derivation using the salt with exactly one iteration (even if iteration count is > 1). The derived key is then used for the decryption operation.

salt: The salt is used only if the iteration count is non-zero and key derivation is being done. The salt is fed to the HKDF module to derive the key. The salt fields should be 32bytes.

For recommendation on the salt, please refer to Enabling Secure Boot.

Note
It is recommended to update key derivation salt everytime there is a firmware upgrade. SBL, HSMRt and application images need to be prepared again, once the salt is changed.
  • HS-SE device: Image Encryption is optional
  • HS-FS device: Image Encryption is optional

Derivation OID (1.3.6.1.4.1.294.1.5)

derivationKey ::= SEQUENCE {
salt: OCTET STRING -- encryption salt value
}

The Boot-ROM will leave a derived key in the assets interface for the TIFS-MCU. The key is derived using HKDF from the parameters specified here. This is useful for decrypting application images by sending request to TIFS-MCU. For recommendation on the salt, please refer to Enabling Secure Boot.

Elements of the extension:

salt: The salt is limited to be 32bytes and is used for key derivation

This OID is ignored as part of HSM Runtime certificates. This OID is ignored as part of SBL certificates if the device type is HS-FS. Key derivation is always done using the active user symmetric key.

Debug OID (1.3.6.1.4.1.294.1.8)

Debug::= SEQUENCE {
uid OCTET STRING -- Device unique ID
debugType INTEGER -- Debug type
coreDbgEn INTEGER -- Enable core debug mask
secCoreDbgEn INTEGER -- Enable secure core debug mask
}

The debug object identifier if specified allows the debug ports to be enabled for a specific device.

Elements of the extension:

UID: This is the unique identifier associated with the device. Device specific unique identifiers can be retrieved using the SOC_ID Parser.

The UID field of all 0s is considered to be a wildcard. This is what is supported by default in the script.

Debug Type: This is the privilege level of debug.

The privilege levels supported by ROM are as follows:

Privilege Level Value Description
DBG_PERM_DISABLE 0 Disable debug ports for all cores.
DBG_SOC_DEFAULT 1 Maintain debug ports for all cores to device type defaults.
DBG_PUBLIC_ENABLE 2 Enable debug ports on R5FSS0-0 core.

coreDbgEn and secCoreDbgEn: These fields are not used and will be ignored.

Note
The Debug OID is not applicable for HSM Runtime (TIFS-MCU) image.

In the SBL Signing scripts, DEBUG_OPTION is used to exercise the debug level if the SBL certificate has debug extension. The SBL certificate as mentioned before, is processed by ROM. This is different from the debug certificate supported by TIFS-MCU.

This feature is leveraged via compile time flags in MCU+ SDK for SBL images.

By default, in SDK, the debug extension is not engaged for SBL images. This is decided by the flag DEBUG_TIFS defined in devconfig.mak. By default, DEBUG_TIFS is set to yes.This means that the debug extension will not be added to SBL and if the debug needs to be exercised via the certificate to TIFS-MCU via the debug authentication service, it can be safely done. This is done to ensure that the registers are written once only to exercise the debug during a POR cycle. If the user wants to open up debug on an HS-SE device, they can set DEBUG_TIFS=no. This is when the debug extension is added to the certificate for SBL images.

Note
ROM does not allow FULL_ENABLE privilege level via SBL certificate. To open up debug on HSM core, please refer to Debug Authentication services provided via TIFS-MCU. In this case, please use the default value of DEBUG_TIFS i.e. yes when compiling SBL examples.

The default debug privilege used in SDK is DBG_SOC_DEFAULT.

To enable debug on public cores on HS-SE device, one can use the following command to compile SBL examples.

make -s -C examples/drivers/boot/sbl_qspi/am263x-cc/r5fss0-0_nortos/ti-arm-clang all DEVICE=am263x DEVICE_TYPE=HS DEBUG_TIFS=no DEBUG_OPTION=DBG_PUBLIC_ENABLE
  • Here,
    • SBL_RUN_ADDRESS is 0x70002000
    • In the case of HS-FS devices, the key value is disregarded. A degenerate RSA public key is used to sign the certificate. The image integrity is checked in ROM, nevertheless.
    • In the case of HS-SE device, more details can be found at Enabling Secure Boot
    • Refer to TRM Chapter on Initialization, section 5.6.4.1.1 to get help on RSA key pair generation.

These scripts are invoked in makefiles, and the image generation happens automatically along with the example build. So mostly these scripts need not be manually run. If the user build-system is different from TI's makefile system, it needs to be ensured that the same is followed as part of the post build steps. The devconfig has ENC_SBL_ENABLED=yes and that is why for HS-SE devices, the SBL image is encrypted by default.

The Boot Information Object identifier provides information about the image which is being loaded.

Elements of the extension:

Certificate Type: The certificate type defines the type of the image which is being loaded by the Boot-ROM.

These are the supported values:

  • 0xA5A50000 Application Image

Boot core: This field is reserved and should be assigned with 0.

Core Options: This field is reserved and should be assigned with 0.

Load Address: This field is reserved and should be assigned with 0.

Image Size: This is the size in bytes of the R5 SBL or HSM Runtime Image to which the certificate has been attached.

Image Integrity OID (1.3.6.1.4.1.294.1.2)

imageIntegrity ::= SEQUENCE {
sha_type: OID, -- Identifies the SHA type
hash: OCTET STRING -- The SHA of the boot image
}

If the X.509 certificate provides the image integrity boot extension, the TIFS-MCU will perform the hash calculation on the entire image and will verify the computed hash with the hash provided in the boot extension. In the case of a mismatch the boot will fail.

Elements of the extension:

SHA Type:

The following values are supported:

  • 2.16.840.1.101.3.4.2.1 SHA-256 Object Identifier
  • 2.16.840.1.101.3.4.2.2 SHA-384 Object Identifier
  • 2.16.840.1.101.3.4.2.3 SHA-512 Object Identifier

Amongst these, SDK has been validated against SHA-512 OID.

Hash: This is SHA-512 hash which is calculated over the application image

Software Revision OID (1.3.6.1.4.1.294.1.3)

softwareRevision ::= SEQUENCE {
revision: INTEGER -- Software revision
}

The information in the software revision is used to indicate the version of the image which is being loaded.

Elements of the extension:

revision: This is the version number. This will be matched to the EFUSE programmed version to indicate if the image loading should be done or not.

The following fields in efuse ROM help support the above feature:

  • SWRV_APP- This is used to perform the revision checking while loading the application

For more information, about how to fuse in these values, please refer to OTP Keywriter Documentation available on MySecureSW.

Image Encryption OID (1.3.6.1.4.1.294.1.4)

imageEncryption ::= SEQUENCE {
iv: OCTET STRING -- The initialization vector
rs: OCTET STRING -- Random string
iter: INTEGER -- Reserved
salt: OCTET STRING -- Reserved
}

TIFS-MCU only supports AES-CBC mode with 256bit keys. The information in the image encryption object identifier is used to decrypt the image.

Elements of the extension:

IV: The initialization vector is used during the AES-CBC decryption procedure. The initialization vector needs to be 16bytes.

rs: This is the random string which is 32bytes long and is appended by the script at the end of the image. TIFS-MCU will decrypt the image and will perform a random string comparison to determine if the decryption was successful.

iter: This field is unused and reserved.

salt: This field is unused and reserved.

Keyring Index OID (1.3.6.1.4.1.294.1.12)

keyring_index ::= SEQUENCE {
sign_key_id: INTEGER -- index of public key hash in public keyring for authentication
enc_key_id: INTEGER -- index of aes key in keyring for decryption
}

TIFS-MCU only supports authentication with keyring. The information in enc_key_id is ignored and decryption is done against root of trust if Image Encryption OID is available in the certificate.

Elements of the extension:

sign_key_id: This is the index used in public keyring for retrieving the public key hash for authentication.

enc_key_id: This is the index used in keyring for retrieving the aes key for decryption of application image.

Application Signing

For Application images, the script /source/security/security_common/tools/boot/signing/mcu_appimage_x509_cert_gen.py.

For HS-SE devices:

cd ${SDK_INSTALL_PATH}/source/security/security_common/tools/boot/signing
$(PYTHON) mcu_appimage_x509_cert_gen.py --bin <path-to-the-binary> --key <signing-key-configured-in-devconfig> --enc y --enckey <encryption-key-configured-in-devconfig> --kd-salt <path-to-key-derivation-salt> --output <output-image-name>

Signing of application images is not required for HS-FS device types.

Here, we deep dive into the extension supported with certificate for Application images as processed by TIFS-MCU. To get access to the HSM Runtime code and ability to build it for HS-SE device, please contact your TI representative to get access to the TIFS-MCU package from MySecureSW.

Boot Information OID (1.3.6.1.4.1.294.1.1)

bootInfo ::= SEQUENCE {
cert_type: INTEGER, -- identifies the certificate type
boot_core: INTEGER, -- Reserved
core_opts: INTEGER, -- Reserved
load_addr: OCTET STRING, -- Reserved
image_size: INTEGER, -- Image size in bytes
}

Keyring Cert Generation Python Script

Note
Support for encryption with symmetric auxiliary keys will be added in future releases.

Keyring certificate generation and import
$python3 keyring_cert_gen.py --root_key ../../source/security/security_common/tools/boot/signing/mcu_custMpk.pem --keys_info keys.json
  • This script is used to generate X.509 certificate for keyring.
  • Make sure that python3 and its dependent modules are installed in the host machine as mentioned in Python3
  • keyring_cert_gen.py parses json object containing the following meta-data for keyring cert generation:
    • keyring_sw_rev: This integer value is used for anti-rollback check against the keyring software revision available in device efuses.
    • keyring_ver: Keyring version is of type integer and is the version which is supported against the TIFS-MCU version being used in HSM.
    • num_of_asymm_keys: Number of Asymmetric keys being imported.
    • num_of_symm_keys: Number of Symmetric keys being imported.
    • keyring_asymm: Array of asymmetric keys with respective key rights and hash algorithm to compute and store the hash of the public key.
      {
      "keyring_sw_rev" : 1,
      "keyring_ver" : 1,
      "num_of_asymm_keys" : 7,
      "num_of_symm_keys" : 0,
      "keyring_asymm" : [
      {
      "key_rights": "000000AA",
      "pub_key": "aux_keys/public2k.pem",
      "hash_algo": "SHA256"
      },
      {
      "key_rights": "000000AA",
      "pub_key": "aux_keys/public3k.pem",
      "hash_algo" : "SHA512"
      },
      {
      "key_rights": "000000AA",
      "pub_key": "aux_keys/public4k.pem",
      "hash_algo" : "SHA512"
      },
      {
      "key_rights": "000000AA",
      "pub_key": "aux_keys/prime265v1_public.pem",
      "hash_algo" : "SHA512"
      },
      {
      "key_rights": "000000AA",
      "pub_key": "aux_keys/secp384r1_public.pem",
      "hash_algo" : "SHA512"
      },
      {
      "key_rights": "000000AA",
      "pub_key": "aux_keys/secp521r1_public.pem",
      "hash_algo" : "SHA384"
      },
      {
      "key_rights": "000000AA",
      "pub_key": "aux_keys/brainpoolp512r1_public.pem",
      "hash_algo" : "SHA384"
      }
      ],
      "keyring_symm" : []
      }
  • Each asymmetric key json object contain 3 fields:
    • key_rights: Integer value in HEX format which signifies the rights associated with the key.
      • debugAuth (0-3b) - flag to indicate key right for debug certificate authentication
      • imageAuth (4-7b) - flag to indicate key right for application image authentication
      • For example: 0x000000AA represents the public can be used for both imageAuth and debugAuth
    • pub_key: Location of the public key
    • hash_algo: Hash algorithm used for hashing public key.
      • SHA256, SHA384 and SHA512 are valid hash algorithms.
  • keyring_cert_gen.py expects 2 mandatory arguments:
    • root_key: certificate is signed using customer MPK and expects path to customer active ROT.
    • keys_info: json file with keyring meta data.
  • If RSASSA-PSS algorithm for authentication of keyring certificate is required, provide the –rsassa_pss flag and –pss_saltlen value. Maximum supported salt length value for RSASSA-PSS is 255. Please refer to the command below
    $python3 keyring_cert_gen.py --root_key ../../source/security/security_common/tools/boot/signing/mcu_custMpk.pem --keys_info keys.json --rsassa_pss --pss_saltlen 64
  • A dummy json and keyring certificate header file is also availble in ${SDK_INSTALL_PATH}/tools/keyring_cert for reference.
  • Below are the logs after execution of script
    keyring version = 1
    keyring software revision = 1
    Number of asymmetric keys = 7
    Number of symmetric keys = 0
    [ keyring_asymm ]
    asymm_key0=SEQUENCE:comp0
    asymm_key1=SEQUENCE:comp1
    asymm_key2=SEQUENCE:comp2
    asymm_key3=SEQUENCE:comp3
    asymm_key4=SEQUENCE:comp4
    asymm_key5=SEQUENCE:comp5
    asymm_key6=SEQUENCE:comp6
    [ comp0 ]
    keyId=INTEGER:32
    key_rights=FORMAT:HEX,OCT:000000AA
    hash_algo=INTEGER:6
    public_key=FORMAT:HEX,OCT:582fc2a6cc997d2df6c0299aeef0a7b606d3fcc2261dfade8c2684c6663ab50b
    [ comp1 ]
    keyId=INTEGER:33
    key_rights=FORMAT:HEX,OCT:000000AA
    hash_algo=INTEGER:4
    public_key=FORMAT:HEX,OCT:6e430c4a09572240f9acd4b4777b2d662fe28c73ef475280d8a4e7c766d13680b14549a84e6e6c7b69a0ba33840dc9f51f110afb156251a6139c26693e6d4ddf
    [ comp2 ]
    keyId=INTEGER:34
    key_rights=FORMAT:HEX,OCT:000000AA
    hash_algo=INTEGER:4
    public_key=FORMAT:HEX,OCT:67cd4b91e7966af635a53642102abb2c8fdab1a47277c88eb4ec3e1a6ce5155a2325f66b3d392f3f5091e526057cd5e6b6d5085ae46f169c61de77c7dffbb238
    [ comp3 ]
    keyId=INTEGER:35
    key_rights=FORMAT:HEX,OCT:000000AA
    hash_algo=INTEGER:4
    public_key=FORMAT:HEX,OCT:79bd183d942cbf1542a2bad2a469242392c515c1546fc8a43e86a024097ba4bb4db65ccade7fb6b252deccd255491151df927f998d468153072cf3e4949d6002
    [ comp4 ]
    keyId=INTEGER:36
    key_rights=FORMAT:HEX,OCT:000000AA
    hash_algo=INTEGER:4
    public_key=FORMAT:HEX,OCT:4a8959978336886acbe3cf294b1b8e1aa68f1cb836d78aa11332a57cb44c435c82fc672901a2a242e5169543502106ac0cda1b04a9769723154d640e832298ba
    [ comp5 ]
    keyId=INTEGER:37
    key_rights=FORMAT:HEX,OCT:000000AA
    hash_algo=INTEGER:2
    public_key=FORMAT:HEX,OCT:1b759f0c0b04796cc599033bd58e33730ce6b2380f7442fe030beffa3cc844ce0d196f48e5ebeb6d88eea0f7ddc3beb7
    [ comp6 ]
    keyId=INTEGER:38
    key_rights=FORMAT:HEX,OCT:000000AA
    hash_algo=INTEGER:2
    public_key=FORMAT:HEX,OCT:b502e951a5f5ed4bc99191511b530597d3a2d356d0f83887a54253a7ec46fb2c081c7d39391f846932357a57133f8c11

Boot time calculator tool

Checkout the secure boot time calculator tool here.