AM263Px MCU+ SDK  11.01.00
Enet CPSW Ether-Ring TSN Example

Introduction

This example application illustrates the configuration and usage of Ether-Ring topology with 4 nodes connected in loop where each node works as central compute, zone left, zone right and zone tail. The example application enables both MAC ports by default and each node is connected to it's neighbouring node in a loop. This application uses Concurrence execution of gPTP IEEE 802.1AS stack and IEEE 802.1 Qbv (EST) configuration and Ether-ring (‘802.1CB-like’) to support Packet Duplication, Ring Termination in Hardware and Duplicate Rejection in Software.

The example application opens two DMA TX channels and two DMA RX channels. The TX0 and RX0 DMA channel will be used by the application to send the Class-A and Class-D stream packets via Ether-Ring Driver. The TX0 and RX0 DMA channel will be used for GPTP.

The application will also open the both MAC port and will wait until the port gets link up with neighbouring node. The application waits for GPTP synchronization to happen and then applies the EST Schedule on both MAC ports.

The application uses Enet Time Aware Shaper API for EST configuration ,Ethernet TSN and gPTP Stack - API and Integration Guide for gPTP and Enet Data Path (DMA) API for packet transmission.

Note
This application only provides the Etherring Functionality. But the Performance will be acheived in further releases.

Ether-Ring overview

Please refer here for Ether-Ring overview

Configuration Parameters

Typically, the application's parameters that a developer may want to change are:

  • Number of Nodes. By default the example application configures the etherring for 4 Nodes, but the user can choose to update the number of nodes in etherring using MAX_NODES_IN_LOOP = 4 in config.h.
  • Number of Class A Streams. By default the number of Class A Streams are configured as 1 for each Node. User can update the configuration bye changes NUM_CLASSA_STREAMS in config.h.
  • Class A Payload Length. Class A payload length is configured as 1000 be default and user can update CLASSA_PAYLOAD_LENGTH in config.h .
  • Class D Payload Length. Class D payload length is configured as 1450 be default and user can update CLASSD_PAYLOAD_LENGTH in config.h .

Application Functionality

Ether-Ring Application Flow

The Application creates Class-A, Class-D stream RTOS tasks which creates the 802.1Q Ethernet Multicast packet with stream configuration and calls "EtherRing_submitTxPktQ" API from Ether-Ring Driver. "EtherRing_submitTxPktQ" creates a custom 802.1 CB-like header(4 bytes) which consists of CB-like Ethertype(0xF1C1), unique sequence ID for each Ethernet packet and adds the CB-like Header to the packet sent from application without modifying the payload using zero-copy (using Transmit Scatter-Gather feature of HW). The packet is submitted to DMA and CPSW duplicates the multicast packet and sent it to both MAC ports.

Ether-Ring Transmit Flow

When the packets are received RX DMA ISR will be triggered and "EtherRing_retrieveRxPktQ" is called from RTOS Rx application task. "EtherRing_retrieveRxPktQ" calls the DMA Retrieve API to retrieve the packets and Duplicate Packet Rejection is done using {SrcMacAddr, Sequence Number} based Look-up Table. Original stream packets found using look-up table are sent to Application and Duplicate packets received are submitted back to the DMA.

Ether-Ring Receive Flow

EST Schedule

This EST schedule is 1 msec long and is composed of 8 intervals, each with a gate mask that enables transmission of 2,3 are configured for Class A and Class D streams.

EST schedule parameters
Parameter Time Value
BaseTime Current time + MAX_BASE_TIME_US
CycleTime 1 msec
Gate control list
Gate Control Time Interval
oCCCooCC 125 usecs
oCCCCCCC 125 usecs
oCCCCCCC 125 usecs
oCCCCCCC 125 usecs
oCCCCCCC 125 usecs
oCCCCCCC 125 usecs
oCCCCCCC 125 usecs
oCCCCCCC 125 usecs

The priority being referred to in the EST schedule described above corresponds to the CPSW destination port hardware switch priority. For VLAN tagged packets that ingress through CPSW host port, the hardware switch priority can be determined by either the CPPI channel number (P0_RX_REMAP_VLAN = 0) or the packet priority value from the VLAN tag (P0_RX_REMAP_VLAN = 1).

/* Hardware switch priority is taken from packet's PCP or DSCP */
hostPortCfg->rxVlanRemapEn = true;
hostPortCfg->rxDscpIPv4RemapEn = true;
hostPortCfg->rxDscpIPv6RemapEn = true;

RX Host Time stamping

RX Host time stamping is enabled from syscfg to measure the jitter in latency for the Received packets and timestamp value is stored in "rxPktTs" for each received packet(pktInfo). The timestamp values are stored in Ether-Ring driver for Jitter measurement.

ALE Configuration

  • The Default Multicast ALE Entry for PTP has been updated to send PTP Packets only to the Host port. The port mask has been updated to 0x1 and ALE Entry is added.
  • Vlan entry for default port vlan is updated to enable forceUntaggedEgressMask for all ports so that vlan tag is not added to ptp packets when ALE is in vlanAware mode.

Ether-Ring Start Menu

The following helper options are also provided in the application's start menu to configure the each node uniquely in Etherring:

0 - Central Compute Node
1 - Zone Left Node
2 - Zone Right Node
3 - Zone Tail Node
Enter the nodeId :

Supported Combinations

Parameter Value
CPU + OS r5fss0-0_freertos
Toolchain ti-arm-clang
Boards am263px-lp
Example folder source/networking/enet/core/examples/ether_ring

Packet pool configuration

To change packet pool configuration from syscfg, please refer to Ethernet Packet Pool Allocation Guidelines

Steps to Run the Example

Build the example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

HW Setup

Make sure you have setup the EVM with cable connections as shown in below Diagram. In addition, follow the steps in the next section.

Ether-Ring EVM Connections
Note
Ethernet cable must be connected to both the ports in loop for the example application to run with expected results.

Run the example

Basic Test

The simplest test that one can run with the ETHERRING example consists of:

  • Configuring the each node uniqly in the Ether-ring Network and wait for PTP synchronization to happen for all the Nodes.
  • Enabling EST and programming a custom EST schedule on the both MAC ports once PTP is synchronized.
  • Sending Class A and Class D stream packets with different priorities to the adjacent node in clock-wise and anti clock-wise direction in the loop.

The steps to run this test are:

  • Connect the MAC port as described in HW Setup section and configure the Nodes using UART Terminal.
  • Launch a CCS debug session and run the example executable, see CCS Launch, Load and Run.
  • Application logs such as cycle time, time intervals and gate masks will be printed in the serial console. Sample logs are shown in the next section.
  • Configure the each node as mentioned in Ether-Ring Start Menu section using UART Terminal around the same time in all the Nodes to start the application and wait for ----------ETHERRING DEMONSTRATION COMPLETED---------- to be printed on UART Terminal.

Sample output

==========================
EtherRing App
==========================
0 - Central Compute Node
1 - Zone Left Node
2 - Zone Right Node
3 - Zone Tail Node
Enter the nodeId :
0
start to open driver.
EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:0 From 4 To 2
Init all configs
----------------------------------------------
sitara-cpsw: init config
Open MAC port 1
EnetPhy_bindDriver:1843
Open MAC port 2
EnetPhy_bindDriver:1843
PHY 3 is alive
PHY 12 is alive
sitara-cpsw: Create RX task for regular traffic
initQs() txFreePktInfoQ initialized with 48 pkts
MAC port addr: 70:ff:76:1f:6a:46
sitara-cpsw: default RX flow started
Waiting for GPTP ready!!
Start: uniconf_task
EnetApp_uniconfTask: dbname: NULL
EnetApp_gptpYangConfig:domain=0
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_SINGLE_CLOCK_MODE=1
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_USE_HW_PHASE_ADJUSTMENT=1
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_CLOCK_COMPUTE_INTERVAL_MSEC=100
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_FREQ_OFFSET_IIR_ALPHA_START_VALUE=1
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_FREQ_OFFSET_IIR_ALPHA_STABLE_VALUE=4
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_PHASE_OFFSET_IIR_ALPHA_START_VALUE=1
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_PHASE_OFFSET_IIR_ALPHA_STABLE_VALUE=4
EnetApp_gptpNonYangConfig:XL4_EXTMOD_XL4GPTP_MAX_DOMAIN_NUMBER=1
Start: gptp2d_task
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
GPTP ready!!
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
Start: melcoApp_EST
EnetApp_initTsn:TSN app start done!
ClassA stream count:1
ClassD stream count:1
Waiting for GPTP ready!!
GPTP ready!!
Waiting for GPTP ready!!
GPTP ready!!
Logger_task: started
unibase-1.1.4
INF:cbase:tilld0: has mac: 70:FF:76:1F:6A:46
INF:cbase:tilld1: has mac: 00:00:00:00:00:00
INF:cbase:cb_lld_task_create: uniconf_task stack_size=8192
INF:uconf:simpledb_open:no data is imported
INF:uconf:get_next_nameid:a new mod=xl4-data, enum=0
INF:uconf:get_next_nameid:a new mod=xl4-extmod, enum=1
INF:uconf:uc_hwal_open:
INF:cbase:cb_rawsock_open:combase-1.1.3
INF:cbase:cb_rawsock_open:dmaTxChId=-1 numRxChannels=1 dmaRxChId=-1 nTxPkts=0 nRxPkts=0 pktSize=0
INF:uconf:get_next_nameid:a new mod=ietf-interfaces, enum=2
INF:uconf:get_next_nameid:a new mod=ieee1588-ptp-tt, enum=3
INF:uconf:get_next_nameid:a new mod=ieee802-dot1q-bridge, enum=4
INF:uconf:get_next_nameid:a new mod=excelfore-tsn-remote, enum=5
INF:uconf:get_next_nameid:a new mod=excelfore-netconf-server, enum=6
INF:uconf:get_next_nameid:a new mod=ietf-netconf-monitoring, enum=7
INF:uconf:get_next_nameid:a new mod=ietf-yang-library, enum=8
INF:uconf:get_next_nameid:a new mod=ieee802-dot1ab-lldp, enum=9
INF:uconf:get_nWRN:gptp:gptpgcfg_link_check:can't read speed
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
Cpsw_handleLinkUp:1645
MAC Port 1: link up
INF:cbase:cbl_query_response:tilld0: link UP, speed=1000, duplex=1 !!!!
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
WRN:gptp:000013-500229:waiting_for_pdelay_interval_timer_proc:portIndex=1, sourcePortIdentity=34:08:E1:FF:FE:84:DB:CF, thisClock=70:FF:76:FF:FE:1F:6A:46, neighborPropDelay=392
Cpsw_handleLinkUp:1645
MAC Port 2: link up
INF:cbase:cbl_query_response:tilld1: link UP, speed=1000, duplex=1 !!!!
portIdx=0 netdev tilld0
Current port-state: 3
portIdx=1 netdev tilld1
Current port-state: 3
Waiting errfor PTP clock to be synchronized!
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
WRN:gptp:000014-625027:waiting_for_pdelay_interval_timer_proc:portIndex=2, sourcePortIdentity=34:08:E1:FF:FE:84:DD:31, thisClock=70:FF:76:FF:FE:1F:6A:46, neighborPropDelay=392
portIdx=0 netdev tilld0
syncFlag: 0
Current port-state: 9
EnetApp_enableCBS
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:ydbi_get_item_ifk4vk1:no data
INF:uconf:get_queue_map_params:netdev=tilld0, num_tc=0
The following AdminList param will be configured for EST:
GateMask[7..0]=oCCCoCCC (0x88), start=0 ns, end=19999 ns, dur=20000 ns
GateMask[7..0]=oCCCCoCC (0x84), start=20000 ns, end=124999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=125000 ns, end=144999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=145000 ns, end=249999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=250000 ns, end=269999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=270000 ns, end=374999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=375000 ns, end=394999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=395000 ns, end=499999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=500000 ns, end=519999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=520000 ns, end=624999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=625000 ns, end=644999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=645000 ns, end=749999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=750000 ns, end=769999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=770000 ns, end=874999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=875000 ns, end=894999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=895000 ns, end=999999 ns, dur=105000 ns
Base time=20000000000ns,Cycle time=1000000ns
Set admin control list succesfully
EnetApp_enableCBS
INF:uconf:create_semname_with_dbname:null dbname is specified.
INF:uconf:ydbi_get_item_ifk4vk1:no data
INF:uconf:get_queue_map_params:netdev=tilld1, num_tc=0
INF:uconf:get_queue_map_params:netdev=tilld0, num_tc=8
INF:cbase:TAS state is set to 2
INF:cbase:TAS operational list status updated:
INF:cbase:TAS state is set to 1
INF:cbase:Successfully configure TAS
The following AdminList param will be configured for EST:
GateMask[7..0]=oCCCoCCC (0x88), start=0 ns, end=19999 ns, dur=20000 ns
GateMask[7..0]=oCCCCoCC (0x84), start=20000 ns, end=124999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=125000 ns, end=144999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=145000 ns, end=249999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=250000 ns, end=269999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=270000 ns, end=374999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=375000 ns, end=394999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=395000 ns, end=499999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=500000 ns, end=519999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=520000 ns, end=624999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=625000 ns, end=644999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=645000 ns, end=749999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=750000 ns, end=769999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=770000 ns, end=874999 ns, dur=105000 ns
GateMask[7..0]=oCCCoCCC (0x88), start=875000 ns, end=894999 ns, dur=20000 ns
GateMask[7..0]=oCCCCCCC (0x80), start=895000 ns, end=999999 ns, dur=105000 ns
Base time=20000000000ns,Cycle time=1000000ns
Set admin control list succesfully
INF:uconf:get_queue_map_params:netdev=tilld1, num_tc=8
INF:cbase:TAS state is set to 2
INF:cbase:TAS operational list status updated:
INF:cbase:TAS state is set to 1
INF:cbase:Successfully configure TAS
WRN:gptp:000018-746101:md_pdelay_resp_sm_recv_req: port=2, expected SeqID=10723, but received=10724
Starting the Stream Traffic
RxTs and CurrentTs values stored
[RXTS]: 29954385101
[RXTS]: 29954510117
[RXTS]: 29954635123
[RXTS]: 29954760134
[RXTS]: 29954885145
[RXTS]: 29955010066
[RXTS]: 29955135082
[RXTS]: 29955260083
[RXTS]: 29955385094
[RXTS]: 29955510120
[RXTS]: 29955635121
[RXTS]: 29955760127
[RXTS]: 29955885143
[RXTS]: 29956010069
[RXTS]: 29956135075
[RXTS]: 29956260086
[RXTS]: 29956385097
[RXTS]: 29956510113
[RXTS]: 29956635119
[RXTS]: 29956760130
[RXTS]: 29956885126
[RXTS]: 29957010072
[RXTS]: 29957135078
----------ETHERRING DEMONSTRATION COMPLETED----------

Troubleshooting issues

  • To ensure compatibility with CPSW RGMII2 port on am263px-cc board, make sure that SW-15(switch) should be set to LOW for board versions(E2/A/B versions). This configuration ensures seamless out-of-box support and functionality with the CPSW RGMII2 port on the specified versions.

See Also

Ethernet And Networking