AM263Px MCU+ SDK  11.01.00
Ethernet Add-on Boards

Introduction


AM263Px Control Card(TMDSCND263P) board provides the support for Ethernet add-on boards.

  1. Automotive Ethernet add-on Board(DP83TG720-EVM-AM2)
  2. Industrial Ethernet add-on Board(DP83826-EVM-AM2)

The diagram below shoes the top view of AM263Px Control Card which shows the Ethernet add-on board connector.

Figure: AM263px Control Card with DP83TG720 Ethernet Add-on Board

Important Usage Guidelines

Note
Automotive Ethernet PHY(DP83TG720-EVM-AM2) doesn't support auto negotiation and works only in 1Gbps.
In order to support Automotive Ethernet add-on board on AM263Px Control Card, board modifications are needed. Please refer to the Table 2-16(Ethernet Routing) in User Guide for board modifications. AM263Px Control Card Evaluation Module User's Guide (Rev. A)

In order to run Out-of-Box examples for Automotive Ethernet PHY(DP83TG720-EVM-AM2) and Industrial Ethernet PHY(DP83826-EVM-AM2), make following changes in the syscfg tool:

Syscfg tool to configure only for Ethernet Add-on board(Auto PHY):

Figure: Syscfg tool to configure Ethernet Add-on board(Auto PHY)

Make these below changes in the API EnetApp_initLinkArgs to change the speed and duplexity in order to support Automotive Ethernet PHY(DP83TG720-EVM-AM2) usecases.

Figure: Change speed and duplexity