AM263Px MCU+ SDK  11.01.00
Enet CPSW Operation Modes Demo

Introduction

  • CPSW operates in two modes
    • Switch Mode - packet forwarding is enabled and packets are forwarded to Host + Other MAC ports. This is the default configuration for CPSW.
    • MAC mode - packets are only given to the Host port and are not forwarded to other MAC Ports.

CPSW DUAL MAC Mode

  • In this mode, both the MAC ports of AM263PX are configured to be in MAC mode.
  • This mode requires two Network interfaces to operate.
  • It is recommended to use two separate subnets for working with DUAL MAC.
  • A single implementation of network interface and shared pool is used for both the Netifs.
  • Dual MAC feature is illustrated by the below image:

DUAL MAC Operation

See Also

Ethernet And Networking