AM263Px MCU+ SDK  11.01.00
SHA

Access Protection Scheme

AES and SHA IP in DTHE support two contexts, namely Public and Secure.

Note
Dma functionality is not yet added in dthe R5f, it will be added in the future.

SHA

  • The Hash/HMAC engine performs the SHA-1, SHA-2, and MD5 hash computation. When loaded with a data block, and optionally an intermediate digest, it independently performs the hash computation (64 or 80 rounds, depending on the algorithm) on that data block.
  • The engine can also start from the specified initial digest values instead of a loaded intermediate. Furthermore, it can perform the IPAD and OPAD XORs for MAC operations. The hash core does not perform any hash padding; this is performed in the host interface block, where the data input registers are located. A loaded data block must always be a full 64 bytes (512 bits) long.

sha module block diagram

API Sequence for SHA Algorithms

This sequence performs SHA-512 and SHA-256.

API Sequence for HMAC-SHA Algorithms

This sequence performs HMAC SHA-512 and SHA-256.

API