![Logo](ti_logo.svg) |
AM263Px MCU+ SDK
09.01.00
|
|
Go to the documentation of this file.
47 #ifndef ENET_MOD_HOSTPORT_H_
48 #define ENET_MOD_HOSTPORT_H_
67 #define ENET_HOSTPORT_PUBLIC_IOCTL(x) (ENET_IOCTL_TYPE_PUBLIC | \
68 ENET_IOCTL_HOSTPORT_BASE | \
78 typedef enum EnetHostPort_Ioctl_e
237 typedef enum EnetHostPort_IngressPriorityType_e
@ ENET_HOSTPORT_IOCTL_SET_INGRESS_DSCP_PRI_MAP
Set ingress DSCP priority (TOS) map.
Definition: enet_mod_hostport.h:123
#define ENET_HOSTPORT_PUBLIC_IOCTL(x)
Helper macro to create IOCTL commands for host port module.
Definition: enet_mod_hostport.h:67
@ ENET_HOSTPORT_IOCTL_SET_CREDIT_BASED_SHAPING
Set Idleslope for Credit Based Shaper on Host Port.
Definition: enet_mod_hostport.h:222
@ ENET_HOSTPORT_IOCTL_ENABLE
Enable host port.
Definition: enet_mod_hostport.h:105
@ ENET_HOSTPORT_IS_CSUM_OFFLOAD_ENABLED
Check if checksum offload is enabled.
Definition: enet_mod_hostport.h:213
This file contains the type definitions and helper macros that are common for host and MAC ports.
EnetHostPort_Ioctl
Host port IOCTL commands.
Definition: enet_mod_hostport.h:79
@ ENET_HOSTPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP
Set QoS egress priority map.
Definition: enet_mod_hostport.h:159
@ ENET_HOSTPORT_IOCTL_GET_EGRESS_QOS_PRI_MAP
Get QoS egress priority map.
Definition: enet_mod_hostport.h:168
@ ENET_INGRESS_PRI_TYPE_FIXED
Definition: enet_mod_hostport.h:240
EnetHostPort_IngressPriorityType
Port priority type.
Definition: enet_mod_hostport.h:238
@ ENET_HOSTPORT_IOCTL_ENABLE_INGRESS_TRAFFIC_SHAPING
Enable ingress traffic shaping configuration.
Definition: enet_mod_hostport.h:177
@ ENET_HOSTPORT_IOCTL_GET_INGRESS_DSCP_PRI_MAP
Get ingress DSCP priority (TOS) map.
Definition: enet_mod_hostport.h:132
@ ENET_HOSTPORT_IOCTL_GET_MAXLEN
Get MRU and MTU.
Definition: enet_mod_hostport.h:204
@ ENET_HOSTPORT_IOCTL_GET_INGRESS_TRAFFIC_SHAPING
Get ingress traffic shaping configuration.
Definition: enet_mod_hostport.h:195
@ ENET_HOSTPORT_IOCTL_PRINT_REGS
Print host port registers.
Definition: enet_mod_hostport.h:96
@ ENET_HOSTPORT_IOCTL_SET_PRI_REGEN_MAP
Set VLAN priority regeneration map.
Definition: enet_mod_hostport.h:141
@ ENET_HOSTPORT_IOCTL_GET_PRI_REGEN_MAP
Get VLAN priority regeneration map.
Definition: enet_mod_hostport.h:150
This file contains the type definitions and helper macros for the Enet Module interface.
@ ENET_HOSTPORT_IOCTL_GET_CREDIT_BASED_SHAPING
Get Idleslope of Credit Based Shaper on Host Port.
Definition: enet_mod_hostport.h:231
@ ENET_INGRESS_PRI_TYPE_RR
Definition: enet_mod_hostport.h:243
@ ENET_HOSTPORT_IOCTL_DISABLE_INGRESS_TRAFFIC_SHAPING
Disable ingress traffic shaping configuration.
Definition: enet_mod_hostport.h:186
@ ENET_HOSTPORT_IOCTL_GET_VERSION
Get the hardware version of the host port module.
Definition: enet_mod_hostport.h:87
@ ENET_HOSTPORT_IOCTL_DISABLE
Disable host port.
Definition: enet_mod_hostport.h:114