|
AM261x MCU+ SDK
26.00.00
|
|
Go to the documentation of this file.
59 #include <drivers/hw_include/csl_types.h>
60 #include <drivers/hw_include/cslr_ospi.h>
62 #include <drivers/ospi/v0/cslr_ospi.h>
81 #define OSPI_TRANSFER_COMPLETED (0U)
82 #define OSPI_TRANSFER_STARTED (1U)
83 #define OSPI_TRANSFER_CANCELLED (2U)
84 #define OSPI_TRANSFER_FAILED (3U)
85 #define OSPI_TRANSFER_CSN_DEASSERT (4U)
86 #define OSPI_TRANSFER_TIMEOUT (5U)
108 #define OSPI_TRANSFER_MODE_BLOCKING (0U)
113 #define OSPI_TRANSFER_MODE_CALLBACK (1U)
118 #define OSPI_TRANSFER_MODE_POLLING (2U)
135 #define OSPI_FF_POL0_PHA0 (0U)
136 #define OSPI_FF_POL0_PHA1 (CSL_OSPI_FLASH_CFG_CONFIG_REG_SEL_CLK_PHASE_FLD_MASK | 0U)
137 #define OSPI_FF_POL1_PHA0 (0U | CSL_OSPI_FLASH_CFG_CONFIG_REG_SEL_CLK_POL_FLD_MASK)
138 #define OSPI_FF_POL1_PHA1 (CSL_OSPI_FLASH_CFG_CONFIG_REG_SEL_CLK_PHASE_FLD_MASK | \
139 CSL_OSPI_FLASH_CFG_CONFIG_REG_SEL_CLK_POL_FLD_MASK)
150 #define OSPI_CMD_INVALID_OPCODE (0xFFU)
151 #define OSPI_CMD_INVALID_DUMMY (0xFFU)
152 #define OSPI_CMD_INVALID_ADDR (0xFFFFFFFFU)
163 #define OSPI_CMD_EXT_TYPE_REPEAT (0x00U)
164 #define OSPI_CMD_EXT_TYPE_INVERSE (0x01U)
165 #define OSPI_CMD_EXT_TYPE_NONE (0x02U)
176 #define OSPI_NOR_PROTOCOL(cmd, addr, data, dtr) (uint32_t)(((uint32_t)(dtr) << 24) | \
177 ((uint32_t)(cmd) << 16) | \
178 ((uint32_t)(addr) << 8) | \
179 ((uint32_t)(data) << 0))
180 #define OSPI_NOR_PROTOCOL_INVALID (uint32_t)(0xFFFFFFFF)
182 #define OSPI_PROTO_1S_1S_1S (0x0001)
183 #define OSPI_PROTO_1S_1S_2S (0x0002)
184 #define OSPI_PROTO_1S_1S_4S (0x0003)
185 #define OSPI_PROTO_1S_1S_8S (0x0004)
186 #define OSPI_PROTO_1S_8S_8S (0x000A)
187 #define OSPI_PROTO_4S_4S_4S (0x0005)
188 #define OSPI_PROTO_4S_4D_4D (0x0006)
189 #define OSPI_PROTO_8S_8S_8S (0x0007)
190 #define OSPI_PROTO_8D_8D_8D (0x0008)
191 #define OSPI_PROTO_CUSTOM (0x0009)
193 #define OSPI_NAND_PROTOCOL(cmd, addr, data, dtr) (uint32_t)(((uint32_t)(dtr) << 24) | \
194 ((uint32_t)(cmd) << 16) | \
195 ((uint32_t)(addr) << 8) | \
196 ((uint32_t)(data) << 0))
197 #define OSPI_NAND_PROTOCOL_INVALID (uint32_t)(0xFFFFFFFF)
208 #define OSPI_CS0 (0U)
209 #define OSPI_CS1 (1U)
210 #define OSPI_CS2 (2U)
211 #define OSPI_CS3 (3U)
214 #define OSPI_CHIP_SELECT(x) ((~((1U) << (x))) & 0xFU)
217 #define OSPI_RESETPIN_DQ3 (0U)
218 #define OSPI_RESETPIN_DEDICATED (1U)
229 #define CSL_OSPI_BAUD_RATE_DIVISOR(x) (((x) - 2U) >> 1U)
230 #define MAX_BAUDRATE_DIVIDER (32U)
231 #define CSL_OSPI_BAUD_RATE_DIVISOR_DEFAULT (CSL_OSPI_BAUD_RATE_DIVISOR(MAX_BAUDRATE_DIVIDER))
241 #define OSPI_DECODER_SELECT4 ((uint32_t) 0U)
242 #define OSPI_DECODER_SELECT16 ((uint32_t) 1U)
253 #define OSPI_STATE_RESET ((uint32_t) 0U)
256 #define OSPI_STATE_IDLE ((uint32_t) 1U)
259 #define OSPI_STATE_BUSY ((uint32_t) 2U)
262 #define OSPI_STATE_ERROR ((uint32_t) 3U)
272 #define OSPI_SYSTEM_SUCCESS ((int32_t )0)
276 #define OSPI_SYSTEM_FAILURE ((int32_t)-1)
280 #define OSPI_TIMEOUT ((int32_t)-2)
284 #define OSPI_LLD_INVALID_PARAM ((int32_t)-3)
288 #define OSPI_BUSY ((int32_t)-4)
292 #define OSPI_INVALID_STATE ((int32_t)-5)
303 #define OSPI_NO_WAIT ((uint32_t)0)
307 #define OSPI_WAIT_FOREVER ((uint32_t)-1)
317 #define OSPI_TRANS_IDLE ((uint32_t)0)
321 #define OSPI_TRANS_READ ((uint32_t)1)
325 #define OSPI_TRANS_WRITE ((uint32_t)2)
347 #define OSPI_FLASH_CFG_PHY_MASTER_CONTROL_REG_PHY_MASTER_MODE (0U)
348 #define OSPI_FLASH_CFG_PHY_MASTER_CONTROL_REG_PHY_BYPASS_MODE (1U)
361 #define OSPI_PHY_DLL_FULL_CYCLE_LOCK ((uint16_t) 0U)
362 #define OSPI_PHY_DLL_HALF_CYCLE_LOCK ((uint16_t) 1U)
373 #define OSPI_FLASH_ATTACK_VECTOR_SIZE (128U)
605 uint32_t devDelays[4];
int32_t OSPI_lld_disableDacMode(OSPILLD_Handle handle)
This function disables the Direct Access Mode.
int32_t OSPI_dmaOpen(OSPILLD_Handle hOspi)
API to open an OSPI DMA channel.
void OSPI_lld_setNumAddrBytes(OSPILLD_Handle handle, uint32_t numAddrBytes)
This function set the number of bytes used to send address while reading or writing to flash memory.
uint32_t writeTimeout
Definition: ospi_lld.h:470
int32_t OSPI_lld_disablePhyPipeline(OSPILLD_Handle handle)
This function disables the PHY Pipeline.
uint32_t regionSize
Definition: ospi_lld.h:507
uint32_t moduleId
Definition: ospi_lld.h:581
void * args
Definition: hsmclient_msg.h:4
int32_t OSPI_lld_enablePhyPipeline(OSPILLD_Handle handle)
This function enables the PHY Pipeline.
uint16_t rxDataLen
Definition: ospi_lld.h:489
int32_t OSPI_lld_norFlashReadId(OSPILLD_Handle handle, uint32_t *manufacturerId, uint32_t *deviceId)
This function tries to read the JEDEC ID from the NOR flash connected to the OSPI peripheral.
int32_t txDllLowWindowEnd
Definition: ospi_lld.h:541
uint32_t status
Definition: ospi_lld.h:443
void OSPI_lld_setCmdExtType(OSPILLD_Handle handle, uint32_t cmdExtType)
This function sets the type of command extension used in dual byte opcode mode.
uint32_t OSPI_lld_isIntrEnable(OSPILLD_Handle handle)
This function checks if interrupts are enabled.
uint32_t(* OSPI_Clock_usecToTicks)(uint64_t usecs)
The definition of a micro seconds to ticks function used by the QSPI driver to get ticks from microse...
Definition: ospi_lld.h:398
struct OSPILLD_InitObject * OSPILLD_InitHandle
OSPI LLD DMA header file.
uint32_t phyEnableSuccess
Definition: ospi_lld.h:669
int32_t OSPI_lld_norFlashInit1s1s1s(OSPILLD_Handle handle)
This function initializes the NOR flash to work in 1-1-1 mode.
uint8_t numAddrBytes
Definition: ospi_lld.h:483
int32_t txDllLowWindowStart
Definition: ospi_lld.h:540
OSPI Instance Read Command Structure.
Definition: ospi_lld.h:477
int32_t OSPI_lld_configResetPin(OSPILLD_Handle handle, uint32_t config)
This function configures reset functionality.
uint32_t intrNum
Definition: ospi_lld.h:591
OSPI_PhyWindowParams tuningWindowParams
Definition: ospi_lld.h:571
OSPI Instance Write Command Structure.
Definition: ospi_lld.h:458
int32_t OSPI_lld_deInitDma(OSPILLD_Handle hOspi)
Function to close a OSPI peripheral specified by the OSPI handle in DMA mode.
void OSPI_lld_isr(void *args)
QSPI ISR for Read and Write Functionality.
uint32_t transferTimeout
Definition: ospi_lld.h:449
OSPI_Transaction * currTrans
Definition: ospi_lld.h:672
Data structure used with OSPI_Transfers - OSPI_lld_readDirect, OSPI_lld_writeDirect,...
Definition: ospi_lld.h:436
uint32_t transferMode
Definition: ospi_lld.h:644
uint32_t cmdDummyCycles
Definition: ospi_lld.h:655
uint32_t inputClkFreq
Definition: ospi_lld.h:585
uint32_t cmdAddr
Definition: ospi_lld.h:461
uint32_t OSPI_lld_isPhyEnable(OSPILLD_Handle handle)
This function checks if the OSPI PHY controller is enabled.
OSPI_lld_InterruptCallback interruptCallback
Definition: ospi_lld.h:695
int32_t OSPI_lld_norFlashWrite(OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
This function writes data to the flash at a specified offset.
void OSPI_lld_norFlashSetCmds(uint8_t rdCmd, uint8_t wrCmd, uint8_t eraseCmd)
This function sets up internal bookkeeping variables for read, write and erase commands....
int32_t OSPI_lld_readCmd(OSPILLD_Handle handle, OSPI_ReadCmdParams *rdParams)
Function to send specific commands and receive related data from flash.
int32_t OSPI_dmaCopy(OSPILLD_Handle handle, void *dst, void *src, uint32_t length, uint32_t timeout)
API to do a DMA Copy using appropriate DMA Channel opened.
OSPILLD_InitHandle hOspiInit
Definition: ospi_lld.h:678
OSPI PHY Configuration.
Definition: ospi_lld.h:567
void(* OSPI_lld_dma_readCompleteCallback)(void *args)
The definition of a dma read completion callback function used by the QSPI driver.
Definition: ospi_lld.h:423
OSPI_PhyConfiguration phyConfiguration
Definition: ospi_lld.h:625
int32_t rxLowSearchEnd
Definition: ospi_lld.h:545
uint32_t numAddrBytes
Definition: ospi_lld.h:661
int32_t OSPI_dmaClose(OSPILLD_Handle handle)
API to close an OSPI DMA channel.
int32_t rxHighSearchStart
Definition: ospi_lld.h:546
void OSPI_lld_setCmdDummyCycles(OSPILLD_Handle handle, uint32_t cmdDummyCycles)
This function sets appropriate dummy cycles to be used while sending STIG commands to flash.
uint32_t cmdAddr
Definition: ospi_lld.h:480
void OSPI_lld_Transaction_init(OSPI_Transaction *trans)
Function to initialize the OSPI_Transaction structure.
OSPI_Clock_usecToTicks Clock_usecToTicks
Definition: ospi_lld.h:691
int32_t OSPI_lld_init(OSPILLD_Handle hOspi)
This function opens a given OSPI peripheral.
uint32_t count
Definition: ospi_lld.h:437
uint32_t cmdExtType
Definition: ospi_lld.h:666
int32_t OSPI_lld_phyTuneDDR(OSPILLD_Handle handle, uint32_t flashOffset)
This function tunes the OSPI PHY for DDR mode to set optimal PHY parameters.
int32_t OSPI_lld_initDma(OSPILLD_Handle hOspi)
This function opens a given OSPI peripheral in DMA mode.
uint32_t OSPI_lld_isDacEnable(OSPILLD_Handle handle)
This function checks if the Direct Access Controller is enabled.
int32_t OSPI_lld_writeCmd(OSPILLD_Handle handle, OSPI_WriteCmdParams *wrParams)
Function to send specific commands and related data to flash.
uint32_t dmaEnable
Definition: ospi_lld.h:597
uint32_t dllLockMode
Definition: ospi_lld.h:570
OSPI Parameters.
Definition: ospi_lld.h:523
uint32_t OSPI_lld_isValidateOtpEnable(OSPILLD_Handle hOspi)
Checks if OTP validation is enabled for the OSPI controller.
uint32_t dacEnable
Definition: ospi_lld.h:601
int32_t txDLLSearchOffset
Definition: ospi_lld.h:552
int32_t txHighSearchStart
Definition: ospi_lld.h:550
int32_t OSPI_lld_writeIndirect(OSPILLD_Handle handle, OSPI_Transaction *trans)
Function to perform indirect writes to the flash using INDAC controller.
uint32_t(* OSPI_Clock_getTicks)(void)
The definition of a get System Tick function used by the QSPI driver to keep track of time.
Definition: ospi_lld.h:387
int32_t txDllHighWindowStart
Definition: ospi_lld.h:542
uint32_t txDataLen
Definition: ospi_lld.h:468
void * txDataBuf
Definition: ospi_lld.h:466
uint32_t validateOtp
Definition: ospi_lld.h:613
int32_t OSPI_lld_phyTuneGrapher(OSPILLD_Handle handle, uint32_t flashOffset, uint8_t arrays[5][128][128])
This function takes a 4x128x128 array and fills it with TX RX DLL data for graphing purpose.
uint32_t OSPI_lld_getFlashDataBaseAddr(OSPILLD_Handle handle)
This function gets the SOC mapped data base address of the flash.
void OSPI_lld_setProtocol(OSPILLD_Handle handle, uint32_t protocol)
This function sets the number of transfer lines in the OSPI driver to set the requested protocol.
int32_t OSPI_lld_writeDirect(OSPILLD_Handle handle, OSPI_Transaction *trans)
Function to perform direct writes to the flash using DAC controller.
int32_t OSPI_lld_enableDDR(OSPILLD_Handle handle)
This function enables the Dual Data Rate (DDR)
void OSPI_lld_setXferOpCodes(OSPILLD_Handle handle, uint8_t readCmd, uint8_t pageProgCmd)
This function sets the opcodes for reading and page programming the flash.
void OSPI_lld_clearDualOpCodeMode(OSPILLD_Handle handle)
This function sets OSPI controller to not use dual byte opcodes.
int32_t rxHighSearchEnd
Definition: ospi_lld.h:547
void OSPI_lld_readCompleteCallback(void *args)
QSPI Read complete callback for DMA mode.
int32_t OSPI_lld_enableDdrRdCmds(OSPILLD_Handle handle)
This function sets DDR bit in INSTR_RD register for RD commands.
uint32_t rdDataCapDelay
Definition: ospi_lld.h:657
int32_t txDllHighWindowEnd
Definition: ospi_lld.h:543
OSPI driver object.
Definition: ospi_lld.h:633
int32_t OSPI_lld_norFlashErase(OSPILLD_Handle handle, uint32_t address)
This function erases 1 block of data starting from a provided address.
uint32_t protocol
Definition: ospi_lld.h:646
int32_t OSPI_lld_setFrequency(OSPILLD_Handle hOspi, uint64_t inputClkFreq)
Sets the operating frequency for the OSPI peripheral.
int32_t OSPI_lld_readIndirect(OSPILLD_Handle handle, OSPI_Transaction *trans)
Function to perform indirect reads from the flash using INDAC controller.
OSPI PHY Tuning Window Parameters.
Definition: ospi_lld.h:539
void * rxDataBuf
Definition: ospi_lld.h:487
uint32_t phyEnable
Definition: ospi_lld.h:599
uint8_t cmd
Definition: ospi_lld.h:459
int32_t rxLowSearchStart
Definition: ospi_lld.h:544
OSPI_DmaHandle ospiDmaHandle
Definition: ospi_lld.h:621
int32_t OSPI_lld_configBaudrate(OSPILLD_Handle handle, uint32_t baud)
Configures baud divider.
uint32_t OSPI_lld_getInputClk(OSPILLD_Handle handle)
This function returns the input clk frequency OSPI was programmed at.
int32_t OSPI_lld_enablePhy(OSPILLD_Handle handle)
This function enables the PHY.
OSPI_Clock_getTicks Clock_getTicks
Definition: ospi_lld.h:689
int32_t OSPI_lld_disableDdrRdCmds(OSPILLD_Handle hOspi)
This function resets DDR bit in INSTR_RD register for RD commands.
int32_t ospiDmaChIndex
Definition: ospi_lld.h:524
int32_t OSPI_lld_enableSDR(OSPILLD_Handle handle)
This function enables the Single Data Rate (SDR)
int32_t OSPI_lld_setDelays(OSPILLD_Handle hOspi, uint32_t inputClkFreq)
Sets timing delays for the OSPI interface based on input clock frequency.
void * buf
Definition: ospi_lld.h:439
int32_t OSPI_lld_phyReadAttackVector(OSPILLD_Handle handle, uint32_t offset)
This function checks if the attack vector, or the data used for tuning the PHY is present at an offse...
uint32_t chipSelect
Definition: ospi_lld.h:607
const OSPI_Params * openParams
Definition: ospi_lld.h:643
int32_t OSPI_lld_phyValidateTuningPoint(OSPILLD_Handle hOspi, uint32_t flashOffset)
Validates a tuning point for the OSPI physical interface.
const OSPI_AddrRegion * dmaRestrictedRegions
Definition: ospi_lld.h:615
uint32_t state
Definition: ospi_lld.h:684
uint32_t rdDelayMax
Definition: ospi_lld.h:555
OSPI Address Region.
Definition: ospi_lld.h:504
int32_t txHighSearchEnd
Definition: ospi_lld.h:551
uint32_t decChipSelect
Definition: ospi_lld.h:609
void OSPI_lld_setWriteDummyCycles(OSPILLD_Handle handle, uint32_t dummyCycles)
This function sets appropriate dummy cycles for flash write.
int32_t OSPI_lld_set1sProtocol(OSPILLD_Handle hOspi)
Resets the OSPI controller to operate in 1S-1S-1S mode.
int32_t OSPI_lld_disablePhy(OSPILLD_Handle handle)
This function disables the PHY.
int32_t OSPI_lld_norFlashReadIndirect(OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
This function reads data from the flash from a specified offset in INDAC mode.
int32_t txLowSearchStart
Definition: ospi_lld.h:548
uint32_t baseAddr
Definition: ospi_lld.h:637
uint32_t OSPI_lld_getPhyEnableSuccess(OSPILLD_Handle handle)
This function fetches the phyEnableSuccess field in OSPILLD_Object.
uint8_t numAddrBytes
Definition: ospi_lld.h:464
uint32_t rdDummyCycles
Definition: ospi_lld.h:653
OSPI_lld_dma_readCompleteCallback readCompleteCallback
Definition: ospi_lld.h:697
void OSPI_lld_setReadDummyCycles(OSPILLD_Handle handle, uint32_t dummyCycles)
This function sets appropriate dummy cycles for flash read.
int32_t OSPI_lld_norFlashRead(OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
This function reads data from the flash from a specified offset in DAC mode.
int32_t OSPI_lld_readBaudRateDivFromReg(OSPILLD_Handle handle, uint32_t *baudDiv)
Return value of baudrate that is programmed in IP register.
uint32_t phyControlMode
Definition: ospi_lld.h:569
void OSPI_lld_phyGetTuningData(uint32_t *tuningData, uint32_t *tuningDataSize)
This function returns the address to the attack vector buf required for tuning the PHY.
int32_t OSPI_lld_deInit(OSPILLD_Handle hOspi)
Function to close a OSPI peripheral specified by the OSPI handle.
uint32_t OSPI_lld_isDmaEnable(OSPILLD_Handle handle)
This function checks if DMA is enabled for reads.
uint32_t baudRateDiv
Definition: ospi_lld.h:611
int32_t OSPI_lld_getBaudRateDivFromObj(OSPILLD_Handle handle, uint32_t *baudDiv)
Return value of baudrate that is saved in OSPI Object.
void * args
Definition: ospi_lld.h:686
void OSPI_lld_setDeviceSize(OSPILLD_Handle handle, uint32_t pageSize, uint32_t blkSize)
This function sets the block size and page size of the flash to the device size register in OSPI.
void OSPI_lld_setModeBits(OSPILLD_Handle handle, uint32_t modeBits)
This function sets mode bits in the mode bit field of OSPI config register.
int32_t txLowSearchEnd
Definition: ospi_lld.h:549
void OSPI_lld_readCmdParams_init(OSPI_ReadCmdParams *rdParams)
Function to initialize the OSPI_ReadCmdParams structure.
uint8_t dummyBits
Definition: ospi_lld.h:485
void(* OSPI_Clock_usec)(uint32_t usecs)
Sleep for user specified usecs.
Definition: ospi_lld.h:406
OSPI_Transaction trans
Definition: ospi_lld.h:675
int32_t OSPI_lld_enableDacMode(OSPILLD_Handle handle)
This function enables the Direct Access Mode.
uint32_t addrOffset
Definition: ospi_lld.h:441
uint32_t state
Definition: ospi_lld.h:451
uint32_t OSPI_lld_getProtocol(OSPILLD_Handle handle)
This function returns the current protocol for which the transfer lines in OSPI driver is configured ...
uint32_t phyRdDataCapDelay
Definition: ospi_lld.h:659
uint32_t regionStartAddr
Definition: ospi_lld.h:505
void OSPI_lld_enableModeBitsCmd(OSPILLD_Handle handle)
This function enables mode bits transmission while sending CMDs.
uint32_t dataLen
Definition: ospi_lld.h:445
uint32_t frmFmt
Definition: ospi_lld.h:603
uint32_t rdDelayMin
Definition: ospi_lld.h:554
uint8_t intrPriority
Definition: ospi_lld.h:595
void OSPI_lld_setPhyEnableSuccess(OSPILLD_Handle handle, uint32_t success)
This function sets the phyEnableSuccess field in OSPILLD_Object. Has to be called from flash driver.
OSPI driver initialization object.
Definition: ospi_lld.h:578
int32_t OSPI_lld_readDirectDma(OSPILLD_Handle handle, OSPI_Transaction *trans)
Function to perform direct reads from the flash using DAC controller in DMA mode.
uint32_t clkId
Definition: ospi_lld.h:583
struct OSPILLD_Object * OSPILLD_Handle
uint32_t rxTxDLLSearchStep
Definition: ospi_lld.h:553
int32_t OSPI_isDmaInterruptEnabled(OSPILLD_Handle handle)
API to get the DMA Interrupt status.
void OSPI_lld_enableModeBitsRead(OSPILLD_Handle handle)
This function enables mode bits transmission while reading.
uint8_t cmd
Definition: ospi_lld.h:478
int32_t OSPI_lld_setResetPinStatus(OSPILLD_Handle hOspi, uint32_t pinStatus)
This function activates the RESET pin feature.
uint32_t dataBaseAddr
Definition: ospi_lld.h:579
int32_t OSPI_lld_setBaudRateDiv(OSPILLD_Handle hOspi, uint32_t baudRateDiv)
Sets the baud rate divider for OSPI communication.
void(* OSPI_lld_InterruptCallback)(void *args)
The definition of a interrupt completion callback function used by the QSPI driver.
Definition: ospi_lld.h:415
int32_t OSPI_lld_readDirect(OSPILLD_Handle handle, OSPI_Transaction *trans)
Function to perform direct reads from the flash using DAC controller.
int32_t OSPI_lld_setRdDataCaptureDelay(OSPILLD_Handle handle, uint32_t rdDataCapDelay)
This function sets read data capture cycles in the OSPI controller.
uint32_t phaseDelayElement
Definition: ospi_lld.h:568
int32_t OSPI_lld_norFlashReadSfdp(OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
This function reads SFDP table from the flash from a specified offset.
OSPI_Clock_usec Clock_usleep
Definition: ospi_lld.h:693
uint32_t readTimeout
Definition: ospi_lld.h:491
void OSPI_lld_setDualOpCodeMode(OSPILLD_Handle handle)
This function sets OSPI controller to use dual byte opcodes.
uint32_t transferOffset
Definition: ospi_lld.h:447
uint32_t intrEnable
Definition: ospi_lld.h:593
int32_t OSPI_lld_phyTuneSDR(OSPILLD_Handle handle, uint32_t flashOffset)
This function tunes the OSPI PHY for SDR mode to set optimal PHY parameters.
void OSPI_lld_writeCmdParams_init(OSPI_WriteCmdParams *wrParams)
Function to initialize the OSPI_WriteCmdParams structure.
OSPI_DmaChConfig ospiDmaChConfig
Definition: ospi_lld.h:623