AM261x MCU+ SDK  26.00.00
Optiflash XIP Benchmark

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
Toolchain ti-arm-clang
Boards am261x-lp, am261x-som
Example folder examples/benchmarks/optiflash_benchmark/flash_xip

Introduction

This is the same application as Optiflash OCRAM Benchmark, however, target functions are kept in external flash. The effect of it is seen in the execution time.

Steps to Run the Example

Building the application

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

Running the application

Flash the application binary to the device, follow the steps mentioned here (see Flash a Hello World example).

Sample output

Starting OSPI Bootloader ...
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media Clock : 166.667 MHz
KPI_DATA: [BOOTLOADER_PROFILE] Boot Image Size : 6 KB
KPI_DATA: [BOOTLOADER_PROFILE] Cores present :
r5f0-0
KPI_DATA: [BOOTLOADER PROFILE] System_init : 497us
KPI_DATA: [BOOTLOADER PROFILE] Drivers_open : 96us
KPI_DATA: [BOOTLOADER PROFILE] LoadHsmRtFw : 1us
KPI_DATA: [BOOTLOADER PROFILE] Board_driversOpen : 4475us
KPI_DATA: [BOOTLOADER PROFILE] CPU load : 3601us
KPI_DATA: [BOOTLOADER PROFILE] SBL End : 8us
KPI_DATA: [BOOTLOADER_PROFILE] SBL Total Time Taken : 8679us
Image loading done, switching to application ...
OCMC benchmarking:: Board_init success
Filling up the buffers
master_task
master_task -- start sending
memcpy Exec Time I$ Miss I$ Acc INST ICM/sec INST/sec
0B 37013us 87162 1074736 2170362 2.9 72.4
100B 37628us 86327 1222952 2359690 2.8 77.4
200B 37858us 85448 1373268 2559775 2.8 83.5
400B 39842us 88104 1676065 2961887 2.7 91.8
700B 39757us 83118 2115272 3547263 2.6 110.2
1000B 43627us 85863 2580078 4162379 2.4 117.8
1500B 48945us 85644 3326582 5154946 2.2 130.1
2250B 57802us 88279 4470783 6669791 1.9 142.5
2500B 60022us 88601 4836857 7157313 1.8 147.3
4096B 72074us 86891 7237837 10352783 1.5 177.4
All tests have passed