AM261x MCU+ SDK  11.01.00
SDFM

The SDFM driver provides API to configure the SDFM module. Below are the high level features supported by the SDFM driver.

Features Supported

  • Ability to detect over-value, under-value and threshold-crossing conditions.
  • A programmable mode FIFO in data filter unit to reduce interrupt overhead.
  • FIFO can interrupt CPU after programmable number of data-ready events.
  • Ability to ignore data-ready events until the PWM synchronization signal is received.
  • PWMs can be used to generate a modulator clock for sigma-delta modulators.
  • Ability to use one filter channel clock to provide clock to other filter clock channels.

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.

Features NOT Supported

NA

Important Usage Guidelines

NA

Example Usage

Include the below file to access the APIs

#include <drivers/sdfm.h>

API

APIs for SDFM

sdfm.h