AM261x MCU+ SDK  10.02.00
Watchdog reset mode

Introduction

This example uses the WDT module in reset mode to trigger SOC warm reset. Servicing the WDT for few iterations before triggering the warm reset. It will reset the device once it reaches the expiry time set by user. Note that this example won't work in the debug mode as the user must not service the watchdog while in debug mode. For it to work, we can flash the image to get the expected result.

Supported Combinations

Supported Combinations

Steps to Run the Example

See Also

WATCHDOG

Sample Output

Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console.

Note
Console prints will be stopped once WDT triggers warm reset.

CCS Console:

[MAIN_Cortex_R5_0_0] Watchdog reset Mode Test Started ...
Servicing WDT for 3 iterations
Servicing WDT !!
Servicing WDT !!
Servicing WDT !!
Watchdog triggers warm reset in 3000 (ms)
All tests have passed!!
3
2
1

UART Console:

Watchdog reset Mode Test Started ...
Servicing WDT for 3 iterations
Servicing WDT !!
Servicing WDT !!
Servicing WDT !!
Watchdog triggers warm reset in 3000 (ms)
All tests have passed!!
3
2
1