AM261x MCU+ SDK  10.02.00
MCAN Loopback DMA

Introduction

This example demonstrates the CAN message transmission and reception in digital loop back mode with the following configuration.

  • CAN FD Message Format.
  • Message ID Type is Standard, Msg Id 0xC0.
  • MCAN is configured in DMA Mode.
  • Arbitration Bit Rate 1Mbps.
  • Data Bit Rate 5Mbps.
  • Buffer mode is used for Tx and RX to store message in message RAM.

Message is transmitted and received back internally using internal loopback mode. When the received message id and the data matches with the transmitted one, then the example is completed.

Supported Combinations

Steps to Run the Example

See Also

MCAN

Sample Output

Shown below is a sample output when the application is run,

[MCAN] Loopback DMA mode, application started ...
All tests have passed!!