|
AM243x MCU+ SDK
12.01.00
|
|
Go to the documentation of this file.
44 #include <drivers/hw_include/soc_config.h>
45 #include <board/flash/flash_config.h>
47 #define FLASH_INVALID_VALUE (0xFFFFFFFFU)
49 #define CONFIG_FLASH_TYPE_SERIAL ((uint32_t)0x1)
50 #define CONFIG_FLASH_TYPE_PARALLEL ((uint32_t)0x2)
55 #define CONFIG_FLASH_TYPE_SERIAL_NOR (0x00U)
56 #define CONFIG_FLASH_TYPE_SERIAL_NAND (0x01U)
57 #define CONFIG_FLASH_TYPE_PARALLEL_NOR (0x02U)
58 #define CONFIG_FLASH_TYPE_PARALLEL_NAND (0x03U)
59 #define CONFIG_FLASH_TYPE_INVALID (0xFFU)
112 typedef struct Flash_DevConfig_s {
199 uint8_t *buf, uint32_t len) ;
215 uint8_t *buf, uint32_t len) ;
315 typedef struct Flash_Params_s {
326 typedef struct Flash_Fxns_s
344 typedef struct Flash_Attrs_s {
365 typedef struct Flash_Config_s
377 #if defined (DRV_VERSION_FLASH_V0)
378 #include <board/flash/ospi/flash_nor_ospi.h>
381 #if defined (DRV_VERSION_FLASH_V1)
382 #include <board/flash/qspi/flash_nor_qspi.h>
385 #if defined (DRV_VERSION_FLASH_V2)
386 #include <board/flash/ospi/flash_nor_ospi.h>
387 #include <board/flash/ospi/flash_nand_ospi.h>
390 #if defined (DRV_VERSION_GPMC_V0)
391 #include <board/flash/gpmc/flash_nand_gpmc.h>
uint8_t cmdPageLoadCyc1
Definition: flash.h:124
uint32_t flashType
Definition: flash.h:346
uint8_t cmdPageProgCyc1
Definition: flash.h:129
void Flash_close(Flash_Handle handle)
Close flash driver.
uint8_t cmdReadStatus
Definition: flash.h:133
Flash_Attrs * attrs
Definition: flash.h:367
uint32_t flashSize
Definition: flash.h:351
uint8_t srEraseStatus
Definition: flash.h:105
Flash_OpenFxn openFxn
Definition: flash.h:328
FlashCfg_EraseConfig eraseCfg
Definition: flash.h:147
uint32_t srWipReg
Definition: flash.h:98
Flash_EnableDacModeFxn enableDacModeFxn
Definition: flash.h:335
uint32_t blockCount
Definition: flash.h:352
FlashCfg_ProtoEnConfig protocolCfg
Definition: flash.h:149
uint8_t cmdExtType
Definition: flash.h:114
void(* Flash_CloseFxn)(Flash_Config *config)
Driver implementation to close a specific flash driver.
Definition: flash.h:183
uint8_t cmdWren
Definition: flash.h:120
Flash_DevConfig * devConfig
Definition: flash.h:369
uint32_t driverInstance
Definition: flash.h:350
Flash driver configuration, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:366
int32_t Flash_offsetToBlkPage(Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page)
Utility API to convert offset in bytes to (Block Num, Page Num)
int32_t Flash_SectorPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t sector, uint32_t page)
Utility API to convert (Sector Num, Page Num) to offset in bytes.
uint8_t deviceBusyType
Definition: flash.h:139
uint8_t cmdRdsr
Definition: flash.h:121
uint32_t xspiWipReg
Definition: flash.h:142
uint8_t cmdPageProgCyc2
Definition: flash.h:130
Flash_EraseSectorFxn eraseSectorFxn
Definition: flash.h:333
uint32_t progStatusReg
Definition: flash.h:100
uint32_t flashBusyTimeout
Definition: flash.h:145
uint32_t sectorSize
Definition: flash.h:357
Flash_Fxns * fxns
Definition: flash.h:368
uint8_t srWriteProtectMask
Definition: flash.h:107
int32_t(* Flash_EnableDacModeFxn)(Flash_Config *config)
Driver implementation to enable DAC mode in Flash.
Definition: flash.h:265
uint32_t pageSize
Definition: flash.h:355
uint8_t addrByteSupport
Definition: flash.h:117
int32_t(* Flash_ReadFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to read from flash using a specific flash driver.
Definition: flash.h:198
int32_t Flash_blkPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t block, uint32_t page)
Utility API to convert (Block Num, Page Num) to offset in bytes.
Flash_quirksFxn bootQuirksFxn
Definition: flash.h:318
Flash device attributes, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:344
char * flashName
Definition: flash.h:347
uint8_t cmdRandomReadCyc2
Definition: flash.h:127
uint32_t xspiWipBit
Definition: flash.h:143
Flash_EraseFxn eraseFxn
Definition: flash.h:332
Flash_Handle Flash_getHandle(uint32_t instanceId)
Get handle to flash driver.
Driver implementation callbacks.
Definition: flash.h:327
int32_t(* Flash_EraseFxn)(Flash_Config *config, uint32_t blockNum)
Driver implementation to erase a block using a specific flash driver.
Definition: flash.h:228
uint8_t cmdWrsr
Definition: flash.h:95
uint32_t xspiEraseStatusReg
Definition: flash.h:103
uint32_t Flash_getPhyTuningOffset(Flash_Handle handle)
Return flash offset to write PHY tuning data.
uint8_t cmdPageLoad
Definition: flash.h:96
Flash_NandConfig * nandCfg
Definition: flash.h:150
uint8_t fourByteAddrEnSeq
Definition: flash.h:119
uint8_t srProgStatus
Definition: flash.h:104
uint32_t rwOffset
Definition: flash.h:372
uint8_t srWip
Definition: flash.h:122
uint8_t srWel
Definition: flash.h:137
struct Flash_Config_s Flash_Config
Forward declaration of Flash_Config.
Definition: flash.h:80
uint8_t resetType
Definition: flash.h:138
int32_t(* Flash_WriteFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to write to flash using specific flash driver.
Definition: flash.h:214
void * fallBackCfg
Definition: flash.h:373
Flash_CloseFxn closeFxn
Definition: flash.h:329
uint8_t cmdPageLoadCyc2
Definition: flash.h:125
int32_t Flash_phyTune(Flash_Handle handle)
Tunes the flash controller physical layer parameters.
uint32_t flashWriteTimeout
Definition: flash.h:144
void Flash_Params_init(Flash_Params *params)
Set default parameters in the Flash_Params structure.
int32_t(* Flash_ResetFxn)(Flash_Config *config)
Driver implementation to soft reset the flash.
Definition: flash.h:253
uint8_t srWriteProtectReg
Definition: flash.h:106
uint32_t pageCount
Definition: flash.h:354
Flash_DisableDacModeFxn disableDacModeFxn
Definition: flash.h:336
struct Flash_Params_s Flash_Params
Forward declaration of Flash_Params.
Definition: flash.h:85
uint32_t spareAreaSize
Definition: flash.h:358
uint8_t pageRowAddrCyc
Definition: flash.h:132
int32_t(* Flash_custProtocolFxn)(Flash_Config *config)
User implementation of a custom function to configure flash to operate in a specific protocol.
Definition: flash.h:298
uint32_t skipHwInit
Definition: flash.h:371
Flash_Attrs * Flash_getAttrs(uint32_t instanceId)
Return flash attributes.
uint8_t xspiWipRdCmd
Definition: flash.h:140
Flash device config. This will be part of the flash config, so has to be filled by sysconfig or other...
Definition: flash.h:93
int32_t(* Flash_DisableDacModeFxn)(Flash_Config *config)
Driver implementation to enable DAC mode in Flash.
Definition: flash.h:277
uint32_t blockSize
Definition: flash.h:353
FlashCfg_ReadIDConfig idCfg
Definition: flash.h:148
uint32_t eraseStatusReg
Definition: flash.h:102
int32_t Flash_offsetToSectorPage(Flash_Handle handle, uint32_t offset, uint32_t *sector, uint32_t *page)
Utility API to convert offset in bytes to (Sector Num, Page Num)
int32_t Flash_eraseSector(Flash_Handle handle, uint32_t sectorNum)
Erase a sector from flash.
uint32_t deviceId
Definition: flash.h:348
Flash_ReadFxn readFxn
Definition: flash.h:330
uint8_t enable4BAddr
Definition: flash.h:116
uint32_t phyTuningOffset
Definition: flash.h:359
int32_t Flash_reset(Flash_Handle handle)
Do a soft reset of the flash.
int32_t(* Flash_EraseSectorFxn)(Flash_Config *config, uint32_t sectorNum)
Driver implementation to erase a sector using a specific flash driver.
Definition: flash.h:241
Flash_WriteFxn writeFxn
Definition: flash.h:331
int32_t(* Flash_OpenFxn)(Flash_Config *config, Flash_Params *params)
Driver implementation to open a specific flash driver.
Definition: flash.h:171
uint8_t cmdReset
Definition: flash.h:134
Flash_Handle Flash_open(uint32_t instanceId, Flash_Params *params)
Open flash driver.
uint8_t cmdRandomInput
Definition: flash.h:128
uint8_t cmdRandomReadCyc1
Definition: flash.h:126
uint32_t xspiRdsrDummy
Definition: flash.h:99
uint8_t byteOrder
Definition: flash.h:115
uint32_t manufacturerId
Definition: flash.h:349
Flash_phyTuneFxn phyTuneFxn
Definition: flash.h:337
int32_t Flash_disableDacMode(Flash_Handle handle)
Disable DAC mode in flash.
Flash_ResetFxn resetFxn
Definition: flash.h:334
uint8_t pageColAddrCyc
Definition: flash.h:131
int32_t(* Flash_phyTuneFxn)(Flash_Config *confifg)
Driver implementation to perform phy tune flash.
Definition: flash.h:307
int32_t Flash_eraseBlk(Flash_Handle handle, uint32_t blockNum)
Erase a block from flash.
int32_t Flash_write(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Write to flash.
uint8_t cmdPageProg
Definition: flash.h:97
int32_t(* Flash_quirksFxn)(Flash_Config *config)
User implementation of a custom function to handle vendor specific quirks.
Definition: flash.h:289
uint32_t sectorCount
Definition: flash.h:356
Parameters passed during Flash_open()
Definition: flash.h:315
void * Flash_Handle
Handle to the FLash driver returned by Flash_opem()
Definition: flash.h:75
int32_t Flash_enableDacMode(Flash_Handle handle)
Enables DAC mode in flash.
Flash_quirksFxn quirksFxn
Definition: flash.h:317
Flash_custProtocolFxn custProtoFxn
Definition: flash.h:319
int32_t Flash_read(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Read data from flash.
uint32_t xspiProgStatusReg
Definition: flash.h:101
void * object
Definition: flash.h:370