|
AM243x MCU+ SDK
12.01.00
|
|
Go to the documentation of this file.
44 #include <drivers/soc.h>
45 #include <drivers/hw_include/csl_types.h>
46 #include <drivers/hw_include/cslr_soc.h>
47 #include <drivers/bootloader/soc/bootloader_soc.h>
48 #include <drivers/bootloader/bootloader_profile.h>
49 #include <drivers/hw_include/soc_config.h>
68 #define BOOTLOADER_INVALID_ID (0xDEADBABE)
73 #define BOOTLOADER_OPMODE_LOCKSTEP (0U)
74 #define BOOTLOADER_OPMODE_STANDALONE (1U)
79 #define BOOTLOADER_MEDIA_MEM (0xB0070001)
80 #define BOOTLOADER_MEDIA_FLASH (0xB0070002)
81 #define BOOTLOADER_MEDIA_EMMC (0xB0070003)
82 #define BOOTLOADER_MEDIA_SD (0xB0070004)
83 #define BOOTLOADER_MEDIA_BUFIO (0xB0070005)
84 #define BOOTLOADER_MEDIA_PCIE (0xB0070006)
85 #define BOOTLOADER_MEDIA_USB (0xB0070007)
86 #define BOOTLOADER_MEDIA_UART (0xB0070008)
91 #define BOOTLOADER_SCRATCH_MEM_ENABLE (1U)
96 #define LINUX_LOAD_ONLY_IMAGE_ID (21U)
106 typedef struct Bootloader_Params_s
214 typedef struct Bootloader_Fxns_s
228 typedef struct Bootloader_Config_s
247 #include <drivers/bootloader/bootloader_flash.h>
248 #include <drivers/bootloader/bootloader_mem.h>
249 #include <drivers/bootloader/bootloader_buf_io.h>
250 #if defined(SOC_AM64X) || defined(SOC_AM243X)
251 #include <drivers/bootloader/bootloader_uart.h>
257 typedef struct Bootloader_CpuInfo_s
269 typedef struct Bootloader_BootImageInfo_s
536 #if defined(SOC_AM64X)
573 #if defined(SOC_AM64X) || defined(SOC_AM243X)
#define CSL_CORE_ID_MAX
Definition: cslr_soc_defines.h:77
uint32_t coresPresentMap
Definition: bootloader.h:234
Bootloader_Fxns * fxns
Definition: bootloader.h:230
uint32_t disableAppImageAuth
Definition: bootloader.h:240
uint32_t Bootloader_isCorePresent(Bootloader_Handle handle, uint32_t cslCoreId)
API to check if a particular core's image is present in the multicore image.
uint32_t memArgsAppImageBaseAddr
Definition: bootloader.h:108
int32_t Bootloader_bootSelfCpu(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
API to boot self CPU.
void(* Bootloader_imgCloseFxn)(void *handle, void *args)
Driver implementation to close a specific bootloader driver - Memory, OSPI, UART, MMCSD etc.
Definition: bootloader.h:194
int32_t Bootloader_rprcImageParseEntryPoint(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
Parse entrypoint from RPRC.
uint32_t Bootloader_getBootMedia(Bootloader_Handle handle)
API to get the selected boot media in the bootloader instance.
Bootloader_imgOpenFxn imgOpenFxn
Definition: bootloader.h:216
void Bootloader_BootImageInfo_init(Bootloader_BootImageInfo *bootImageInfo)
Initialize BootImage info.
uint32_t isAppimageSigned
Definition: bootloader.h:239
uint32_t bufIoDeviceIndex
Definition: bootloader.h:117
void Bootloader_Params_init(Bootloader_Params *params)
Initialize Bootloader params.
uint32_t Bootloader_getMulticoreImageSize(Bootloader_Handle handle)
API to fetch the size of the multicore image.
uint32_t rprcOffset
Definition: bootloader.h:261
void * args
Definition: bootloader.h:231
Bootloader_imgSeekFxn imgSeekFxn
Definition: bootloader.h:219
int32_t Bootloader_runSelfCpuWithLinux(void)
API to boot self CPU with Linux.
int32_t Bootloader_parseAndLoadMultiCoreELF(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
API to parse and load MCELF image.
uint8_t * bufIoTempBuf
Definition: bootloader.h:111
int32_t Bootloader_parseMultiCoreAppImage(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
Parse Multicore Appimage.
Bootloader driver configuration, these are filled by SysCfg based on the boot media selected.
Definition: bootloader.h:229
int32_t(* Bootloader_imgCustomFxn)(void *args)
Driver implementation to enable a custom function for a specific bootloader driver - Memory,...
Definition: bootloader.h:206
uint32_t(* Bootloader_imgOffsetFxn)(void *args)
Driver implementation to get the current offset in the boot media.
Definition: bootloader.h:168
Bootloader_imgOffsetFxn imgOffsetFxn
Definition: bootloader.h:218
void Bootloader_close(Bootloader_Handle handle)
Close bootloader driver.
void * socCoreOpMode
Definition: bootloader.h:236
int32_t Bootloader_cpuSetAppEntryPoint(Bootloader_BootImageInfo *bootImageInfo, uint32_t bDualSelfR5F)
Set Application entry point for self CPU in the AM65x SOC from reset.
int32_t Bootloader_loadSelfCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo, uint32_t skipLoad)
API to load self CPU.
int32_t Bootloader_bootCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to boot a non-self CPU.
int32_t Bootloader_runCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to run a non-self CPU.
uint32_t bootImageSize
Definition: bootloader.h:233
uint32_t bufIoTempBufSize
Definition: bootloader.h:114
char * fileName
Definition: bootloader.h:120
uint32_t Bootloader_getMsgLen(uint8_t *x509_cert_ptr, uint32_t x509_cert_size)
API to get image length from a x509 certificate.
uint32_t clkHz
Definition: bootloader.h:260
uint32_t cpuId
Definition: bootloader.h:259
Data structure containing information related to a particular CPU, required for RPRC loading.
Definition: bootloader.h:258
int32_t(* Bootloader_imgOpenFxn)(void *args, Bootloader_Params *params)
Driver implementation to open a specific bootloader driver - Memory, OSPI, UART, MMCSD etc.
Definition: bootloader.h:142
Data structure containing information related all CPUs, this will be filled by Bootloader_parseMultiC...
Definition: bootloader.h:270
uint32_t bootMedia
Definition: bootloader.h:232
int32_t Bootloader_runSelfCpu(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
API to boot self CPU.
Bootloader_imgCustomFxn imgCustomFxn
Definition: bootloader.h:221
int32_t Bootloader_initCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to initialize a non-self CPU.
int32_t Bootloader_rprcImageLoad(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
Load application binaries into SOC memory.
void(* Bootloader_imgSeekFxn)(uint32_t location, void *args)
Driver implementation to read from boot media using a specific bootloader driver - Memory,...
Definition: bootloader.h:181
Bootloader_imgCloseFxn imgCloseFxn
Definition: bootloader.h:220
int32_t Bootloader_parseAndLoadLinuxAppImage(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
Parse and load linux Appimage, containing linux binaries(ATF, OPTEE, SPL)
Driver implementation callbacks.
Definition: bootloader.h:215
uint32_t Bootloader_getX509CertLen(uint8_t *x509_cert_ptr)
API to get the length of an x509 certificate.
uint32_t enableScratchMem
Definition: bootloader.h:243
int32_t(* Bootloader_imgReadFxn)(void *dstAddr, uint32_t length, void *args)
Driver implementation to read from boot media using a specific bootloader driver - Memory,...
Definition: bootloader.h:156
void * Bootloader_Handle
Handle to the Bootloader driver returned by Bootloader_open()
Definition: bootloader.h:101
void Bootloader_CpuInfo_init(Bootloader_CpuInfo *cpuInfo)
Initialize CPU info.
Parameters passed during Bootloader_open()
Definition: bootloader.h:107
Bootloader_Handle Bootloader_open(uint32_t instanceNum, Bootloader_Params *openParams)
Open bootloader driver.
int32_t Bootloader_loadCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to load a non-self CPU.
uint8_t * scratchMemPtr
Definition: bootloader.h:235
uintptr_t entryPoint
Definition: bootloader.h:262
uint32_t initICSSCores
Definition: bootloader.h:242
Bootloader_imgReadFxn imgReadFxn
Definition: bootloader.h:217