AM243x MCU+ SDK  12.01.00
HwiP.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2018-2023 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef HWIP_H
34 #define HWIP_H
35 
36 #ifdef __cplusplus
37 extern "C" {
38 #endif
39 
40 #include <stdint.h>
41 #include <kernel/dpl/SystemP.h>
42 
52 #if defined(__ARM_ARCH_7R__) || defined(__ARM7R__)
53 
54  /* compile flag to enable or disable save/restore of FPU context in FIQ */
55  // #define HWIP_FPU_CONTEXT_SAVE_RESTORE_ENABLE
56 
57  /* compile flag to enable or disable interrupt nesting */
58  #define HWIP_NESTED_INTERRUPTS_IRQ_ENABLE
59 
60  #if defined (OS_NORTOS)
61 
62  /* compile flag to enable or disable interrupt priority mask based critical sections */
63  // #define HWIP_USE_INTERRUPT_PRIORITY_BASED_CRITICAL_SECTIONS
64 
71  #if defined (HWIP_USE_INTERRUPT_PRIORITY_BASED_CRITICAL_SECTIONS)
72 
85  #define HWIP_CRITICAL_SECTION_INTERRUPT_PRIORITY_THRESHOLD (4U)
86 
95  #define HWIP_ENTER_CRITICAL_SECTION() HwiP_setVimIrqPriMaskAtomic(HWIP_CRITICAL_SECTION_INTERRUPT_PRIORITY_THRESHOLD)
96 
99  #define HWIP_EXIT_CRITICAL_SECTION(key) HwiP_restoreVimIrqPriMask(key)
100 
101  #endif /* HWIP_USE_INTERRUPT_PRIORITY_BASED_CRITICAL_SECTIONS */
102 
103  #endif /* OS_NORTOS */
104 
105 #endif /* __ARM_ARCH_7R__ */
106 
112 typedef void (*HwiP_FxnCallback)(void *args);
113 
114 
118 typedef struct HwiP_Config_
119 {
120  uint32_t intcBaseAddr;
122 } HwiP_Config;
123 
127 typedef struct HwiP_Params_ {
128 
129  uint32_t intNum;
131  void *args;
132  uint16_t eventId;
133  uint8_t priority;
134  uint8_t isFIQ;
135  uint8_t isPulse;
137 } HwiP_Params;
138 
142 typedef struct HwiP_Object_ {
143 
144  uint32_t intNum;
145 
146 } HwiP_Object;
147 
156 
165 int32_t HwiP_construct(HwiP_Object *obj, HwiP_Params *params);
166 
167 
176 int32_t HwiP_setArgs(HwiP_Object *obj, void *args);
177 
184 
190 void HwiP_enableInt(uint32_t intNum);
191 
202 uint32_t HwiP_disableInt(uint32_t intNum);
203 
213 void HwiP_restoreInt(uint32_t intNum, uint32_t oldIntState);
214 
220 void HwiP_clearInt(uint32_t intNum);
221 
222 
223 
229 void HwiP_post(uint32_t intNum);
230 
240 uintptr_t HwiP_disable(void);
241 
248 void HwiP_enable(void);
249 
258 void HwiP_restore(uintptr_t oldIntState);
259 
260 
277 uint32_t HwiP_inISR(void);
278 
289 void HwiP_init(void);
290 
299 int32_t HwiP_registerNmiHandler(HwiP_FxnCallback nmiHandler, void *args);
300 
307 
308 typedef struct {
309  volatile uint32_t index;
310  /* index bit*/
311  volatile uint32_t side_ext;
312  /* side extension*/
313  volatile uint32_t recoverable_error;
314  /* recoverable error*/
315  volatile uint32_t cacheway;
316  /* cacheway*/
317 }AIFSR;
318 
319 typedef struct {
320  volatile uint32_t status;
321  /* status */
322  volatile uint32_t sd;
323  /* SD bit */
324 }IFSR;
325 
326 typedef struct {
327  volatile uint32_t index;
328  /* index bit*/
329  volatile uint32_t side_ext;
330  /* side extension*/
331  volatile uint32_t recoverable_error;
332  /* recoverable error*/
333  volatile uint32_t cacheway;
334  /* cacheway*/
335 }ADFSR;
336 typedef struct {
337  volatile uint32_t status;
338  /* status */
339  volatile uint32_t sd;
340  /* SD bit */
341  volatile uint32_t rw;
342  /* read or write error */
343 }DFSR;
344 
345 
346 
347 
354 #ifdef __cplusplus
355 }
356 #endif
357 
358 #endif /* HWIP_H */
HwiP_Params::eventId
uint16_t eventId
Definition: HwiP.h:132
ADFSR
Definition: HwiP.h:326
DFSR
Definition: HwiP.h:336
IFSR::sd
volatile uint32_t sd
Definition: HwiP.h:322
HwiP_Object::intNum
uint32_t intNum
Definition: HwiP.h:144
HwiP_inISR
uint32_t HwiP_inISR(void)
Check if the caller of this function is inside a ISR or not.
AIFSR
Definition: HwiP.h:308
HwiP_destruct
void HwiP_destruct(HwiP_Object *obj)
Cleanup, delete, destruct a Hwi object.
SystemP.h
HwiP_disableInt
uint32_t HwiP_disableInt(uint32_t intNum)
Disable a specific interrupt.
DFSR::status
volatile uint32_t status
Definition: HwiP.h:337
IFSR
Definition: HwiP.h:319
HwiP_Params
Parameters passed during HwiP_construct.
Definition: HwiP.h:127
HwiP_post
void HwiP_post(uint32_t intNum)
Force trigger a specific interrupt.
HwiP_restoreInt
void HwiP_restoreInt(uint32_t intNum, uint32_t oldIntState)
Restore a specific interrupt.
HwiP_unregisterNmiHandler
int32_t HwiP_unregisterNmiHandler(void)
This API unregisters the current NMI handler.
HwiP_enable
void HwiP_enable(void)
Enable all interrupts.
HwiP_construct
int32_t HwiP_construct(HwiP_Object *obj, HwiP_Params *params)
Create a Hwi object.
HwiP_Params_init
void HwiP_Params_init(HwiP_Params *params)
Set default values to HwiP_Params.
HwiP_Config::intcBaseAddr
uint32_t intcBaseAddr
Definition: HwiP.h:120
IFSR::status
volatile uint32_t status
Definition: HwiP.h:320
AIFSR::recoverable_error
volatile uint32_t recoverable_error
Definition: HwiP.h:313
ADFSR::recoverable_error
volatile uint32_t recoverable_error
Definition: HwiP.h:331
AIFSR::index
volatile uint32_t index
Definition: HwiP.h:309
HwiP_enableInt
void HwiP_enableInt(uint32_t intNum)
Enable a specific interrupt.
HwiP_registerNmiHandler
int32_t HwiP_registerNmiHandler(HwiP_FxnCallback nmiHandler, void *args)
This API registers the NMI handler.
HwiP_Params::priority
uint8_t priority
Definition: HwiP.h:133
HwiP_Params::isPulse
uint8_t isPulse
Definition: HwiP.h:135
DFSR::sd
volatile uint32_t sd
Definition: HwiP.h:339
HwiP_Params::callback
HwiP_FxnCallback callback
Definition: HwiP.h:130
ADFSR::cacheway
volatile uint32_t cacheway
Definition: HwiP.h:333
HwiP_init
void HwiP_init(void)
Initialize Hwi module.
HwiP_Object
Opaque Hwi object used with the Hwi APIs.
Definition: HwiP.h:142
AIFSR::side_ext
volatile uint32_t side_ext
Definition: HwiP.h:311
HwiP_Params::isFIQ
uint8_t isFIQ
Definition: HwiP.h:134
HwiP_Params::args
void * args
Definition: HwiP.h:131
HwiP_disable
uintptr_t HwiP_disable(void)
Disable all interrupts.
HwiP_restore
void HwiP_restore(uintptr_t oldIntState)
Restores all interrupts to a given state.
ADFSR::index
volatile uint32_t index
Definition: HwiP.h:327
HwiP_clearInt
void HwiP_clearInt(uint32_t intNum)
Clear a pending specific interrupt.
AIFSR::cacheway
volatile uint32_t cacheway
Definition: HwiP.h:315
ADFSR::side_ext
volatile uint32_t side_ext
Definition: HwiP.h:329
HwiP_setArgs
int32_t HwiP_setArgs(HwiP_Object *obj, void *args)
Set argument to pass to the ISR.
HwiP_Params::intNum
uint32_t intNum
Definition: HwiP.h:129
DFSR::rw
volatile uint32_t rw
Definition: HwiP.h:341
HwiP_FxnCallback
void(* HwiP_FxnCallback)(void *args)
Callback that is called when a HW interrupt is received.
Definition: HwiP.h:112
HwiP_Config
HwiP config parameters, setup as part of SysConfig, not to be set by end-users directly.
Definition: HwiP.h:119