AM243x MCU+ SDK  12.01.00
Enet CLI Example

Introduction

This example demonstrates the usage of the Enet CLI commands

This example does the following:

  • Initializes and opens the ethernet drivers.
  • Initializes CLI App and enables built-in commands
  • Registers a few custom commands for various operations like sending and recieving packets, adding unicast address, configuring VLAN, etc.
  • It also registers commands to launch the gPTP stack and LwIP shell.
  • On running the application, it launches a command line interface on the UART terminal.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0_freertos
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp
Example folder source/networking/enet/core/examples/enet_cli_app

Packet pool configuration

To change packet pool configuration from syscfg, please refer to Ethernet Packet Pool Allocation Guidelines

Steps to Run the Example

Build the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

Sample Outputs

Once the application has started, using the help commands will give the following output:

Enabling clocks!
EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:1 From 4 To 2
Mdio_open: MDIO Manual_Mode enabled
EnetPhy_bindDriver: PHY 3: OUI:080028 Model:0f Ver:01 <-> 'dp83869' : OK
EnetPhy_bindDriver: PHY 15: OUI:080028 Model:0f Ver:01 <-> 'dp83869' : OK
PHY 3 is alive
PHY 15 is alive
Cpsw_internalIoctl_handler_ENET_IOCTL_REGISTER_DSTMAC_RX_FLOW: CPSW: Registered MAC address.ALE entry:2, Policer Entry
Cpsw_handleLinkUp: Port 1: Link up: 100-Mbps Full-Duplex
---------------------------------------
CLI for AM243x
Use 'help' to list all available commands
> help
help:
Lists all the registered commands
enet_addtxchn <tx_ch_num>:
Opens a Tx channel.
enet_addrxchn <rx_ch_num>:
Opens an Rx channel.
enet_sendraw <tx_ch_num> [-dm <dest_mac_addr>] [-sm <src_mac_addr>] [-v <vlan_id>] [-pcp <priority>] [-m <message>]:
Sends a raw ethernet packet.
enet_capture {start | stop} <rx_ch_num>:
Start/stop capturing incoming ethernet packets.
enet_capturedump <rx_ch_num>:
Returns the last 4 packets recieved at the specified channel.
quit:
Closes the CLI application.
enet_adducast <mac_addr> [-d]:
Adds a unicast ALE entry with the given MAC address.
Use the -d tag to make the MAC address as the default source address for sending packets.
enet_remucast <mac_addr>:
Removes unicast ALE entry with the given MAC address.
enet_addvlan <vlan_id> {<port1> ...}:
Configures the given ports to the specified VLAN id.
enet_remvlan <vlan_id>:
Removes VLAN config with specified ID.
enet_ptpd {start | stop} <dma_channel> [-p1 <priority_1>] [-p2 <priority_2>] [-s <sync_interval>]:
Start/stop gPTP stack.
enet_hostmacaddr:
Prints the host port MAC address.
lwip_shell {start | stop}:
Opens an LwIP shell.
enet_cfg {help|mqprio|tracelvl|classifier}:
Commands to modify ethernet configurations.
enet_dbg {help|cpswstats|dumpale|dumppolicer}:
Commands to print debug data.
phy {help|scan|status|dump|write|read}:
Commands to access ethernet PHYs.
utils {help|cpuload|readmem|writemem}:
Utility commands for SOC.
>

The commands enet_cfg, enet_dbg, phy and utils are the built-in commands. The rest of the commands are user defined.

Accessing the LwIP Shell

The LwIP shell can be launched by using the command lwip_shell start. Starting the LwIP shell will give the following output:

> lwip_shell start
Starting lwIP, local interface IP is dhcp-enabled
[LWIPIF_LWIP] NETIF INIT SUCCESS
Host MAC address-2 : 70:ff:76:1e:95:b7
[0]Enet IF UP Event. Local interface IP:0.0.0.0
[LWIPIF_LWIP] Enet has been started successfully
[0]Network Link UP Event
[0]Enet IF UP Event. Local interface IP:172.24.227.48
Shell Opened
>

DMA channel 2 is dedicated for the LwIP stack.

The LwIP shell can be accessed on any telnet terminal. The below steps have been tried with a Linux Ubuntu 20.04 host PC running bash shell

  1. Install 'telnet' package if not installed by using the below command:
    $ sudo apt install telnet
  2. Open a telnet connection using the command:
    $ telnet <ip_addr>
    Here the <ip_addr> is the IP address of the microcontroller.

After launching the telnet terminal and connecting to the microcontroller, using the help command in the host PC will give the following output:

Trying 172.24.227.48...
Connected to 172.24.227.48.
Escape character is '^]'.
lwIP simple interactive shell.
(c) Copyright 2001, Swedish Institute of Computer Science.
Written by Adam Dunkels.
For help, try the "help" command.
> help
Available commands:
open [IP address] [TCP port]: opens a TCP connection to the specified address.
lstn [TCP port]: sets up a server on the specified port.
acpt [connection #]: waits for an incoming connection request.
send [connection #] [message]: sends a message on a TCP connection.
udpc [local UDP port] [IP address] [remote port]: opens a UDP "connection".
udpl [local UDP port] [IP address] [remote port]: opens a UDP-Lite "connection".
udpn [local UDP port] [IP address] [remote port]: opens a UDP "connection" without checksums.
udpb [local port] [remote port]: opens a UDP broadcast "connection".
usnd [connection #] [message]: sends a message on a UDP connection.
recv [connection #]: receives data on a TCP or UDP connection.
clos [connection #]: closes a TCP or UDP connection.
stat: prints out lwIP statistics.
idxtoname [index]: outputs interface name from index.
nametoidx [name]: outputs interface index from name.
gethostnm [name]: outputs IP address of host.
quit: quits
>

These are the built-in commands provided by the LwIP shell.

See Also

Ethernet And Networking