AM243x MCU+ SDK  12.01.00
UDMA Chaining

Introduction

UDMA chaining sample application performs a chain of block copy transfer using channel global trigger. Channel 0 completion triggers Channel 1 transfer: CH0 -> CH1. The application opens and configures two BCDMA channel using SysConfig.

The first channel doesn't user a global trigger and each channel triggers the next channel's global trigger through the channel's TR event register.

A channel's source buffer is previous channel's destination buffer. This ensures that chaining trigger works in a synchronized manner when the memory compare matches.

The transfer completion is based on last channel's DMA completion event. Once the transfer it completes, it does cache operation for data coherency and compares the source and destination buffers for any data mismatch.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp
Example folder examples/drivers/udma/udma_chaining

Steps to Run the Example

See Also

UDMA

Sample Output

Shown below is a sample output when the application is run,

[UDMA] Chaining application started ...
All tests have passed!!