AM243x MCU+ SDK  12.01.00
SBL UART

Introduction

This bootloader does SOC initializations and attempts to boot a multicore application image received over UART via XMODEM. The image file is sent using a python script (See UART Bootloader Python Script). Once image is received, the SBL parses it. Each core is then initialized, application image is loaded, entry points are set and the core is released from reset. For more on bootflow/bootloaders, please refer Understanding the bootflow and bootloaders

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp
Example folder examples/drivers/boot/sbl_uart

Steps to Run the Example

Since this is a bootloader and is used as a SOC initialization binary, the example will be run every time you boot an application using this example. It is generally run from a boot media (OSPI Flash, SD Card or over UART) unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Note
From release 12.00.00 onwards, when configuring the SBL UART bootloader in syscfg, ensure that the boot media is set to UART and not SOC_Memory. This configuration is required for proper UART bootloader operation.

See Also

BOOTLOADER

Sample Output

Since this SBL receives the application image over UART using XMODEM protocol, it doesn't print anything to the console so as not to corrupt the XMODEM transport.