|
AM243x MCU+ SDK
12.01.00
|
|
The General-Purpose Timer driver provides APIs to configure the available timer modules in multiple modes.
Features Supported
- Interrupts generated on overflow, compare, and capture
- Free-running 32-bit upward counter
- Compare and capture modes
- Autoreload mode
- Start/stop mode
- Programmable divider clock source (2 exponent n, where n = [0-8])
- Dedicated input trigger for capture mode and dedicated output trigger/PWM signal
- On-the-fly read/write register
SysConfig Features
- Note
- It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
- Set mode of operation of the timer
- Enable/Disable and Set counter Prescaler
- Enable/Disable Auto reload Mode and set Auto reload Value
- Enable Interrupt and Assign User Callback
- Set Compare value when Compare Match mode is set
- Set Counter mode and Capture event when Timer configured to capture input
- Set PWM output Trigger mode and Compare Value in PWM mode
- Set Default Output Polarity in PWM mode
- Set Output Pin Modulation in PWM mode
Features NOT Supported
- Atomic 64-bit timer value read of cascaded timers
- Smart-idle with wake-up mode
Example Usage
Include the below file to access the APIs
Instance Open Example
gGpTimerObjects[CONFIG_GPTIMER0].overflowCallbackFunction = NULL,
gGpTimerObjects[CONFIG_GPTIMER0].compareMatchCallbackFunction = NULL,
gGpTimerObjects[CONFIG_GPTIMER0].captureCallbackFunction = NULL,
Instance Close Example
GPTIMER configuration in Free Running Mode without interrupt
void gptimer_free_run_no_interrupt(void)
{
}
GPTIMER configuration in Free Running Mode with interrupt
{
}
void gptimer_free_run_interrupt(void)
{
}
GPTIMER configuration in Output Compare Mode
{
}
void gptimer_output_compare_interrupt(void)
{
compareConfig.cntCompareValComp = (0x017D7840U);
}
GPTIMER configuration in Input Capture Mode
{
}
void gptimer_input_capture_interrupt(void)
{
}
GPTIMER configuration in PWM Generation Mode
void gptimer_pwm_gen(void)
{
pwmConfig.cntCompareValPWM = 4294954795,
}
API
APIs for GPTIMER
#define GPTIMER_INPUT_CAPTURE_MODE_SECOND
Capture Two Events.
Definition: gp_timer/v0/gp_timer.h:93
void GPTIMER_setCallbackFxn(GPTIMER_Handle handle, GPTIMER_OverflowCallbackFxn overflowCbFxn, GPTIMER_CompareMatchCallbackFxn compMatchCbFxn, GPTIMER_CaptureCallbackFxn captureCbFxn)
Update Callback Functions.
struct GPTIMER_Config_s * GPTIMER_Handle
A handle that is returned from a GPTIMER_open() call.
Definition: gp_timer/v0/gp_timer.h:178
#define GPTIMER_PWM_OUT_PIN_DEFAULT_0
Pin Default value 0.
Definition: gp_timer/v0/gp_timer.h:136
#define GPTIMER_PWM_OUT_OVERFLOW_MATCH_TRIGGER
PWM uses overflow and compare match as a trigger.
Definition: gp_timer/v0/gp_timer.h:125
void GPTIMER_start(GPTIMER_Handle handle)
Start the Timer.
#define SystemP_WAIT_FOREVER
Value to use when needing a timeout of infinity or wait forver until resource is available.
Definition: SystemP.h:83
#define GPTIMER_MODE_CONFIG_FREE_RUN
Free Running Mode.
Definition: gp_timer/v0/gp_timer.h:74
int32_t GPTIMER_setOpCompareMode(GPTIMER_Handle handle, GPTIMER_Compare_Config *config)
Change Timer Configuration to output compare mode.
bool oneShotMode
Definition: gp_timer/v0/gp_timer.h:260
int32_t GPTIMER_setIpCaptureMode(GPTIMER_Handle handle, GPTIMER_Capture_Config *config)
Change Timer Configuration to Input capture mode.
int32_t GPTIMER_setPWMGenMode(GPTIMER_Handle handle, GPTIMER_PWM_Config *config)
Change Timer Configuration to PWM generation mode.
uint32_t overflowMaskCount
Definition: gp_timer/v0/gp_timer.h:264
void SemaphoreP_destruct(SemaphoreP_Object *obj)
Cleanup, delete, destruct a semaphore object.
bool enablePrescaler
Definition: gp_timer/v0/gp_timer.h:256
void GPTIMER_Params_init(GPTIMER_Params *params)
Function to set default values of GPTIMER_Params in params.
#define GPTIMER_PWM_OUT_PIN_MODULATION_TOGGLE
Pin Modulation type Toggle.
Definition: gp_timer/v0/gp_timer.h:155
uint32_t cntPrescaler
Definition: gp_timer/v0/gp_timer.h:258
GPTIMER Parameters.
Definition: gp_timer/v0/gp_timer.h:253
void SemaphoreP_post(SemaphoreP_Object *obj)
Post a semaphore object or unlock a mutex.
uint32_t counterInitVal
Definition: gp_timer/v0/gp_timer.h:266
#define GPTIMER_INPUT_CAPTURE_EVENT_EDGE
Capture Event on both rising and falling edge.
Definition: gp_timer/v0/gp_timer.h:110
int32_t SemaphoreP_constructBinary(SemaphoreP_Object *obj, uint32_t initValue)
Create a binary semaphore object.
uint32_t cntReloadVal
Definition: gp_timer/v0/gp_timer.h:262
void GPTIMER_close(GPTIMER_Handle handle)
Function to close the GPTIMER Peripheral specified by the handle.
#define DebugP_assert(expression)
Function to call for assert check.
Definition: DebugP.h:187
GPTIMER_Handle GPTIMER_open(uint32_t idx, const GPTIMER_Params *params)
Open the GPTIMER at index idx with parameters params.
int32_t SemaphoreP_pend(SemaphoreP_Object *obj, uint32_t timeToWaitInTicks)
Pend on a semaphore object or lock a mutex.
int32_t GPTIMER_setFreeRunMode(GPTIMER_Handle handle)
Change Timer Configuration to freerun mode.