AM243x MCU+ SDK  11.02.00
SA2UL PKA ECDSA Signing and Verification Test

Introduction

This example demonstrates the SA2UL PKA ECDSA Signing and Verification operations.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am243x-evm, am243x-lp
Example folder examples/security/crypto/sa2ul_pka/ecdsa_signing_verification/ecdsa_signing_verification.c

Steps to Run the Example

See Also

PKA

Sample Output

Shown below is a sample output when the application is run.

CCS Console:

[AsymCrypt] ECDSA Signing and Verification example started ...
[AsymCrypt] ECDSA Signing and Verification example completed!!
All tests have passed!!