AM243x MCU+ SDK  10.00.00
Datasheet

Introduction

This datasheet provides the performance numbers of various device drivers in MCU PLUS SDK for AM243X

Generic Setup details

SOC Details Values
Core R5F
Core Operating Speed 800 MHz
Cache Status Enabled
Optimization Details Values
Build Profile Release
R5F Compiler flags -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -Wall -Werror -g -mthumb -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function
R5F Linker flags -Wl,–diag_suppress=10063 -Wl,–ram_model -Wl,–reread_libs
Code Placement MSRAM
Data Placement MSRAM

Performance Numbers

AM243X-EVM

  • Software/Application used : sbl_ospi and ipc_notify_echo
  • Size of sbl_ospi appimage : 256 KB
  • Size of ipc_notify_echo appimage : 77 KB
  • Cores present in the appimage : m4f0-0, r5f0-0, r5f0-1, r5f1-0, r5f1-1
  • Boot Media Clock : 166.667 MHz (Octal DDR mode)
Boot time breakdown Time (ms)
ROM : init + SBL load from flash 12.00
SBL : SYSFW Load 12.159
SBL : System Init 0.553
SBL : Drivers_open 0.280
SBL : Board_driversOpen 22.23
SBL : Sciclient Get Version 9.9
SBL : CPU Load 38.25
SBL : Total time taken 95.372
  • The time taken for Board_driversOpen (around 20 ms) is mostly for the PHY tuning of OSPI. If this needs to be further reduced, one can pre-train the PHY, note down delay values and set it directly instead of the tuning procedure.
  • Most of the time taken for the CPU load is in loading the M4F. Other CPUs take ~1.5ms each. This needs more investigation. Possible reason is the M4F IRAM and DRAM initialization time.
  • Here the CPU load or section copy takes place from the OSPI memory to the respective memory directly, this would be slower that mem to mem copy.
  • The time taken for Sciclient Get Version can be avoided if the version check is disabled

SBL SD performance

  • Software/Application used : sbl_sd and adc_singleshot
  • Size of sbl_sd appimage : 300 KB
  • Size of adc_singleshot appimage : 34 KB
  • Cores present in the appimage : r5f0-0
  • SD card read speed : 12.5 MBps mode
Boot time breakdown Time (ms)
ROM : init + SBL load from flash 12.00
SBL : SYSFW Load 12.161
SBL : System Init 0.131
SBL : Drivers_open 13.958
SBL : Board_driversOpen 0.00
SBL : Sciclient Get Version 9.892
SBL : File read from SD Card 6.48
SBL : CPU Load 57.09
-------------------------------------— -----------—
SBL : Total time taken 111.712
  • The MMCSD driver and SD card initialization is done as part of Drivers_open, so Board_driversOpen happens instantaneously.
  • Most of the time taken for the CPU load is in loading the M4F. Other CPUs take ~1.5ms each. This needs more investigation. Possible reason is the M4F IRAM and DRAM initialization time.
  • The CPU load is faster in this case because SD bootloader is at its core a memory bootloader. Appimage file from SD card is read into the memory (this takes 15 ms in this case). The CPU load now is mostly memcpy in the OCRAM. This would be quite fast. The only caveat here is that the buffer size to receive appimage is allocated in OCRAM, so it's limited. This is not the case in OSPI.
  • The time taken for Sciclient Get Version can be avoided if the version check is disabled

XIP Benchmark

  • Software/Application used : xip_benchmark
  • FIR operation
Caching status Cycles taken
Code/Data fully cached 26710
Code/Data not cached 178717
Code/Data not cached 1 of 10 iterations 42210
  • MEMCPY operation
Caching status Cycles taken
Code/Data fully cached 1564
Code/Data not cached 6284
Code/Data not cached 1 of 10 iterations 2043

MCAN performance

  • Internal loopback mode of operation
  • Memory Mode : TX Buffer Mode, RX FIFO Mode
  • MCAN CLK : 80MHz
  • CPU : R5F
Frame Type Arbitration BitRate(Mbps) Data BitRate(Mbps) Arb Phase bits Data Phase bits Throughput (Msg/Sec)
CAN FD STANDARD FORMAT 1 5 27 538 6666
CAN FD EXTENDED FORMAT 1 5 46 538 5780

MCSPI performance

MCSPI driver performance in different modes

  • measurement is provided for Master mode in Loopback configuration with TX and RX.
  • Transfer time captured with driver API in different operation mode.
  • Throughput comparison is added for transfer of 400 Bytes with different word width and corresponding number of words.
  • Time
  • CPU : R5F
  • Transfer Length : 400 Bytes
  • SPI Clock speed : 50MHz
Number of Words Word Width (Bits) Polled mode Throughput / Transfer time Interrupt mode (Mbps) Throughput / Transfer time Dma mode (Mbps) Throughput / Transfer time
400 08 12.91 Mbps / 247.78 us 23.74 Mbps / 134.81 us 0.91 Mbps / 3500.67 us
200 16 26.22 Mbps / 122.05 us 31.49 Mbps / 101.60 us 0.95 Mbps / 3356.72 us
100 32 38.84 Mbps / 82.40 us 37.58 Mbps / 85.15 us 0.97 Mbps / 3284.85 us
  • Theoretically for 400 Bytes at 50MHz time required for clocks is 64us.
  • Additionally hardware adds 160ns + 1bit time delay between each word transfer as measured in the scope

CPSW Performance

TCP Test

  • Software/Application used : enet_lwip_cpsw
  • iperf test type : TCP iperf
  • iperf command used : iperf -c 192.168.0.158 -i 10 -t 100 -r

TCP Performance(am64x/243x emvs):

TCP direction B/W (Mb/s) CPU load(%)
TCP RX 93.4 45.37
TCP TX 93.3 57.42
TCP Biderectional TX = 87 + RX = 87 93.94

TCP Performance(am243x-lp):

TCP direction B/W (Mb/s) CPU load(%)
TCP RX 93.35 31.01
TCP TX 93.30 34.92
TCP Biderectional TX = 93.20 + RX = 93.2 63.28

UDP Test

  • Software/Application used : enet_lwip_cpsw
  • iperf test type : UDP iperf
  • iperf command used : iperf -c 192.168.0.158 -u -b 60M -l 256 -i 10 -t 100 -r

UDP TX Performance(am64x/243x emvs):

  • For Packet Size: 1500 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 100 0 -
50 Mbps 100 0.03 -
100 Mbps 100 0.07 -

UDP TX Performance(am243x-lp):

  • For Packet Size: 1500 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 100 0 -
50 Mbps 100 0 -
100 Mbps 100 0 -

UDP RX Performance(am64x/243x emvs):

  • For Packet Size: 256 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 52.26 0.08 -
50 Mbps 60.34 41 -
100 Mbps - - -
  • For Packet Size: 512 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 30.83 0 -
50 Mbps 56.74 0.09 -
100 Mbps 65.61 41 -
  • For Packet Size: 1500 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 16.84 0 -
50 Mbps 28.93 0 -
100 Mbps 53.16 0.06 -
Max(158 Mbps) 80.83 1.1 -

UDP RX Performance(am243x-lp):

  • For Packet Size: 256 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 42 0 -
50 Mbps 49 41 -
100 Mbps - - -
  • For Packet Size: 512 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 24 0 -
50 Mbps 45 0.05 -
100 Mbps 61 41 -
  • For Packet Size: 1500 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 12 0 -
50 Mbps 21 0 -
100 Mbps 38 0.03 -

IPC performance

IPC NOTIFY

  • 10000 messages are sent and average one way message latency is measured
Local Core Remote Core Average Message Latency (us)
r5f0-0 m4f0-0 1.76
r5f0-0 r5f0-1 0.77
r5f0-0 r5f1-0 0.83
r5f0-0 r5f1-1 0.89
r5f0-0 a530-0 1.03
r5f0-0 a530-1 0.00

IPC RPMSG

  • 10000 messages are sent and average one way message latency is measured
Local Core Remote Core Message Size Average Message Latency (us)
r5f0-0 r5f0-1 32 7.870
r5f0-0 r5f0-1 64 10.416
r5f0-0 r5f0-1 112 14.273
r5f0-0 m4f0-0 32 17.348
r5f0-0 m4f0-0 64 23.326
r5f0-0 m4f0-0 112 32.296
r5f0-0 a530-0 32 7.239
r5f0-0 a530-0 64 8.545
r5f0-0 a530-0 112 10.751

MATHLIB

MATHLIB BENCHMARK

  • Calculated for the 500 samples taken between 0 and 2 * Pi
  • Trignometric function timings compared between the optimized Mathlib mcusdk implementation and the compiler mathlib version
  • The max error for each operation between the optimized Mathlib mcusdk functions and the compiler mathlib version is printed
    Function Err Max Cycles Mathlib (mcusdk) avg cycles Mathlib (mcusdk) max cycles mathlib (clang) avg cycles mathlib (clang)
    sin 0.0000007150 52 52.250000 659 277.497986
    cos 0.0000002870 64 63.896000 593 278.550018
    sincos sin 0.0000001790 79 79.094002 467 274.223999
    sincos cos 0.0000001900
    asin 0.0000003430 73 73.096001 1271 431.056000
    acos 0.0000004770 74 74.194000 1075 385.683990
    atan 0.0000005360 85 85.085999 623 371.787994
    atan2 0.0000007150 120 107.704002 660 478.279999
- Function Err Max Cycles Mathlib (fastrts) avg cycles Mathlib (fastrts) max cycles mathlib (clang) avg cycles mathlib (clang)
sin 0.0000004170 51 51.048000 517 275.503998
cos 0.0000003870 54 54.015999 512 276.832001
sincos sin 0.0000004170 58 58.084000 483 274.227997
sincos cos 0.0000003750
asin 0.0000003430 75 75.038002 578 428.697998
acos 0.0000004770 76 76.033997 810 383.730011
atan 0.0000001190 70 70.113998 493 371.148010
atan2 0.0000002380 109 109.122002 729 478.171997

SA2UL

PKA RSA SIGN VERIFY

  • Software/Application used : test_sa2ul_pka
  • Supported keys : 4K and 2K
  • CPU with operating speed : R5F with 800MHZ
  • OS used : nortos
    ECDSA Sign/sec Verify/sec Sign and verify/sec
    2048 632 8849 589
    4096 97 2801 94

SHA

  • Software/Application used : test_sa2ul_sha
  • Code Placement : OCMC
  • Data Placement : OCMC
  • Input Data sizes : 512B, 1KB, 2KB, 4KB, 8KB, 16KB and 32KB
  • CPU with operating speed : R5F with 800MHZ
    SHA Size Performance (Mbps)
    512 32.00 KB 2042.136834
    512 16.00 KB 1799.234716
    512 8.00 KB 1401.427388
    512 4.00 KB 954.153017
    512 2.00 KB 579.451813
    512 1024.00 B 331.040057
    512 512.00 B 176.086840
    256 32.00 KB 1586.191978
    256 16.00 KB 1406.767018
    256 8.00 KB 1142.388983
    256 4.00 KB 829.254713
    256 2.00 KB 537.951980
    256 1024.00 B 316.537867
    256 512.00 B 172.299926

PKA ECDSA

  • Software/Application used : test_sa2ul_pka
  • Supported Curves : p-256 and p-384
  • CPU with operating speed : R5F with 800MHZ
  • OS used : nortos
    ECDSA Sign/sec Verify/sec Sign and verify/sec
    256 1136 693 430
    384 586 349 218

AES

  • Software/Application used : test_sa2ul_aes
  • Code Placement : OCMC
  • Data Placement : OCMC
  • Input Data sizes : 512B, 1KB, 2KB, 4KB, 8KB, 16KB and 32KB
  • CPU with operating speed : R5F with 800MHZ
    Key Length operation Size Performance (Mbps)
    128 Encryption 32.00 KB 1402.083250
    128 Decryption 32.00 KB 1820.570873
    128 Encryption 16.00 KB 1273.409113
    128 Decryption 16.00 KB 1618.172840
    128 Encryption 8.00 KB 1070.259457
    128 Decryption 8.00 KB 1338.015517
    128 Encryption 4.00 KB 839.989746
    128 Decryption 4.00 KB 981.445152
    128 Encryption 2.00 KB 590.574029
    128 Decryption 2.00 KB 674.204002
    128 Encryption 1024.00 B 371.856559
    128 Decryption 1024.00 B 394.154087
    128 Encryption 512.00 B 217.698645
    128 Decryption 512.00 B 217.915808
    256 Encryption 32.00 KB 1324.377644
    256 Decryption 32.00 KB 1507.473565
    256 Encryption 16.00 KB 1206.341318
    256 Decryption 16.00 KB 1361.150631
    256 Encryption 8.00 KB 1037.885777
    256 Decryption 8.00 KB 1137.456881
    256 Encryption 4.00 KB 822.928897
    256 Decryption 4.00 KB 874.804779
    256 Encryption 2.00 KB 585.875201
    256 Decryption 2.00 KB 615.910906
    256 Encryption 1024.00 B 374.555638
    256 Decryption 1024.00 B 382.200968
    256 Encryption 512.00 B 211.161232
    256 Decryption 512.00 B 208.288838

RSA ENCRYPT DECRYPT

  • Software/Application used : test_sa2ul_rsa
  • Code Placement : OCMC
  • Supported keys : 4K and 2K
  • CPU with operating speed : R5F with 800MHZ
  • Software/Application used : test_sa2ul_rsa
    Key Length operation Size Performance(Mbps)
    2048 Encryption 256.00 B 0.554899
    2048 Decryption 256.00 B 1.295114
    4096 Encryption 512.00 B 0.597249
    4096 Decryption 512.00 B 0.400690

USB

NET Driver ( RNDIS )

  • Measures TCP only TX bandwidth at every 1 sec interval using standard lwip-perf application.
  • Software/Applicaiton used : rndis_nortos
  • Input media : USB 2.0
  • Linux Host application used : iperf
  • CPU with operating speed : R5F with 800MHz
  • lwip-webserver ip address : 192.168.7.1
  • RNDIS Host ip address : 192.168.7.2
  • TCP window size : 85.0 KByte
ID Interval Transfer Bandwidth
0 0.0- 1.0 sec 4.25 MBytes 35.7 Mbits/sec
1 1.0- 2.0 sec 4.12 MBytes 34.6 Mbits/sec
2 2.0- 3.0 sec 4.12 MBytes 34.6 Mbits/sec
3 3.0- 4.0 sec 4.12 MBytes 34.6 Mbits/sec
4 4.0- 5.0 sec 4.12 MBytes 34.6 Mbits/sec
5 5.0- 6.0 sec 4.12 MBytes 34.6 Mbits/sec
6 6.0- 7.0 sec 4.12 MBytes 34.6 Mbits/sec
7 7.0- 8.0 sec 4.12 MBytes 34.6 Mbits/sec
8 8.0- 9.0 sec 4.25 MBytes 35.7 Mbits/sec
9 9.0-10.0 sec 4.12 MBytes 34.6 Mbits/sec
10 0.0-10.0 sec 41.5 MBytes 34.8 Mbits/sec