![Logo](ti_logo.svg) |
AM243x MCU+ SDK
09.02.01
|
|
Go to the documentation of this file.
53 #include <drivers/hw_include/am64x_am243x/cslr_soc_baseaddress.h>
60 #define SOC_DOMAIN_ID_MAIN (0U)
61 #define SOC_DOMAIN_ID_MCU (1U)
70 #define SOC_PSC_DOMAIN_ID_MAIN (0U)
71 #define SOC_PSC_DOMAIN_ID_MCU (1U)
80 #define SOC_PSC_SYNCRESETDISABLE (0x0U)
81 #define SOC_PSC_SYNCRESET (0x1U)
82 #define SOC_PSC_DISABLE (0x2U)
83 #define SOC_PSC_ENABLE (0x3U)
91 #define SOC_PSC_DOMAIN_OFF (0x0U)
92 #define SOC_PSC_DOMAIN_ON (0x1U)
98 #define SOC_BOOTMODE_MMCSD (0X36C3)
103 #define SOC_FWL_OPEN_MAGIC_NUM (0XFEDCBA98u)
106 #define MCU_MCSPI0_CFG_BASE_AFTER_ADDR_TRANSLATE (CSL_MCU_MCSPI0_CFG_BASE + 0x80000000)
107 #define MCU_MCSPI1_CFG_BASE_AFTER_ADDR_TRANSLATE (CSL_MCU_MCSPI1_CFG_BASE + 0x80000000)
108 #define MCU_UART0_BASE_AFTER_ADDR_TRANSLATE (CSL_MCU_UART0_BASE + 0x80000000)
109 #define MCU_UART1_BASE_AFTER_ADDR_TRANSLATE (CSL_MCU_UART1_BASE + 0x80000000)
115 int32_t status = (int32_t)(-3);
117 if ( (baseAddr == CSL_I2C0_CFG_BASE) || \
118 (baseAddr == CSL_I2C1_CFG_BASE) || \
119 (baseAddr == CSL_I2C2_CFG_BASE) || \
120 (baseAddr == CSL_I2C3_CFG_BASE) )
132 int32_t status = (int32_t)-3;
134 if ((baseAddr == CSL_MCSPI0_CFG_BASE) || \
135 (baseAddr == CSL_MCSPI1_CFG_BASE) || \
136 (baseAddr == CSL_MCSPI2_CFG_BASE) || \
137 (baseAddr == CSL_MCSPI3_CFG_BASE) || \
138 (baseAddr == CSL_MCSPI4_CFG_BASE) || \
139 (baseAddr == CSL_MCU_MCSPI0_CFG_BASE) || \
140 (baseAddr == CSL_MCU_MCSPI1_CFG_BASE) || \
153 int32_t status = (int32_t)-3;
155 if ((baseAddr == CSL_UART0_BASE) ||
156 (baseAddr == CSL_UART1_BASE) ||
157 (baseAddr == CSL_UART2_BASE) ||
158 (baseAddr == CSL_UART3_BASE) ||
159 (baseAddr == CSL_UART4_BASE) ||
160 (baseAddr == CSL_UART5_BASE) ||
161 (baseAddr == CSL_UART6_BASE) ||
162 (baseAddr == CSL_MCU_UART0_BASE) ||
163 (baseAddr == CSL_MCU_UART1_BASE) ||
370 uint32_t debugIsolationEnable);
397 uint32_t *domainState, uint32_t *moduleState);
409 int32_t
SOC_setPSCState(uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t pscState);
This file contains prototypes for APIs contained as a part of SCICLIENT as well as the structures of ...
int32_t SOC_moduleSetClockFrequency(uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
Set module clock to specified frequency.
int32_t SOC_moduleSetClockFrequencyWithParent(uint32_t moduleId, uint32_t clkId, uint32_t clkParent, uint64_t clkRate)
Set module clock to specified frequency and with a specific parent.
void SOC_controlModuleUnlockMMR(uint32_t domainId, uint32_t partition)
Unlock control module partition to allow writes into control MMRs.
uint64_t SOC_virtToPhy(void *virtAddr)
SOC Virtual (CPU) to Physical address translation function.
#define MCU_UART1_BASE_AFTER_ADDR_TRANSLATE
Definition: soc.h:109
void SOC_generateSwWarmResetMainDomainFromMcuDomain(void)
Generate SW WARM Reset Main Domain from Mcu Domain.
void SOC_generateSwPORResetMainDomainFromMcuDomain(void)
Generate SW POR Reset Main Domain from Mcu Domain.
uint32_t SOC_getFlashDataBaseAddr(void)
This function gets the SOC mapped data base address of the flash.
void SOC_clearResetCauseMainMcuDomain(uint32_t resetCause)
Clears reason for Warm and Main/Mcu Domain Power On Resets. CTRLMMR_RST_SRC is just a mirror of CTRLM...
#define MCU_MCSPI0_CFG_BASE_AFTER_ADDR_TRANSLATE
Definition: soc.h:106
void SOC_unlockAllMMR(void)
Unlocks all the control MMRs.
void SOC_setMCUResetIsolationDone(uint32_t value)
Set MCU reset isolation done flag.
void SOC_generateSwWarmResetMcuDomain(void)
Generate SW WARM Reset Mcu Domain.
void SOC_waitForFwlUnlock(void)
Wait for Firewall unlock from SBL. The function polls for a Software defined Magic number at the PSRA...
int32_t SOC_moduleGetClockFrequency(uint32_t moduleId, uint32_t clkId, uint64_t *clkRate)
Get module clock frequency.
uint32_t SOC_getWarmResetCauseMainDomain(void)
Get the reset reason source for Main Domain.
int32_t SOC_isHsDevice(void)
Check the device is HS or not.
void SOC_waitMainDomainReset(void)
Wait for main domain reset to complete.
void * SOC_phyToVirt(uint64_t phyAddr)
Physical to Virtual (CPU) address translation function.
Structure containing the CPU Info such as CPU ID and Cluster Group ID.
Definition: CpuIdP.h:57
#define MCU_MCSPI1_CFG_BASE_AFTER_ADDR_TRANSLATE
Definition: soc.h:107
uint32_t value
Definition: tisci_otp_revision.h:2
int32_t SOC_setPSCState(uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t pscState)
Set PSC (Power Sleep Controller) state.
uint64_t SOC_getSelfCpuClk(void)
Get the clock frequency in Hz of the CPU on which the driver is running.
int32_t SOC_enableResetIsolation(uint32_t main2McuIsolation, uint32_t mcu2MainIsolation, uint32_t debugIsolationEnable)
Enable reset isolation of MCU domain for safety applications.
static int32_t UART_IsBaseAddrValid(uint32_t baseAddr)
API to validate UART base address.
Definition: soc.h:151
void SOC_generateSwWarmResetMainDomain(void)
Generate SW Warm Reset Main Domain.
void SOC_allowEpwmTzReg(uint32_t epwmInstance, uint32_t enable)
Enable or disable writes to the EPWM tripZone registers.
static int32_t I2C_lld_isBaseAddrValid(uint32_t baseAddr)
API to validate I2C base address.
Definition: soc.h:112
static int32_t MCSPI_lld_isBaseAddrValid(uint32_t baseAddr)
API to validate MCSPI base address.
Definition: soc.h:130
void SOC_generateSwPORResetMainDomain(void)
Generate SW POR Reset Main Domain.
void SOC_controlModuleLockMMR(uint32_t domainId, uint32_t partition)
Lock control module partition to prevent writes into control MMRs.
int32_t SOC_moduleClockEnable(uint32_t moduleId, uint32_t enable)
Enable clock to specified module.
void SOC_setDevStat(uint32_t bootMode)
Change boot mode by setting devstat register.
int32_t SOC_getPSCState(uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t *domainState, uint32_t *moduleState)
Get PSC (Power Sleep Controller) state.
const char * SOC_getCoreName(uint16_t coreId)
Convert a core ID to a user readable name.
uint32_t SOC_isR5FDualCoreMode(CSL_ArmR5CPUInfo *cpuInfo)
Return R5SS supporting single or dual core mode.
void SOC_setEpwmTbClk(uint32_t epwmInstance, uint32_t enable)
Enable or disable ePWM time base clock from Control MMR.
#define MCU_UART0_BASE_AFTER_ADDR_TRANSLATE
Definition: soc.h:108
uint32_t SOC_getWarmResetCauseMcuDomain(void)
Get the reset reason source for Mcu Domain.