![Logo](ti_logo.svg) |
AM243x MCU+ SDK
09.02.01
|
|
Go to the documentation of this file.
55 #ifndef INCLUDE_SDL_UTILS_H_
56 #define INCLUDE_SDL_UTILS_H_
63 #include <sdl/include/sdl_types.h>
uint32_t CONTEXTIDR
Definition: sdl_r5_utils.h:161
uint32_t MPUIR
Definition: sdl_r5_utils.h:99
uint32_t SDL_UTILS_getCONTEXTIDR(void)
uint32_t SDL_UTILS_getMIDR(void)
uint32_t ID_MMFR3
Definition: sdl_r5_utils.h:117
uint32_t nVALIRQSET
Definition: sdl_r5_utils.h:169
uint32_t SDL_UTILS_getID_AFR0(void)
uint32_t ADFSR
Definition: sdl_r5_utils.h:203
uint32_t SDL_UTILS_getID_ISAR5(void)
uint32_t SDL_UTILS_getnVALIRQSET(void)
uint32_t BTCMRegionR
Definition: sdl_r5_utils.h:155
uint32_t SDL_UTILS_getnVALDEBUGCLEAR(void)
uint32_t SDL_UTILS_getPinOptionR(void)
uint32_t nVALDEBUGSET
Definition: sdl_r5_utils.h:175
uint32_t SDL_UTILS_getID_DFR0(void)
uint32_t SDL_UTILS_getID_MMFR2(void)
uint32_t PinOptionR
Definition: sdl_r5_utils.h:189
uint32_t PFR0
Definition: sdl_r5_utils.h:103
uint32_t ACTLR
Definition: sdl_r5_utils.h:141
uint32_t SDL_UTILS_getMPURegionBaseADDR(void)
uint32_t CSSELR
Definition: sdl_r5_utils.h:137
uint32_t SDL_UTILS_getBuildOption1R(void)
uint32_t DFSR
Definition: sdl_r5_utils.h:201
uint32_t SDL_UTILS_getSlavePortControlR(void)
uint32_t AHBRR
Definition: sdl_r5_utils.h:195
uint32_t ID_MMFR0
Definition: sdl_r5_utils.h:111
Structure containing R5F CPU Static Registers.
Definition: sdl_r5_utils.h:92
uint32_t nVALIRQCLEAR
Definition: sdl_r5_utils.h:177
uint32_t nVALRESETSET
Definition: sdl_r5_utils.h:173
uint32_t SDL_UTILS_getnVALRESETSET(void)
uint32_t SDL_UTILS_getADFSR(void)
uint32_t ThreadProcessIDR3
Definition: sdl_r5_utils.h:167
uint32_t SDL_UTILS_getnVALFIQSET(void)
uint32_t ID_ISAR0
Definition: sdl_r5_utils.h:119
uint32_t SDL_UTILS_getID_MMFR3(void)
uint32_t SlavePortControlR
Definition: sdl_r5_utils.h:159
uint32_t SDL_UTILS_getMPIDR(void)
uint32_t SDL_UTILS_getLLPPvirtualAXIRR(void)
uint32_t SDL_UTILS_getThreadProcessIDR1(void)
uint32_t SDL_UTILS_getCTR(void)
void SDL_UTILS_enable_cache_event_bus(void)
uint32_t DFAR
Definition: sdl_r5_utils.h:205
uint32_t ID_ISAR2
Definition: sdl_r5_utils.h:123
uint32_t SDL_UTILS_getThreadProcessIDR2(void)
uint32_t SDL_UTILS_getnVALFIQCLEAR(void)
uint32_t SDL_UTILS_getnVALIRQCLEAR(void)
uint32_t PFR1
Definition: sdl_r5_utils.h:105
int32_t SDL_CPU_staticRegisterRead(SDL_R5FCPU_StaticRegs *pCPUStaticRegs)
This API is used to get the value of static registers for R5F CPU.
uint32_t PMOVSR
Definition: sdl_r5_utils.h:199
uint32_t SDL_UTILS_getID_ISAR3(void)
uint32_t SDL_UTILS_getMPUIR(void)
uint32_t SDL_UTILS_getIFAR(void)
uint32_t SDL_UTILS_getBuildOption2R(void)
uint32_t SDL_UTILS_getSCTLR(void)
uint32_t SDL_UTILS_getCFLR(void)
uint32_t SDL_UTILS_getID_MMFR1(void)
uint32_t ATCMRegionR
Definition: sdl_r5_utils.h:157
uint32_t ID_ISAR5
Definition: sdl_r5_utils.h:129
uint32_t SDL_UTILS_getID_ISAR0(void)
uint32_t nVALRESETCLEAR
Definition: sdl_r5_utils.h:181
uint32_t ID_MMFR1
Definition: sdl_r5_utils.h:113
uint32_t SDL_UTILS_getSecondaryACTLR(void)
uint32_t SDL_UTILS_getID_MMFR0(void)
uint32_t SDL_UTILS_getPFR1(void)
uint32_t MIDR
Definition: sdl_r5_utils.h:93
uint32_t IFAR
Definition: sdl_r5_utils.h:209
uint32_t MPURegionAccessControlR
Definition: sdl_r5_utils.h:151
uint32_t ID_MMFR2
Definition: sdl_r5_utils.h:115
uint32_t RGNR
Definition: sdl_r5_utils.h:153
uint32_t SDL_UTILS_getAIDR(void)
uint32_t SDL_UTILS_getID_ISAR1(void)
uint32_t SDL_UTILS_getAIFSR(void)
uint32_t MPURegionEnableR
Definition: sdl_r5_utils.h:149
uint32_t CCSIDR
Definition: sdl_r5_utils.h:131
uint32_t MPIDR
Definition: sdl_r5_utils.h:101
uint32_t SDL_UTILS_getMPURegionEnableR(void)
uint32_t nVALFIQCLEAR
Definition: sdl_r5_utils.h:179
uint32_t MPURegionBaseADDR
Definition: sdl_r5_utils.h:147
uint32_t SDL_UTILS_getID_ISAR2(void)
uint32_t SDL_UTILS_getAHBRR(void)
uint32_t SDL_UTILS_getID_ISAR4(void)
uint32_t ThreadProcessIDR2
Definition: sdl_r5_utils.h:165
uint32_t SDL_UTILS_getDFAR(void)
uint32_t ID_ISAR1
Definition: sdl_r5_utils.h:121
uint32_t ID_AFR0
Definition: sdl_r5_utils.h:109
uint32_t IFSR
Definition: sdl_r5_utils.h:207
uint32_t SDL_UTILS_getCSSELR(void)
void SDL_UTILS_enable_event_bus(void)
uint32_t SDL_UTILS_getATCMRegionR(void)
uint32_t SDL_UTILS_getIFSR(void)
uint32_t AIDR
Definition: sdl_r5_utils.h:135
uint32_t SDL_UTILS_getnVALDEBUGSET(void)
uint32_t CTR
Definition: sdl_r5_utils.h:95
uint32_t SDL_UTILS_getLLPPnormalAXIRR(void)
uint32_t nVALDEBUGCLEAR
Definition: sdl_r5_utils.h:183
uint32_t SDL_UTILS_getPFR0(void)
uint32_t ID_ISAR4
Definition: sdl_r5_utils.h:127
uint32_t CFLR
Definition: sdl_r5_utils.h:197
uint32_t CLIDR
Definition: sdl_r5_utils.h:133
uint32_t SDL_UTILS_getRGNR(void)
uint32_t SDL_UTILS_getnVALRESETCLEAR(void)
uint32_t LLPPnormalAXIRR
Definition: sdl_r5_utils.h:191
uint32_t SDL_UTILS_getACTLR(void)
uint32_t SDL_UTILS_getDFSR(void)
uint32_t nVALFIQSET
Definition: sdl_r5_utils.h:171
uint32_t ThreadProcessIDR1
Definition: sdl_r5_utils.h:163
uint32_t ID_DFR0
Definition: sdl_r5_utils.h:107
uint32_t SDL_UTILS_getPMOVSR(void)
uint32_t SDL_UTILS_getMPURegionAccessControlR(void)
uint32_t BuildOption2R
Definition: sdl_r5_utils.h:187
uint32_t SDL_UTILS_getThreadProcessIDR3(void)
uint32_t SDL_UTILS_getTCMTR(void)
uint32_t CPACR
Definition: sdl_r5_utils.h:145
uint32_t TCMTR
Definition: sdl_r5_utils.h:97
uint32_t SDL_UTILS_getCLIDR(void)
uint32_t SDL_UTILS_getBTCMRegionR(void)
uint32_t SDL_UTILS_getCPACR(void)
uint32_t SDL_UTILS_getCCSIDR(void)
uint32_t LLPPvirtualAXIRR
Definition: sdl_r5_utils.h:193
uint32_t BuildOption1R
Definition: sdl_r5_utils.h:185
uint32_t ID_ISAR3
Definition: sdl_r5_utils.h:125
uint32_t SecondaryACTLR
Definition: sdl_r5_utils.h:143
uint32_t SCTLR
Definition: sdl_r5_utils.h:139
uint32_t AIFSR
Definition: sdl_r5_utils.h:211