AM243x MCU+ SDK  09.02.01
HS FS Migration Guide

The MCU+SDK primarily supports HS-FS (High Security - Field Securable) as the main device and the support for GP is deprecated. This document aims to list out the differences between the two device types and aid the users to develop on HS-FS device type.

System Firmware

One of the major differences between GP and HS-FS is System Firmware (SYSFW). In both devices, SYSFW is always signed with an asymmetric key (RSA/ECC) and wrapped in the resulting x509 certificate. In case of GP, the key used for signing is not verified by ROM, so usually a degenerate key is used. In case of HS-FS device, SYSFW will be encrypted with TI encryption key (TI MEK) and signed with TI asymmetric key (TI MPK). The SDK will contain the encrypted and signed binary.

SYSFW in HS-FS device

NON-SBL Example Appimage Build

In case of example applications other than SBL (hello_world, dpl_demo etc...) the same application image file (*.appimage) can be booted by SBL on HS-FS / GP device, nothing special to be done for HS-FS since there is no extra signing needed.

Note: Appimages would eventually need signing by x509Certificate in HS-FS. This change is yet to be implemented. Once this is done, the appimages would have different extensions for HS-FS image. *.appimage would now become *.appimage.hs_fs

SBL Application Build

In case of SBL applications (sbl_sd, sbl_ospi, sbl_null etc...) since SDK follows combined boot flow, SYSFW is packaged along with the sbl final image (*.tiimage). Since the SYSFW is different between GP and HS-FS, the sbl final image also will change. This is taken care through an additional keyword in the file extension, **'hs_fs'**. The *.tiimage would now become *.hs_fs.tiimage For example in the case of sbl_ospi, with release build profile, the final image in the case of GP device type would be

  • sbl_ospi.release.tiimage

In case of HS-FS device type, it would be

  • sbl_ospi.release.hs_fs.tiimage

HS-FS images will be automatically built when you build SBLs, so no extra build options are required to be passed.

Application boot using SBL (SBL OSPI, SBL NULL, SBL UART, SBL SD etc.)

Since most of the differences in HS-FS is related to image signing, once the SBL and application image is correctly built, rest of the flow is the same as GP for application boot. Take care that the right images are used. For example, to use SBL NULL for your application boot, flash the sbl_null.release.hs_fs.tiimage image. Same goes for other SBLs.

Attention
Please make sure that you use the SBL images with the *.hs_fs.tiimage and application images *.appimage.hs_fs extension while flashing.

Application boot using CCS + GELs

This section refers to the flow where users do not use any SBL, instead uses CCS + GELs and load_dmsc_hsfs.js to initialize SoC, load the DMSC M3 and manually load user application to desired core.

  • M3 JTAG is locked, so can't connect to M3 and run GELs

Steps to do DMSC initialization from CCS

  • Set the board in DEV-BOOT mode (mandatory)
  • Power ON the EVM/board
  • Launch the CCS target configuration file
  • Run the load_dmsc_hs_fs.js script from the scripting console

Since it can't connect to M3, it connects to R5. Now it runs an application (sciclient_ccs_init). The sciclient_ccs_init application will load load M3 with SYSFW and set the boardcfg and initialize the other cores.

The major difference here is the strict adherence of the boot mode to DEV-BOOT mode. This is necessary to be able to connect to the R5 and load the sciclient_ccs_init application. The DEV BOOT mode looks like below:

DEV BOOT MODE

To reiterate, to do application boot using CCS and GELs in HS-FS device

  • Set the board in DEV-BOOT mode (mandatory)
  • Power ON the EVM/board
  • Launch the CCS target configuration file
  • Run the load_dmsc_hs_fs.js script from the scripting console
  • Wait for the SYSFW version to be printed on CCS console
  • Manually reset the R5FSS0_0 core and proceed towards application load

Difference of SYSFW loading in SBL mode and CCS mode in HS-FS

In the SBL based flow, the SBL image will contain the SYSFW in the appropriate format and the ROM will load the SBL and SYSFW. In this scenario, the above mentioned sysfw-hs-fs-enc.bin and sysfw-hs-fs-enc-cert.bin binaries would be used in the image creation. In case of CCS based flow, the loading is done in a different way using an R5 application. Here we have to use a binary concatenation of the certificate and the encrypted image and generate a hex header out of it. This hex header is then included by the R5 application and then loaded. This is already done and the header file is kept at the same location as other SYSFW binaries - sysfw_hs_fs_signed.h

Firewall Configurations

Since HS-FS devices has some the secure services, the firewall configurations are somewhat different compared to the fully open and non-secure GP devices. For example some of the SoC memory regions are firewalled in HS-FS devices. This includes the MSRAM, which cores or DMA engines might need to access. To tackle this, all the SBLs in the SDK opens the MSRAM firewalls right after SYSFW boot notification comes up. If you write your own bootloader, you should also do this. The API Bootloader_socOpenFirewalls can be used for this. For example usage, please check the source of any SBL.

Summary of differences in GP vs HS-FS

Entity GP HS-FS
SYSFW image Plain (sysfw.bin) Signed and encrypted with TI Key (sysfw-hs-fs-enc.bin, sysfw-hs-fs-enc-cert.bin)
Application image name *.appimage *.appimage.hs_fs (eventually)
SBL image name *.tiimage *.hs_fs.tiimage
CCS + GEL flow bootmode NO-BOOT recommended, any bootmode functional DEV-BOOT mode mandatory
CCS + GEL flow js script load_dmsc.js load_dmsc_hs_fs.js
Firewall Configurations Firewalls Open Some regions are firewalled

Signing of Images in GP vs HS-FS

SBL images and non-SBL example application images use different signing scripts. This is due to the difference in the x509 certificate format expected by ROM and SYSFW. These differences and scripting is already part of SDK makefiles, but in case if the user has their own build system and wants to integrate these steps into it, please go through this section. The signing scripts used are python3 based.

SYSFW Signing

SYSFW is not signed with SDK signing scripts. Pre-encrypted SYSFW binaries with x509 certificate binary generated as a result of signing with the TI keys is part of the SDK.

SBL Signing

To create the x509 certificate header-ed SBL image, the script used is rom_image_gen.py. This is located in ${SDK_ROOT}/tools/boot/signing. The usage of the script will be printed if you run it with -h option like so:

$ python3 rom_image_gen.py -h
usage: rom_image_gen.py [-h] [--swrv SWRV] --sbl-bin SBL_BIN [--sbl-enc] [--enc-key ENC_KEY] --sysfw-bin
SYSFW_BIN [--sysfw-inner-cert SYSFW_INNER_CERT] --boardcfg-blob BOARDCFG_BLOB
--sbl-loadaddr SBL_LOADADDR --sysfw-loadaddr SYSFW_LOADADDR --bcfg-loadaddr
BCFG_LOADADDR --key KEY --rom-image ROM_IMAGE [--debug DEBUG]
Creates a ROM-boot-able combined image when the SBL, SYSFW and BoardCfg data are provided
optional arguments:
-h, --help show this help message and exit
--swrv SWRV Software revision number
--sbl-bin SBL_BIN Path to the SBL binary
--sbl-enc Encrypt SBL or not
--enc-key ENC_KEY Path to the SBL Encryption Key
--sysfw-bin SYSFW_BIN
Path to the sysfw binary
--sysfw-inner-cert SYSFW_INNER_CERT
Path to the sysfw inner certificate
--boardcfg-blob BOARDCFG_BLOB
Path to the boardcfg blob
--sbl-loadaddr SBL_LOADADDR
Load address at which SBL needs to be loaded
--sysfw-loadaddr SYSFW_LOADADDR
Load address at which SYSFW needs to be loaded
--bcfg-loadaddr BCFG_LOADADDR
Load address at which BOARDCFG needs to be loaded
--key KEY Path to the signing key to be used while creating the certificate
--rom-image ROM_IMAGE
Output file combined ROM image of SBL+SYSFW+Boardcfg
--debug DEBUG Debug options for the image

The script is usually run after the sbl binary is created using an objcopy utility. That is a *.bin file. In GP, we sign the binary using a degenerate key. We also pass the GP SYSFW binary and the boardcfg binary to the signing script. Here is an example of how it's done in GP for say sbl_ospi.

$ python3 rom_image_gen.py --swrv 1 --sbl-bin /path/to/sbl_ospi.release.bin --sysfw-bin /path/to/sysfw.bin --boardcfg-blob /path/to/boardcfg_blob.bin --sbl-loadaddr 0x70000000 --sysfw-loadaddr 0x44000 --bcfg-loadaddr 0x7B000 --key /path/to/rom_degenerateKey.pem --rom-image /path/to/sbl_ospi.release.tiimage

In the options mentioned here, the values used for SYSFW load address (--sysfw-loadaddr) and BoardCfg load address (--bcfg-loadaddr) are fixed for an SoC, so no need to change. For SBL load address, we generally keep the top part of the MSRAM reserved for loading the SBL in the SDK. So we give the start of MSRAM, 0x70000000. If your SBL needs to be loaded elsewhere, this value can be changed. Notice how just the SYSFW binary is passed in case of GP. This is an unsigned, unencrypted binary.

In case of HS-FS device, we use the same signing script, but there is a small difference in the usage.

$ python3 rom_image_gen.py --swrv 1 --sbl-bin /path/to/sbl_ospi.release.bin --sysfw-bin /path/to/sysfw-hs-fs-enc.bin --sysfw-inner-cert /path/to/sysfw-hs-fs-enc-cert.bin--boardcfg-blob /path/to/boardcfg_blob.bin --sbl-loadaddr 0x70000000 --sysfw-loadaddr 0x44000 --bcfg-loadaddr 0x7B000 --key /path/to/rom_degenerateKey.pem --rom-image /path/to/sbl_ospi.release.hs_fs.tiimage

You can see that we are involving the x509 certificate for the HS-FS SYSFW binary in the image creation. This is the major difference in the SBL image creation of HS-FS devices. You would observe that the other parameters are pretty much the same between both cases.

Appimage Signing

Signing for the application image is new in HS-FS compared to GP. For the signing of application images we use a different script. This is because authentication of application images are done by SYSFW and it expects a different x509 certificate format. For signing application images, the script used in appimage_x509_cert_gen.py located at ${SDK_ROOT}/tools/boot/signing/. The usage of the script will be printed if you run it with -h option like so:

python3 appimage_x509_cert_gen.py -h
usage: appimage_x509_cert_gen.py [-h] [--bin BIN] [--key KEY] [--enckey ENCKEY] [--cert CERT] [--output OUTPUT] [--core CORE] [--enc ENC] [--loadaddr LOADADDR] [--authtype AUTHTYPE]
Generates a x509 certificate for an application binary to boot it in HS device
optional arguments:
-h, --help show this help message and exit
--bin BIN Bin file that needs to be signed
--key KEY File with signing key inside it
--enckey ENCKEY File with encryption key inside it
--cert CERT Certificate file name (optional, will use a default name otherwise)
--output OUTPUT Output file name (concatenated cert+bin)
--core CORE Core on which the binary is meant to be loaded. Optional
--enc ENC If the binary need to be encrypted or not [y/n]
--loadaddr LOADADDR Target load address of the binary in hex. Default to 0x70000000
--authtype AUTHTYPE Authentication type. [0/1/2]. 0 - Move to destination address specified after authentication, 1 - In place authentication, 2 - Move to the certificate start after authentication. Default is 1

Usage of the signing script in HS-FS is fairly simple compared to the SBL signing script. Here is a typical usage for hello_world example:

$ python3 appimage_x509_cert_gen.py --bin /path/to/hello_world.release.appimage --authtype 1 --key /path/to/rom_degenerateKey.pem --output /path/to/hello_world.release.appimage.hs_fs

Note that the key used for signing is rom degenerate.