Introduction
This example uses ADS131M08 ADC IC to convert analog input signal on adc channel to samples and store the results in a shared memory which can be configured by the user (using PRU IPC module). The read samples are finally printed to the R5F console, or can also be visualized using CCS Graph plotter. GUI Composer app available on TI Gallery can also be used to evaluate the ADC using a GUI based interface.
The example does the below
- PRU controls the ADC and reads the samples
- PRU program implements ADC samples transfer interface
- PRU then writes the samples to a shared memory and creates an interrupt after writing 1 block of data
- On interrupt R5F then reads the data and prints it on console
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 freertos |
ICSSG | ICSSG0 - PRU0 |
Toolchain | ti-arm-clang, pru-cgt |
Board | am243x-evm |
Example folder | examples/pru_io/adc/ADS131/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project from the above mentioned Example folder path for R5F (It will automatically import PRU project) for the required combination.
- On importing the project, SysConfig will contain an ADC Config instance with default configurations which are compatible with the T&M SEM Adapter Board. Use SysConfig to configure the required settings for the ADC IC.
ADC SysConfig Options
- You will need to edit linker file whenever changes are made to the configuration for PRU IPC module, refer Update linker command file
Features
Supported:
- Serial Interface
- Interrupt on receiving a block of data
- ADC, Pinmux and other configurations through SysConfig interface
Important files and directory structure
Folder/Files | Description |
${SDK_INSTALL_PATH}/source/pru_io/ |
firmware/ | PRU source files providing macros for interfaces, pru_ipc, etc. |
driver/ | PRU IPC source files for sending ADC samples from PRU to R5F |
Sample Output
Shown below is a sample output when the application is run:
--------------------------------------------------
Initializing App
Initialized
--------------------------------------------------
Powering up ADC...
ADC Powered Up
--------------------------------------------------
Resetting ADC
--------------------------------------------------
Configuring ADC...
ADC Configuration completed
--------------------------------------------------
Starting ADC Conversion
Started ADC Conversion
--------------------------------------------------
----- Channel: 1 -----
Sample 1: 1858
Sample 2: 1552
Sample 3: 2037
Sample 4: 1752
Sample 5: 2005
----- Channel: 2 -----
Sample 1: 1214
Sample 2: 1372
Sample 3: 1256
Sample 4: 1425
Sample 5: 1034
Implementation Details
Refer here for complete implementation explanation: ADS131 Implementation Details