This example demonstrates writing data to & reading data from the EEPROM connected to the I2C controller. Application writes 10 Bytes to the EEPROM in interrupt mode and then reads back the same 10 Bytes.
The application makes use of the I2C LLD driver and it's memory read/write polling APIs.
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | am243x-evm, am243x-lp |
Example folder | examples/drivers/i2c/i2c_memory_read_polling_lld |
Shown below is a sample output when the application is run,