This example performs FSI TX to FSI RX internal loopback in polled mode. The application configures an instance of FSI TX and FSI RX module with below configuration
With above configuration, the application transfers 100 frames of data from FSI TX, waits for data to be received by FSI RX and then compares the data.
Once the transfer it completes, it compares the source and destination buffers for any data mismatch.
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | am243x-evm, am243x-lp |
Example folder | examples/drivers/fsi/fsi_loopback_polling/ |
Shown below is a sample output when the application is run,