![Logo](ti_logo.svg) |
AM243x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
53 #ifndef SCICLIENT_RM_H_
54 #define SCICLIENT_RM_H_
313 uint16_t *dst_input);
336 uint16_t *dst_input);
360 uint16_t *src_output);
Configures a Navigator Subsystem UDMAP transmit channel.
Definition: tisci_rm_udmap.h:1012
int32_t Sciclient_rmIrqTranslateIaOutput(uint16_t ia_dev_id, uint16_t ia_output, uint16_t dst_dev_id, uint16_t *dst_input)
Translates an interrupt aggregator output to the peripheral input it's connected to....
int32_t Sciclient_rmPsilUnpair(const struct tisci_msg_rm_psil_unpair_req *req, uint32_t timeout)
Unpairs a PSI-L source thread and destination thread.
int32_t Sciclient_rmIrqTranslateIrOutput(uint16_t ir_dev_id, uint16_t ir_output, uint16_t dst_dev_id, uint16_t *dst_input)
Translates an interrupt router output to the peripheral input it's connected to. The primary use of t...
Response to configuring a UDMAP transmit channel.
Definition: tisci_rm_udmap.h:1042
Response to configuring a ring monitor.
Definition: tisci_rm_ra.h:421
Configures peripherals within the interrupt subsystem according to the valid configuration provided....
Definition: tisci_rm_irq.h:202
int32_t Sciclient_rmIrqReleaseRaw(const struct tisci_msg_rm_irq_release_req *req, uint32_t timeout)
Releases configurations within individual peripherals within the interrupt subsystem (interrupt route...
int32_t Sciclient_rmIrqRelease(const struct tisci_msg_rm_irq_release_req *req, uint32_t timeout)
Releases a peripheral to processor IRQ.
int32_t Sciclient_rmSetProxyCfg(const struct tisci_msg_rm_proxy_cfg_req *req, uint32_t timeout)
Proxy Configuration Request.
This file contains:
Definition: tisci_rm_proxy.h:87
int32_t Sciclient_rmUdmapTxChCfg(const struct tisci_msg_rm_udmap_tx_ch_cfg_req *req, const struct tisci_msg_rm_udmap_tx_ch_cfg_resp *resp, uint32_t timeout)
Configures a Navigator Subsystem UDMAP transmit channel.
int32_t Sciclient_rmUdmapFlowSizeThreshCfg(const struct tisci_msg_rm_udmap_flow_size_thresh_cfg_req *req, const struct tisci_msg_rm_udmap_flow_size_thresh_cfg_resp *resp, uint32_t timeout)
Configures a Navigator Subsystem UDMAP receive flow's size threshold fields.
Configures a Navigator Subsystem ring monitor. Configures the real-time registers of a Navigator Subs...
Definition: tisci_rm_ra.h:403
Response to configuring a UDMAP receive channel.
Definition: tisci_rm_udmap.h:1271
Reads the specified thread real-time configuration register from a specified PSI-L thread using the P...
Definition: tisci_rm_psil.h:209
int32_t Sciclient_rmIrqTranslateIrqInput(uint16_t dst_dev_id, uint16_t dst_input, uint16_t src_dev_id, uint16_t *src_output)
Translates a peripheral input to the connected interrupt router or aggregator output....
int32_t Sciclient_rmIrqSet(const struct tisci_msg_rm_irq_set_req *req, const struct tisci_msg_rm_irq_set_resp *resp, uint32_t timeout)
Configures a peripheral to processor IRQ.
Get resource range response message.
Definition: tisci_rm_core.h:130
int32_t Sciclient_rmGetResourceRange(const struct tisci_msg_rm_get_resource_range_req *req, struct tisci_msg_rm_get_resource_range_resp *resp, uint32_t timeout)
Retrieves a host's assigned range for a resource.
int32_t Sciclient_rmUdmapGcfgCfg(const struct tisci_msg_rm_udmap_gcfg_cfg_req *req, const struct tisci_msg_rm_udmap_gcfg_cfg_resp *resp, uint32_t timeout)
Configures Navigator Subsystem UDMAP GCFG region.
int32_t Sciclient_rmRingCfg(const struct tisci_msg_rm_ring_cfg_req *req, const struct tisci_msg_rm_ring_cfg_resp *resp, uint32_t timeout)
Configures a Navigator Subsystem ring.
Response to setting a peripheral to processor interrupt.
Definition: tisci_rm_irq.h:222
int32_t Sciclient_rmIrOutpIsFree(uint16_t id, uint16_t outp)
Checks the output's control register to see if the output line has an input line mapped to it.
Unpairs a PSI-L source thread from a destination thread.
Definition: tisci_rm_psil.h:163
int32_t Sciclient_rmPsilPair(const struct tisci_msg_rm_psil_pair_req *req, uint32_t timeout)
Pairs a PSI-L source thread and destination threads.
Configures a Navigator Subsystem UDMAP receive flow.
Definition: tisci_rm_udmap.h:1559
int32_t Sciclient_rmIrqSetRaw(const struct tisci_msg_rm_irq_set_req *req, const struct tisci_msg_rm_irq_set_resp *resp, uint32_t timeout)
Configures individual peripherals within the interrupt subsystem (interrupt routers,...
This file contains:
Definition: tisci_rm_psil.h:107
This file contains:
Definition: tisci_rm_core.h:96
Response to configuring a Navigator Subsystem UDMAP receive flow's size threshold fields.
Definition: tisci_rm_udmap.h:1741
Configures a Navigator Subsystem UDMAP receive flow's size threshold fields.
Definition: tisci_rm_udmap.h:1720
Releases interrupt peripheral resources according to the valid configuration provided....
Definition: tisci_rm_irq.h:332
int32_t Sciclient_rmPsilWrite(const struct tisci_msg_rm_psil_write_req *req, uint32_t timeout)
Writes a PSI-L thread real-time register.
Response to reading a PSI-L thread real-time register.
Definition: tisci_rm_psil.h:226
int32_t Sciclient_rmPsilRead(const struct tisci_msg_rm_psil_read_req *req, struct tisci_msg_rm_psil_read_resp *resp, uint32_t timeout)
Reads a PSI-L thread real-time register.
int32_t Sciclient_rmRingMonCfg(const struct tisci_msg_rm_ring_mon_cfg_req *req, const struct tisci_msg_rm_ring_mon_cfg_resp *resp, uint32_t timeout)
Configures a Navigator Subsystem ring monitor.
int32_t Sciclient_rmUdmapFlowCfg(const struct tisci_msg_rm_udmap_flow_cfg_req *req, const struct tisci_msg_rm_udmap_flow_cfg_resp *resp, uint32_t timeout)
Configures a Navigator Subsystem UDMAP receive flow.
Response to configuring a Navigator Subsystem UDMAP receive flow.
Definition: tisci_rm_udmap.h:1591
Configures a Navigator Subsystem UDMAP global configuration region. Configures the non-real-time regi...
Definition: tisci_rm_udmap.h:768
Write to the specified thread real-time configuration register in a specified PSI-L thread using the ...
Definition: tisci_rm_psil.h:267
Response to configuring a ring.
Definition: tisci_rm_ra.h:326
int32_t Sciclient_rmUdmapRxChCfg(const struct tisci_msg_rm_udmap_rx_ch_cfg_req *req, const struct tisci_msg_rm_udmap_rx_ch_cfg_resp *resp, uint32_t timeout)
Configures a Navigator Subsystem UDMAP receive channel.
Configures a Navigator Subsystem UDMAP receive channel.
Definition: tisci_rm_udmap.h:1244
Configures a Navigator Subsystem ring.
Definition: tisci_rm_ra.h:305
Response to configuring UDMAP global configuration.
Definition: tisci_rm_udmap.h:784