Introduction
This example application demonstrates how to configure the IEEE 802.1 Qbv (EST) through our TSN yang interface.
The yang interface in the TSN is governed by a module called uniconf which runs as a daemon. Any application which interacts with the uniconf is called as a uniconf client. The uniconf client configures 802.1 Qbv by opening yang database (DB), write config yang parameters to DB and triggers the uniconf for reading parameters from DB and writing to HW. The uniconf reads or writes parameters from or to HW by calling Enet LLD driver.
Please note that the file system support is not yet integrated to ethernet examples.
In this example, we configure the talker DUT to send out traffic as per the EST schedule and the listner DUT can verify the time-slots of the received packets.
- Note
- Host based receive packet time-stamping is enabled to estimate the packet reception timing accuracy, on the listner side.However, note we have a HW errata i2401 regarding this feature and hence host based rx packet timestamping feature should be disabled in production code.
See also : Enet CPSW EST Example, Ethernet TSN and gPTP Stack - API and Integration Guide
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0_freertos |
Toolchain | ti-arm-clang |
Boards | am243x-evm, am243x-lp |
Example folder | examples/networking/tsn/est_cpsw_app |
Constraints
- This application only enables one MAC port which has the interface name tilld0. This interface is mapped to Mac port 1 for all MCU devices. To change default Mac port for this example, please change the macro DEFAULT_INTERFACE_INDEX from qosapp_misc.h from 0 another value (1, 2, 3).
- The application can be only run as talker, listener or bridge mode depending on
input characters from UART terminal. (t: talker, l: listener; b: bridge mode)
- Num of streams on talker is 2 with traffic priorities 0 and 2 mapped to HW queue 0 and 2 respectively. Num of streams and priority can be changed by modifying the gEnetEstAppTestLists from the est_init.c.
- Both talker and listener need to apply the same EST schedule with the same baseTime to have accurate test results. Thus, there is a delayOffset added to the baseTime of the EST's AdminList so that both schedules can be applied in the future and at the same time.
- The EST schedule should be applied and talker starts sending test traffic after PTP synchronization is in good condition to have accurate test results.
- The talker sends dummy data which is encapsulated in an AVTP packet. Packet sent with VLAN ID 110.
Configuration Parameters
Each of the 8 gates (one per priority) can be in one of two states:
- Open: Frames in the corresponding queue can be selected for transmission. This is represented by '
o
' in the Gate Control column of previous table.
Closed: Frames in the corresponding queue are not selected for transmission. This is represented by 'C
' in the Gate Control column.
The priority being referred to in the EST schedule described above corresponds to the CPSW destination port hardware switch priority. For VLAN tagged packets that ingress through CPSW host port, the hardware switch priority can be determined by either the CPPI channel number (P0_RX_REMAP_VLAN = 0
) or the packet priority value from the VLAN tag (P0_RX_REMAP_VLAN = 1
).
- The EST schedule is 248us long and it is composed of 4 intervals, each with a gate mask that enables transmission of 2 priorities. PTP traffic can be sent on any non-zero priority. Here we are using the priority 7 for PTP traffic. The gate of this priority is always opened to make sure there is no interruption of the PTP packet which keeps the PTP in good synchronization status. The remaining priorities are for test traffic (avtp packets).
Parameters | TimeValue |
baseTime | ((Current PTP Time + delayOffset)/delayOffset)*delayOffset |
cycleTime | 248us |
Where
baseTime
: PTP time round-off to the delayOffset
to have the same both baseTime
on talker and listener to apply the EST schedule that the same time in the future.
delayOffset
: added time to current PTP time for baseTime
to apply the schedule in the future. It should be a multiple of the cycleTime
and large enough so that user can have enough time to start talker and listener by entering a character to UART terminal. The current delayOffset
is 100000*cycleTime
= 24800000us (24.8 seconds). The factor '100000' is chosen to have delayOffset
above 20secs.
Expected Behavior
- With the schedule configured above, the expectation is that
- all priority 0 packets arrive on listener inside the time windows
- all priority 2 packets arrive on listener inside the time windows
- To check whether packets received inside a time window, the rx timestamp, called rxts (PTP time) of each received packet is captured by host port on the listener's side. Then the
timeSlot
of each packet is calculated using the following formula:
timeSlot = (rxts - BaseTime)%CycleTime
The timeSlot is compared with the time windows above for each packet to check whether the packet received inside or outside the expected time windows. The EST works when percentage of packets received outside of expected time windows less than or equal 1%.
Application Integration Guide
The EST application needs to run with the gPTP and yang configuration daemon. Therefore, the gPTP and uniconf must be run during initializing the application. To register the EST application to the initializer of the TSN App for running after the gPTP and uniconf, add the following line to the EnetApp_initTsnByCfg of the tsninit.c
#ifdef EST_APP_ENABLED
if (res == 0)
{
res = EnetApp_addEstAppModCtx(gModCtxTable);
}
#endif //EST_APP_ENABLED
Then the EST application will be started when the EnetApp_startTsn
is called.
Yang Configuration for 802.1Qbv
- Yang file for the 802.1Qbv is defined at
standard/ieee/draft/802.1/Qcw/ieee802-dot1q-sched-bridge.yang
and standard/ieee/draft/802.1/Qcw/ieee802-dot1q-sched.yang
from the https://github.com/YangModels/yang.git
- Enet-lld supports to configure the
admin-control-list
, baseTime
(admin-base-time
) and cycleTime (admin-cycle-time
), this section describes the parameters of the admin-control-list
Here are parameters of the admin-control-list
after converting parameters from yang to to xml
<?xml version='1.0' encoding='UTF-8'?>
<data xmlns="urn:ietf:params:xml:ns:netconf:base:1.0">
<interfaces xmlns="urn:ietf:params:xml:ns:yang:ietf-interfaces">
<interface>
<name/>
<bridge-port xmlns="urn:ieee:std:802.1Q:yang:ieee802-dot1q-bridge">
<traffic-class>
<traffic-class-table>
<number-of-traffic-classes/>
<priority0/>
...
<priority7/>
</traffic-class-table>
<tc-data>
<tc/>
<lqueue/>
...
</tc-data>
<number-of-pqueues/>
<pqueue-map>
<pqueue/>
<lqueue/>
</pqueue-map>
</traffic-class>
<gate-parameter-table xmlns="urn:ieee:std:802.1Q:yang:ieee802-dot1q-sched-bridge">
<gate-enabled></gate-enabled>
<admin-control-list>
<gate-control-entry>
<index/>
<operation-name/>
<time-interval-value/>
<gate-states-value/>
</gate-control-entry>
</admin-control-list>
<admin-cycle-time>
<numerator/>
<denominator/>
</admin-cycle-time>
<admin-base-time>
<seconds/>
<nanoseconds/>
</admin-base-time>
</gate-parameter-table>
</bridge-port>
</interface>
</interfaces>
</data>
All the supported parameters for 802.1Qbv are from yang standard except the mechanism for mapping traffic class and HW queue are augmented. To configure all parameters of 802.1Qbv above, application calls the yang_db_runtime_put_oneline
to write data to DB. After all required parameters written to the DB, application trigger the uniconf by writing the /ietf-interfaces/interfaces/interface|name:tilld0/bridge-port/gate-parameter-table/gate-enabled
so that the uniconf writes parameters to HW. See EnetEstApp_setAdminControlList
of the est_init.c
for yang configuration.
Note The network interface tilld0
is default network interface name, name of network interface can be changed by changing default Mac port configured for the example.
Build Enet TSN EST Example
Refer Ethernet TSN gPTP Examples to build the enet_cpsw_tsn_est_example
HW Setup
Make sure you have setup the EVM with cable connections as shown in EVM Setup. In addition, follow the steps in the next section.
- Note
- Ethernet cable must be connected and link must be up in order for the example application to continue execution.
Running Enet TSN EST example
- HW devices configuration Connect two MCUs directly through the MAC port 1.
[MCU#1 (talker)]<---------------->[MCU#2 (Listener)]
- Launch a CCS debug session, load and run the example executable, see CCS Launch, Load and Run
- The talker or listener can be run on GM or Slave, whichever devices you choose. However, we recommend running the talker on the Slave device and listener on the GM. The reason for that is the slave device needs to be adjusted PTP time to sync with the GM. Hence, there is a higher possibility that EST use case will fail due to PTP synchronization issue than running the talker on the GM. After running both devices, the PTP slave device is the one which shows the following debug log on UART
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -14648ppb, GMdiff=-24nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -14666ppb, GMdiff=-30nsec
IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -14645ppb, GMdiff=-15nsec
- When the abs(GMdiff) is below 1000ns, it is a good time to start the EST usecase.
- Start the listener. On the GM device, press
l
to start a listener. It will show log on UART terminal as follows
TimeSlots of PacketPriority: 0: [0, 62000]ns, [124000, 186000]ns,
TimeSlots of PacketPriority: 2: [62000, 124000]ns, [186000, 248000]ns,
The following AdminList param will be configured for EST:
GateMask[7..0]=oCCCCCCo (0x81), start=0 ns, end=61999 ns, dur=62000 ns
GateMask[7..0]=oCCCCoCC (0x84), start=62000 ns, end=123999 ns, dur=62000 ns
GateMask[7..0]=oCCCCCCo (0x81), start=124000 ns, end=185999 ns, dur=62000 ns
GateMask[7..0]=oCCCCoCC (0x84), start=186000 ns, end=247999 ns, dur=62000 ns
Base time=74400000000ns,Cycle time=248000ns
INF:cbase:Successfully configure TAS
INF:cbase:LLDEnetFilter:destmac:91:E0:F0:00:FE:00, vlanId:110, ethType:0x22f0
Start the talker right after the listener.
On the slave device, press t
to start a talker, It will show log on UART terminal as follows
GateMask[7..0]=oCCCCCCo (0x81), start=0 ns, end=61999 ns, dur=62000 ns
GateMask[7..0]=oCCCCoCC (0x84), start=62000 ns, end=123999 ns, dur=62000 ns
GateMask[7..0]=oCCCCCCo (0x81), start=124000 ns, end=185999 ns, dur=62000 ns
GateMask[7..0]=oCCCCoCC (0x84), start=186000 ns, end=247999 ns, dur=62000 ns
Base time=74400000000ns,Cycle time=248000ns
INF:cbase:Successfully configure TAS
- The test result will have the best accuracy if the Base time is the same for both talker and listener. To achieve that, we need to start the talker (press t) right after pressing l on the listener.
- After starting the talker, it will start sending traffic after the EST schedule takes effect (around 20 seconds).
- Observe test result The number of packets received inside expected time windows are called good packets and outside the expected time windows are bad packets. Press d on the UART terminal of the listener to display number of good/bad packets and the percentage of the bad packets. The expected result is as follows
Presss d
PacketPriority: 0, nGoodPackets: 10731108, nBadPackets: 88858, percentage of bad packets: 0%
PacketPriority: 2, nGoodPackets: 15960287, nBadPackets: 131973, percentage of bad packets: 0%
CPU Load: 39%
Press d
PacketPriority: 0, nGoodPackets: 10733815, nBadPackets: 88880, percentage of bad packets: 0%
PacketPriority: 2, nGoodPackets: 15964301, nBadPackets: 132010, percentage of bad packets: 0%
Press d
PacketPriority: 0, nGoodPackets: 10736486, nBadPackets: 88901, percentage of bad packets: 0%
PacketPriority: 2, nGoodPackets: 15968259, nBadPackets: 132056, percentage of bad packets: 0%
The expected percentage of bad packets is 0-1%.
Note
- The gPTP log will help to identify which HW device is a slave device. In case that log is not needed or noisy, please suppress them by changing the gptp:66 to gptp:55 in the enet_tsn/enet_tsn_est_example/makefile.
- If the percentage of bad packets is greater than 1%, please check the GMdiff from the gPTP log of the slave device mentioned above, the expected GMdiff less than 1000ns. The EST use case only works when PTP synchronization is in good condition.