|
AM243x MCU+ SDK
09.01.00
|
|
Go to the documentation of this file.
50 #ifndef IEEE802_DOT1AB_LLDP_ACCESS_H_
51 #define IEEE802_DOT1AB_LLDP_ACCESS_H_
52 #include "yang_db_access.h"
64 int ydbi_set_item_abk1vk0(yang_db_item_access_t *ydbia,
void *rval, uint32_t vsize, uint8_t k1,
bool status, uint8_t notice);
66 int ydbi_set_item_abk2vk0(yang_db_item_access_t *ydbia,
void *rval, uint32_t vsize, uint8_t k1, uint8_t k2,
bool status, uint8_t notice);
Definition: ieee802-dot1ab-lldp_access.h:55
int ydbi_get_item_abknvkn(yang_db_item_access_t *ydbia, void **rval, uint8_t kn[], uint8_t kn_sz, attribute_pair_t attrs[], uint8_t kvs_sz, bool status)
Get val base on n key from LLDP until end Also provided vkn as attribute.
int ydbi_set_item_abk2vk0(yang_db_item_access_t *ydbia, void *rval, uint32_t vsize, uint8_t k1, uint8_t k2, bool status, uint8_t notice)
uint32_t value
Definition: tisci_otp_revision.h:2
kvs_t vk
Definition: ieee802-dot1ab-lldp_access.h:56
uint8_t vk_sz
size of kv
Definition: ieee802-dot1ab-lldp_access.h:57
int ydbi_get_item_abk2vk0(yang_db_item_access_t *ydbia, void **rval, uint8_t k1, uint8_t k2, bool status)
int ydbi_set_item_abknvkn(yang_db_item_access_t *ydbia, uint8_t kn[], uint8_t kn_sz, attribute_pair_t attrs[], uint8_t kvs_sz, bool status, void *value, uint32_t vsize, uint8_t notice)
Set val base on n key from LLDP until end Also provided vkn as attribute.
int ydbi_get_item_abk1vk0(yang_db_item_access_t *ydbia, void **rval, uint8_t k1, bool status)
int ydbi_del_item_abknvkn(yang_db_item_access_t *ydbia, uint8_t kn[], uint8_t kn_sz, attribute_pair_t attrs[], uint8_t kvs_sz, bool status, uint8_t notice)
Set val base on n key from LLDP until end Also provided vkn as attribute.
int ydbi_set_item_abk1vk0(yang_db_item_access_t *ydbia, void *rval, uint32_t vsize, uint8_t k1, bool status, uint8_t notice)