The following sections describe the steps to configure projects that contain one PLC implementing EtherNet/IP Scanner functionality and one SITARA AM24x based EtherNet/IP Adapter device.
Examples are provided for CODESYS IEC 61131 development and runtime environments executing on Texas Instruments AM64x evaluation boards (SK-AM64, TMDS64EVM), an industrial RevPi Connect hardware (https://revolution.kunbus.com/) by KUNBUS GmbH, and an Allen-Bradley CompactLogix L16ER PLC that is configured and programmed from the RS Logix 5000 development environment.
stc
directory was removed and replaced by a new soc
directory. EDS file(s) can be found in the following path:
SOC file(s) required for the ODVA CT18 test tool or later can be found in the following path:
See CODESYS Runtime on a Texas Instruments AM64x Sitara Processor
See CODESYS Runtime on a KUNBUS RevPI Controller