![Logo](ti_logo.svg) |
AM243x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
40 #ifndef SCICLIENT_SOC_PRIV_AM64X_H_
41 #define SCICLIENT_SOC_PRIV_AM64X_H_
54 #if defined (SOC_AM64X) || defined (SOC_AM243X)
56 #define SCICLIENT_ROM_R5_TX_NORMAL_THREAD (1U)
58 #define SCICLIENT_ROM_R5_RX_NORMAL_THREAD (0U)
61 #define SCICLIENT_ROM_R5_TX_NORMAL_THREAD (4U)
63 #define SCICLIENT_ROM_R5_RX_NORMAL_THREAD (5U)
#define CSL_CORE_ID_A53SS0_0
Definition: cslr_soc_defines.h:75
#define SCICLIENT_CONTEXT_M4_SEC_0
Definition: sciclient_fmwMsgParams.h:112
#define SCICLIENT_CONTEXT_MAX_NUM
Definition: sciclient_fmwMsgParams.h:115
Private AM64x specific RM interrupt data.
#define TISCI_DEV_R5FSS0_CORE1
Definition: tisci_devices.h:164
#define CSL_CORE_ID_R5FSS1_0
Definition: cslr_soc_defines.h:73
This file contains the definition of all the parameter IDs for PM, RM, Security.
#define CSL_CORE_ID_R5FSS0_0
Definition: cslr_soc_defines.h:71
#define SCICLIENT_CONTEXT_R5_1_NONSEC_1
Definition: sciclient_fmwMsgParams.h:108
uint32_t Sciclient_getDevId(uint32_t coreId)
Definition: sciclient_soc_priv.c:147
#define SCICLIENT_CONTEXT_R5_0_SEC_0
Definition: sciclient_fmwMsgParams.h:84
CSL_SecProxyCfg gSciclientSecProxyCfg
This structure contains configuration parameters for the sec_proxy IP.
Definition: sciclient_soc_priv.c:47
#define TISCI_DEV_R5FSS0_CORE0
Definition: tisci_devices.h:163
#define SCICLIENT_CONTEXT_R5_1_SEC_1
Definition: sciclient_fmwMsgParams.h:106
uint32_t Sciclient_getContext(uint32_t contextType, uint32_t coreId)
API to get the right core context.
Definition: sciclient_soc_priv.c:69
#define TISCI_DEV_R5FSS1_CORE0
Definition: tisci_devices.h:165
#define SCICLIENT_CONTEXT_R5_0_SEC_1
Definition: sciclient_fmwMsgParams.h:88
#define SCICLIENT_CONTEXT_R5_0_NONSEC_1
Definition: sciclient_fmwMsgParams.h:90
#define TISCI_DEV_A53SS0_CORE_0
Definition: tisci_devices.h:176
#define SCICLIENT_CONTEXT_R5_1_SEC_0
Definition: sciclient_fmwMsgParams.h:102
#define CSL_CORE_ID_R5FSS1_1
Definition: cslr_soc_defines.h:74
#define SCICLIENT_CONTEXT_R5_0_NONSEC_0
Definition: sciclient_fmwMsgParams.h:86
#define SCICLIENT_CONTEXT_M4_NONSEC_0
Definition: sciclient_fmwMsgParams.h:100
#define CSL_CORE_ID_R5FSS0_1
Definition: cslr_soc_defines.h:72
#define SCICLIENT_CONTEXT_R5_1_NONSEC_0
Definition: sciclient_fmwMsgParams.h:104
#define TISCI_DEV_R5FSS1_CORE1
Definition: tisci_devices.h:166
#define CSL_CORE_ID_M4FSS0_0
Definition: cslr_soc_defines.h:70
#define TISCI_DEV_MCU_M4FSS0_CORE0
Definition: tisci_devices.h:68
#define SCICLIENT_CONTEXT_A53_NONSEC_1
Definition: sciclient_fmwMsgParams.h:96
#define SCICLIENT_CONTEXT_A53_SEC_0
Definition: sciclient_fmwMsgParams.h:92