Introduction
This example shows setup and usage of some ECC Aggregators for a few events in the Main domain. It shows the following:
- Setup of an ESM application callback to receive Single Error Correction (SEC) and Double Error Detection (DED) events and setup of ECC Aggregators in general
- Triggering of ECC events for a small number of RAM IDs, including Interconnect type and Wrapper type
- Printing out error information within the ECC callback upon reception of ECC events
The following use cases are implemented in this example:
Use Cases
Use Case | Description |
UC-0 | Single DED error on Main ESM for wrapper RAM ID type |
UC-1 | Single SEC error on Main ESM for wrapper RAM ID type |
UC-2 | Parity error injection on Main ESM for interconnect RAM ID type |
Supported Combinations
Parameter | Value |
CPU + OS | m4fss0-0 nortos |
r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am243x-evm |
Example folder | examples/sdl/ecc/ |
Steps to Run the Example
Sample Output
Shown below is a sample output when the application is run,
[BLAZAR_Cortex_M4F_1]
ECC Example Application
Unit tests started ...
ECC_Example_init: Init MAIN ESM complete
ECC_Example_init: Init WKUP ESM complete
SDTF_init: AGGR0 ECC Init complete
ESM Safety Example tests: starting
AGGR0 Double bit error inject Example test UC-1: starting
AGGR0 Double bit error inject test: Subtype 0x00000001 test complete
Waiting for ESM Interrupt
UC-1: Got Low priority ESM Interrupt
AGGR0 Double bit error inject Example test UC-2: starting
AGGR0 Double bit error inject test: Subtype 0x00000002 test complete
Waiting for ESM Interrupt
UC-2: Got High priority ESM Interrupt
**** AGGR0 Memory Parity TEST ****
AGGR0 Single bit error self test: Subtype 0x00000001 test complete
Waiting for ESM Interrupt
Memory Parity Error Test Complete
ECC Safety Example tests: success
ECC UC-1 and UC-2 Test
All Use_Cases have passed.
../../../ecc_main.c:259:ECC_Example_app:MCUSDK-0:PASS
-----------------------
1 Tests 0 Failures 0 Ignored
All tests have passed