AM243x MCU+ SDK  08.06.00
SA2UL HMAC SHA-1 Test

Introduction

This example demonstrates the how to generate HMAC SHA-1 hash using SA2UL module.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am243x-evm, am243x-lp
Example folder examples/security/crypto/sa2ul_hmac_sha/crypto_hmac_sha1/crypto_hmac_sha1.c

Steps to Run the Example

See Also

SA2UL

Sample Output

Shown below is a sample output when the application is run.

CCS Console:

[CRYPTO] HMAC SHA-1 example started ...
[CRYPTO] HMAC SHA-1 example completed!!
All tests have passed!!