![Logo](ti_logo.svg) |
AM243x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
32 #ifndef ICSS_EIP_DRIVER_H_
33 #define ICSS_EIP_DRIVER_H_
76 #define IEP_CMP_DEFAULT_VAL 0x11
77 #define IEP_CMP4_DEFAULT_VAL 0x5000
78 #define IEP_CMP0_DEFAULT_VAL 0xffffffff
81 #define PRU_IEP_CMP_CFG_REG 0x40
83 #define PRU_IEP_CMP0_REG 0x48
86 #define EIP_TICK_PERIOD 1
87 #define LOOPBK_PKT_SEND_PERIOD 1000
89 #define DEFAULT_BC_PKT_SIZE 60
91 #define ONE_SECOND_INTERVAL 1000
92 #define TWO_MINUTE_INTERVAL 120000
95 #define CRS_STATUS_MASK 0x2
97 #define CRS_STATUS_SHIFT 0x1
100 #define PTP_PROT_TYPE 0x88F7
101 #define DLR_MDIO_PHY0 1
102 #define DLR_MDIO_PHY1 2
105 #define PHYBMSR_OFFSET 0x1
106 #define PHYSTS_OFFSET 0x10
108 #define PHY_LINK_STATUS_MASK 0x4
109 #define PHY_LINK_STATUS_SHIFT 0x2
137 uint8_t clockIdentity[8];
181 uint8_t portProfileIdentity[8];
191 uint8_t physicalProtocol[16];
193 uint8_t portPhysicalAddress[16];
205 uint8_t portProtocolAddress[16];
269 uint8_t manufacturerIdentity[4];
296 typedef struct eip_Config_s
clockType
Type of clock supported by PTP Implementation. This is not specified by standard.
Definition: icss_eip_driver.h:117
uint16_t currentUTCOffset
Definition: icss_eip_driver.h:149
uint16_t networkProtocol
Definition: icss_eip_driver.h:203
TimeSync_ParamsHandle_t timeSyncHandle
Definition: icss_eip_driver.h:300
struct ICSS_EMAC_Config_s * ICSS_EMAC_Handle
Alias for ICSS EMAC Handle containing base addresses and modules.
Definition: icss_emac.h:449
uint16_t portNumber
Definition: icss_eip_driver.h:202
port_State
Port States, from IEEE 1588v2.
Definition: icss_timeSyncApi.h:142
clockClass_t parentClkInfo
Definition: icss_eip_driver.h:241
sysTimeOffset_t timeOffset
Definition: icss_eip_driver.h:288
void EIP_drvInit(EIP_Handle icssEipHandle)
Initialization routine for Ethernet/IP driver functions.
struct dlr_Config_s * EIP_DLRHandle
Definition: icss_dlr.h:208
PRUICSS_Handle pruicssHandle
Definition: icss_eip_driver.h:298
struct eip_Config_s * EIP_Handle
Definition: icss_eip_driver.h:111
CIP Sync configuration. Instance Attribute for PTP Class (Class Code 0x43. CIP Spec Vol 1)
Definition: icss_eip_driver.h:223
uint16_t numberOfPorts
Definition: icss_eip_driver.h:245
uint64_t systemOffset
Definition: icss_eip_driver.h:215
uint8_t domainNumber
Definition: icss_eip_driver.h:265
Specifies the physical protocol and physical address (e.g. IEEE 802.3) of each port of the device (e....
Definition: icss_eip_driver.h:190
int8_t EIP_initializeCIPSync(EIP_Handle icssEipHandle)
API to initialize the CIP Sync objects in the EIP handle Initialize CIP Sync member variables based o...
uint32_t size
Definition: icss_eip_driver.h:171
Definition: icss_eip_driver.h:297
uint16_t observedOffsetScaledLogVariance
Definition: icss_eip_driver.h:157
void EIP_drvStart(EIP_Handle icssEipHandle)
EIP driver start API.
uint16_t sizeOfAddress
Definition: icss_eip_driver.h:192
int64_t meanPathDelayToMaster
Definition: icss_eip_driver.h:237
void EIP_drvStop(EIP_Handle icssEipHandle)
EIP driver stop API.
uint16_t timeAccuracy
Definition: icss_eip_driver.h:141
uint16_t offsetScaledLogVariance
Definition: icss_eip_driver.h:144
descr_t revData
Definition: icss_eip_driver.h:273
clockClass_t localClkInfo
Definition: icss_eip_driver.h:243
uint16_t timeSource
Definition: icss_eip_driver.h:153
#define ICSS_EMAC_MAXMTU
Maximum Valid size (incl header + VLAN TAG..., no CRC)
Definition: icss_emac.h:257
uint16_t timePropertyFlags
Definition: icss_eip_driver.h:151
@ BOUNDARY_CLOCK
Definition: icss_eip_driver.h:123
uint8_t IsSynchronized
Definition: icss_eip_driver.h:227
void EIP_processProtocolFrames(uint32_t *queue_number, void *userArg)
API to process the real time Packets.
uint64_t systemTimeMicrosec
Definition: icss_eip_driver.h:229
clockClass_t grandMasterClkInfo
Definition: icss_eip_driver.h:239
@ TRANSPARENT_CLOCK
Definition: icss_eip_driver.h:121
ICSS_EMAC_Handle emacHandle
Definition: icss_eip_driver.h:299
uint64_t systemTimeNanosec
Definition: icss_eip_driver.h:231
uint64_t maxOffsetFromMaster
Definition: icss_eip_driver.h:235
uint8_t priority2
Definition: icss_eip_driver.h:262
Specifies the properties of a clock.
Definition: icss_eip_driver.h:135
EIP_DLRHandle dlrHandle
Definition: icss_eip_driver.h:304
uint8_t ifPTPEnable
Definition: icss_eip_driver.h:225
Specifies the system time in microseconds and the Offset to the local clock value.
Definition: icss_eip_driver.h:213
clockType clockType
Definition: icss_eip_driver.h:267
uint64_t systemTime
Definition: icss_eip_driver.h:214
uint16_t clockClass
Definition: icss_eip_driver.h:139
cipSyncConfig_t cipSyncObj
Definition: icss_eip_driver.h:301
Description in unicode.
Definition: icss_eip_driver.h:169
uint16_t observedPhaseChangeRate
Definition: icss_eip_driver.h:161
descr_t userDesc
Definition: icss_eip_driver.h:275
uint16_t addressSize
Definition: icss_eip_driver.h:204
uint8_t priority1
Definition: icss_eip_driver.h:260
@ ORDINARY_CLOCK
Definition: icss_eip_driver.h:119
descr_t productType
Definition: icss_eip_driver.h:271
Specifies the specifies the network and protocol address of each port of the device (e....
Definition: icss_eip_driver.h:201
struct TimeSync_ParamsHandle_s * TimeSync_ParamsHandle_t
Definition: icss_timeSyncApi.h:962
Specifies the PTP profile of each port of the device.
Definition: icss_eip_driver.h:180
uint16_t stepsRemoved
Definition: icss_eip_driver.h:286
struct PRUICSS_Config_s * PRUICSS_Handle
A handle that is returned from a PRUICSS_open() call. This handle is required for calling other APIs.
Definition: pruicss/g_v0/pruicss.h:235
int64_t offsetFromMaster
Definition: icss_eip_driver.h:233
#define ICSS_EMAC_MAX_PORTS_PER_INSTANCE
Maximum number of Ports in a single ICSS
Definition: icss_emac.h:66