![Logo](ti_logo.svg) |
AM243x MCU+ SDK
08.06.00
|
|
uint32_t nodeTableArbitration
Definition: hsrPrp_red_config.h:62
uint32_t duplicatePortTableSize
Definition: hsrPrp_red_config.h:64
uint32_t duplicatePort1Counter
Definition: hsrPrp_red_config.h:72
uint32_t clearNodeTable
Definition: hsrPrp_red_config.h:75
RED_STATUS RedGetConfiguration(RED_CONFIG *pCfg, PRUICSS_Handle pruicssHandle)
Reads the configuration from DMEM.
uint32_t nodeForgetTime
Definition: hsrPrp_red_config.h:65
uint32_t hostDuplicateArbitration
Definition: hsrPrp_red_config.h:78
uint32_t duplicatePortCheckInterval
Definition: hsrPrp_red_config.h:68
uint32_t duplicateForgetTime
Definition: hsrPrp_red_config.h:66
uint32_t duplicateHostTableSize
Definition: hsrPrp_red_config.h:63
uint32_t nodeTableCheckInterval
Definition: hsrPrp_red_config.h:70
uint32_t supAddressHi
Definition: hsrPrp_red_config.h:76
RED_STATUS
RED Status.
Definition: hsrPrp_red_common.h:526
uint32_t supAddressLow
Definition: hsrPrp_red_config.h:77
uint32_t duplicateHostCheckInterval
Definition: hsrPrp_red_config.h:69
void RedInit(PRUICSS_Handle pruicssHandle)
Initialises DMEM with default configuration values.
uint32_t duplicateHostCounter
Definition: hsrPrp_red_config.h:73
uint32_t brokenPathDifference
Definition: hsrPrp_red_config.h:67
Include file for hsrPrp_red_hsr.c.
uint8_t RedLoadFirmware(PRUICSS_Handle pruicssHandle)
Loads firmware.
Definition: hsrPrp_red_config.h:59
uint32_t nodeTableSize
Definition: hsrPrp_red_config.h:61
struct PRUICSS_Config_s * PRUICSS_Handle
A handle that is returned from a PRUICSS_open() call. This handle is required for calling other APIs.
Definition: pruicss/g_v0/pruicss.h:235
uint32_t duplicatePort0Counter
Definition: hsrPrp_red_config.h:71
uint32_t nodeTableCounter
Definition: hsrPrp_red_config.h:74