Software installation
- Install Code Composer Studio for Sitara(TM) processors (CCS).
- Install ArmĀ® code generation tools - compiler (ARM-CGT)
- Install a System Configuration Tool (sysconfig).
- Install a Software Development Kit (SDK) AM243X with demos and device description ESI files
for details see Getting started
Connect the development board
TMDS243GPEVM/TMDS64GPEVM
Board details: TMDS64GPEVM, TMDS243GPEVM
Setup a dip switches on the board : 25MHz, No-boot / Dev-boot.
No boot mode
Connect the evaluation board to your computer using the micro-USB cables.
One USB cables is required for the JTAG interface (XDS110), a second cable for the UART console.
USB connectors on the AM64x/AM243 GP EVM Board
Connect an ethernet cable from a PC running the TwinCAT to EtherCAT IN/Port0 of the PRU-ICSS on the development board.
EtherCAT ports
- If you have multiple devices in chain, please connect from EtherCAT OUT/Port1 to IN/Port0 of next device. For the last device in chain, OUT/Port1 will be left open (if NOT using redundancy mode).
- Connect the board(s) to the power supply(ies) according to the specifications in the AM64x/AM243x GP EVM User's Guide Rev D
LP-AM243
Board details: LP-AM243
Setup a dip switches on the board : No-boot / Dev-boot
No boot mode
Connect the evaluation board to your computer using two micro-USB cables:
- J28 JTAG interface (XDS110)
- J26 UART console
USB connector on the AM243x LP Board
Connect an ethernet cable from a PC running the TwinCAT to EtherCAT IN/Port0 of the PRU-ICSS on the development board.
EtherCAT connectors on the AM243x LP Board
- If you have multiple devices in chain, please connect from EtherCAT OUT/Port1 to IN/Port0 of next device. For the last device in chain, OUT/Port1 will be left open (if NOT using redundancy mode).
Connect a USB Type-C Power Supply to the board
Board power connector on the AM243x LP
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu, see Using SDK with CCS Projects.
- When using makefiles to build, note the required combination and build using make command, see Using SDK with Makefiles.
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run.