Abort error code index values. Use for mailbox callback return values.
Macros | |
#define | ABORTIDX_TOGGLE_BIT_NOT_CHANGED 0x01 |
Index of "Toggle bit not changed". More... | |
#define | ABORTIDX_SDO_PROTOCOL_TIMEOUT 0x02 |
Index of "SDO timeout". More... | |
#define | ABORTIDX_COMMAND_SPECIFIER_UNKNOWN 0x03 |
Index of "Command specifier unknown". More... | |
#define | ABORTIDX_OUT_OF_MEMORY 0x04 |
Index of "Out of memory". More... | |
#define | ABORTIDX_UNSUPPORTED_ACCESS 0x05 |
Index of "Unsupported Access". More... | |
#define | ABORTIDX_WRITE_ONLY_ENTRY 0x06 |
Index of "Write only entry". More... | |
#define | ABORTIDX_READ_ONLY_ENTRY 0x07 |
Index of "Read only entry". More... | |
#define | ABORTIDX_OBJECT_NOT_EXISTING 0x08 |
Index of "Object not existing". More... | |
#define | ABORTIDX_OBJECT_CANT_BE_PDOMAPPED 0x09 |
Index of "Object can not be mapped to PDO". More... | |
#define | ABORTIDX_MAPPED_OBJECTS_EXCEED_PDO 0x0A |
Index of "Mapped Object exceeds PDO". More... | |
#define | ABORTIDX_PARAM_IS_INCOMPATIBLE 0x0B |
Index of "Parameter is incompatible". More... | |
#define | ABORTIDX_INTERNAL_DEVICE_INCOMPATIBILITY 0x0C |
Index of "Device incompatibility". More... | |
#define | ABORTIDX_HARDWARE_ERROR 0x0D |
Index of "Hardware error". More... | |
#define | ABORTIDX_PARAM_LENGTH_ERROR 0x0E |
Index of "Parameter length error". More... | |
#define | ABORTIDX_PARAM_LENGTH_TOO_LONG 0x0F |
Index of "Parameter is too long". More... | |
#define | ABORTIDX_PARAM_LENGTH_TOO_SHORT 0x10 |
Index of "Parameter is too short". More... | |
#define | ABORTIDX_SUBINDEX_NOT_EXISTING 0x11 |
Index of "Subindex (Entry) not exists". More... | |
#define | ABORTIDX_VALUE_EXCEEDED 0x12 |
Index of "Value exceeds". More... | |
#define | ABORTIDX_VALUE_TOO_GREAT 0x13 |
Index of "Value is too great". More... | |
#define | ABORTIDX_VALUE_TOO_SMALL 0x14 |
Index of "Value is too small". More... | |
#define | ABORTIDX_MODULE_ID_LIST_NOT_MATCH 0x15 |
Index of "Unequal Module Id list". More... | |
#define | ABORTIDX_MAX_VALUE_IS_LESS_THAN_MIN_VALUE 0x16 |
Index of "Value is less than minimum value". More... | |
#define | ABORTIDX_GENERAL_ERROR 0x17 |
Index of "General error". More... | |
#define | ABORTIDX_DATA_CANNOT_BE_READ_OR_STORED 0x18 |
Index of "Data can not be read or written". More... | |
#define | ABORTIDX_DATA_CANNOT_BE_ACCESSED_BECAUSE_OF_LOCAL_CONTROL 0x19 |
Index of "Data can not be accessed because of local control". More... | |
#define | ABORTIDX_IN_THIS_STATE_DATA_CANNOT_BE_READ_OR_STORED 0x1A |
Index of "Data can not be read or written in the current state". More... | |
#define | ABORTIDX_NO_OBJECT_DICTIONARY_IS_PRESENT 0x1B |
Index of "Object is not in the object dictionary". More... | |
#define | ABORTIDX_ENTRY_CANT_BE_WRITTEN_SI0_NOT_0 0x1C |
Index of "Entry can not be written because Subindex0 is not 0". More... | |
#define | ABORTIDX_COMPLETE_ACCESS_NOT_SUPPORTED 0x1D |
The object can not be accessed via complete access. More... | |
#define | ABORTIDX_WORKING 0xFF |
Index of application is handling the SDO request. More... | |