|
void | EC_API_SLV_cbRegisterPhyReset (CUST_PHY_CBreset_t cbFunc_p, void *pContext_p) |
| This is the function to register Phy Reset Function. More...
|
|
bool | EC_API_SLV_registerPhy (uint8_t phyIdx_p, uint8_t phyAddr_p, bool invertLinkPolarity_p, bool useRxLinkPin_p) |
| Register a phy for stack usage. More...
|
|
void | EC_API_SLV_cbRegisterPhyLibDetect (CUST_PHY_CBextPhyLibDetect_t cbFunc_p, void *pContext_p) |
| Register an application specific Phy Library. More...
|
|
uint32_t | EC_API_SLV_phyRegRead (void *pStackContext_p, uint32_t regNum_p, uint16_t *pData_p) |
| Read from PHY using Stack. More...
|
|
void | EC_API_SLV_phyRegWrite (void *pStackContext_p, uint32_t regNum_p, uint16_t wrVal_p) |
|
void | EC_API_SLV_cbRegisterBoardStatusLed (EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_CBBoardStatusLed_t cbFunc_p, void *pLedContext_p) |
| Register Board Status LED callback. More...
|
|