#define TIESC_HW 0
#define PRU_200MHZ 1
#include "project.h"
#include <ecSlvESI.h>
#if (defined DPRAM_REMOTE) && (DPRAM_REMOTE==1)
#include <DPR_Api.h>
#if (defined DPRIMPL_SHAREDRAM) && (DPRIMPL_SHAREDRAM==1)
#include <dprLib_sharedMemory.h>
#endif
#elif (defined FBTL_REMOTE) && (FBTL_REMOTE==1)
#include <sysLib_sharedMemory.h>
#endif
#include <osal.h>
#include <ESL_os.h>
#include <ESL_BOARD_config.h>
#include <ESL_version.h>
#include <ecSlvApi.h>
static OSAL_PJumpBuf_t farJumpBuf_g;
static uint32_t EC_SLV_APP_remoteInit(void** pRemHandle_p);
{
if (!pApplicationInstance)
{
goto Exit;
}
{
OSAL_printf("%s:%d Error code: 0x%08x\n", __func__, __LINE__, error);
OSAL_error(__func__, __LINE__, OSAL_STACK_INIT_ERROR, true, 0);
}
ESL_dumpVersions();
for(;;)
{
{
OSAL_SCHED_yield();
}
else
{
OSAL_SCHED_sleep(10);
}
}
Exit:
ESL_OS_taskLeave();
return;
}
{
uint32_t retVal = OSAL_eERR_NOERROR;
if (!applicationInstance)
{
OSAL_error(__func__, __LINE__, OSAL_eERR_EINVAL, true, 1, "Application instance missing!!!\r\n");
}
if (OSAL_eERR_NOERROR != retVal)
{
OSAL_error(__func__, __LINE__, retVal, true, 1, "OS Board init error\r\n");
}
retVal = EC_SLV_APP_remoteInit(&applicationInstance->
remoteHandle);
if (!(OSAL_CONTAINER_LOCALIMPLEMENTATION == retVal || OSAL_eERR_NOERROR == retVal))
{
OSAL_error(__func__, __LINE__, OSAL_eERR_EINVAL, true, 1, "Fatal error remote API init!!!\r\n");
return;
}
if (0 == retVal)
{
EC_API_SLV_prepareTasks(KBECSLV_PRIO_PDI, KBECSLV_PRIO_LED, KBECSLV_PRIO_SYNC0, KBECSLV_PRIO_SYNC1, KBECSLV_PRIO_EOE);
,applicationInstance
#if !(defined FBTL_REMOTE) || (0==FBTL_REMOTE)
,OSAL_TASK_ePRIO_Normal
#else
,OSAL_TASK_ePRIO_Idle
#endif
,(uint8_t*)EC_SLV_APP_applLoopTaskStack_g
,APPLLOOP_TASK_SIZE_BYTE
,0
,"Appl_LoopTask");
{
OSAL_printf("Error return start Loop Task\r\n");
OSAL_error(__func__, __LINE__, OSAL_STACK_INIT_ERROR, true, 0);
}
for (;;)
{
OSAL_SCHED_sleep(1000);
}
}
else
{
for (;;)
{
for (;;)
{
OSAL_printf("long jmp restart\n");
OSAL_SCHED_sleep(1000);
}
}
}
}
int main(int argc, char *argv[])
{
static
uint32_t selectedPruInstance = ~0;
static
uint32_t error = OSAL_eERR_NOERROR;
ESL_OS_init();
selectedPruInstance = ESL_DEFAULT_PRUICSS;
if (1 < argc)
{
char* inst = argv[1];
selectedPruInstance = strtoul(inst, NULL, 0);
}
#if (defined OSAL_TIRTOS)
if (0x1000 == argc)
{
PRUICSS_pruDisable(NULL, 0);
PRUICSS_pruDisable(NULL, 1);
PRUICSS_registerIrqHandler(NULL, 0, 0, 0, 0, NULL);
}
#endif
OSAL_init();
#if (defined OSAL_FREERTOS) || (defined OSAL_FREERTOS_JACINTO)
TaskP_Params_init(&applicationInstance.mainThreadParam);
applicationInstance.mainThreadParam.name = "mainThread";
applicationInstance.mainThreadParam.stackSize = MAIN_TASK_SIZE_BYTE;
applicationInstance.mainThreadParam.stack = (uint8_t*)EC_SLV_APP_mainTaskStack_g;
applicationInstance.mainThreadParam.priority = (TaskP_PRIORITY_HIGHEST-1);
applicationInstance.mainThreadParam.args = (void*)&applicationInstance;
,&applicationInstance.mainThreadParam);
if (SystemP_SUCCESS != error)
{
OSAL_printf("Error setting create thread of %s (%ld)\r\n", applicationInstance.mainThreadParam.name, error);
OSAL_error(__func__, __LINE__, OSAL_STACK_INIT_ERROR, true, 0);
}
#else
OSAL_TASK_ePRIO_Idle,
(uint8_t*)EC_SLV_APP_mainTaskStack_g,
MAIN_TASK_SIZE_BYTE, 0, "MainTask");
{
OSAL_printf("Error return start Main Task\r\n");
OSAL_error(__func__, __LINE__, OSAL_STACK_INIT_ERROR, true, 0);
error = OSAL_STACK_INIT_ERROR;
}
#endif
OSAL_startOs();
OSAL_error(__func__, __LINE__, OSAL_eERR_EINVAL, true, 1, "Not reachable by design!!!\r\n");
return error;
}
static uint32_t EC_SLV_APP_remoteInit(void** pRemHandle_p)
{
uint32_t retVal = OSAL_CONTAINER_LOCALIMPLEMENTATION;
if (!pRemHandle_p)
{
goto Exit;
}
#if (defined DPRAM_REMOTE) && (DPRAM_REMOTE==1)
OSALUNREF_PARM(pRemHandle_p);
retVal = DPRLIB_init(false);
#elif (defined FBTL_REMOTE) && (FBTL_REMOTE==1)
retVal = SYSLIB_createLibInstance(FBTLSHARED_MEM_NAME, FBTLSHARED_MEM_SIZE, false,
FBTL_MAX_ASYNC_LEN, FBTL_MAX_ASYNC_LEN, FBTL_MAX_PD_LEN, FBTL_MAX_PD_LEN
#if (defined FBTLTRACECALLS) && (FBTLTRACECALLS==1)
,true
#else
,false
#endif
,pRemHandle_p
);
#else
OSALUNREF_PARM(pRemHandle_p);
retVal = OSAL_CONTAINER_LOCALIMPLEMENTATION;
#endif
if (OSAL_CONTAINER_LOCALIMPLEMENTATION == retVal)
{
OSAL_printf("\r\nLocal Implementation\r\n");
}
#if (defined DPRAM_REMOTE) && (DPRAM_REMOTE==1)
else if (0 == retVal)
{
OSAL_printf("\r\nDPRAM usage\r\n");
retVal = EC_API_SLV_DPR_configuration(dprRamBase(), dprRamSize());
if (0 != retVal)
{
OSAL_printf("%s:%d Error code: 0x%08x\n", __func__, __LINE__, retVal);
OSAL_error(__func__, __LINE__, OSAL_STACK_INIT_ERROR, true, 0);
return retVal;
}
}
#elif (defined FBTL_REMOTE) && (FBTL_REMOTE==1)
else if (0 == retVal)
{
retVal = EC_API_SLV_FBTL_configuration(*pRemHandle_p);
if (0 != retVal)
{
OSAL_printf("%s:%d Error code: 0x%08x\n", __func__, __LINE__, retVal);
OSAL_error(__func__, __LINE__, OSAL_STACK_INIT_ERROR, true, 0);
return retVal;
}
}
#endif
Exit:
return retVal;
}