AM243x MCU+ SDK  08.05.00
HDSL Diagnostic with Traces

Introduction

The HDSL diagnostic application described here interacts with the firmware interface.

HDSL diagnostic application does below,

Configures pinmux, GPIO, ICSS clock to 225MHz, Initializes ICSS0-PRU1, ICSS0-IEP0 and IEP1(for SYNC mode support.Timesync router is used to latch the loopback.), Loads lookup table for encoding/decoding of Hiperface data Loads the initialization section of PRU firmware & executes it. Firmware is split to three sections, initialization, datalink and transport. At startup, the application displays details about encoder and status. It then presents the user with menu options, based on the option selected, application communicates with HDSL interface and the result is presented to the user.

Important files and directory structure

Folder/Files Description
${SDK_INSTALL_PATH}/examples/motor_control/hdsl_diagnostic_with_traces
hdsl_diagnostic_ddr.c hdsl_diagnostic_ddr.h
${SDK_INSTALL_PATH}/source/motor_control/position_sense/hdsl
driver/ Folder containing HDSL PRU driver sources.
include/ Folder containing HDSL PRU header sources.
firmware/

Folder containing HDSL PRU firmware sources.

Parameter Value
CPU + OS r5fss0-0 freertos
ICSSG ICSSG0
PRU PRU1
Toolchain ti-arm-clang
Board am243x-evm
Example folder examples/motorcontrol/hdsl_example

Steps to Run the Example

Hardware Prerequisites

Other than the basic EVM setup mentioned in EVM Setup, below additional HW is required to run this demo

  • HDSL encoder
  • Below are two options to connect encoder to AM64x/AM243x EVM.
    • Option 1
      • TIDA-00179 Universal Digital Interface to Absolute Position Encoders, https://www.ti.com/tool/TIDA-00179
      • TIDEP-01015 3 Axis board
      • Interface card connecting EVM and TIDEP-01015 3 Axis board
      • Connect the Hiperface DSL encoder to HDSL+/-(Pin number 6 and 7) signals available on header J7 or Sub-D15 connector of the "Universal Digital Interface to Absolute Position Encoders" board.
    • Option 2
      • HDSL AM64xE1 Transceiver. If application is using this card, define the macro HDSL_AM64xE1_TRANSCEIVER in the CCS project/make file.
      • Connect the Hiperface DSL encoder to J10.
      • HDSL AM64xE1 Transceiver supports two channels that can be used to support HDSL safety, multi axis servo drives.
      • Schematics are shared in the MCU+SDK package. For more design details of the transceiver card, please contact TI via E2E/FAE.
      • HDSL Transceiver Card Schematics document.

Hardware Setup(Using TIDA-00179, TIDEP-01015 and Interface board)

Hardware Setup

Hardware Setup(Using HDSL AM64xE1 Transceiver)

Hardware Setup

Build, load and run

  • When using CCS projects to build, import the CCS project and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • Refer to UART terminal for user interface menu options.

HDSL DDR Traces Flow Chart

Note:

  • If you are using load_dmsc.js file for initialization, Then Go to menu Scripts --> AM64 DDR Initialization -> AM64_DDR_Initialization_ECC_Disabled to initialize DDR.
  • If you are using SBL NULL. DDR initialization will be taken care itself.

Sample Output

Shown below is a sample output when the application is run:

  • Freerun mode:
    HDSL DDR UART Menu