AM243x MCU+ SDK  08.05.00
Driver Porting Layer (DPL) demo

Introduction

This example shows a simple application, which setups the CPU and the underlying RTOS or no-RTOS environment on the supported SOC.

The example does the below

  • Setup a timer with system tick of 1ms, setup MPU and cache (if available)
  • Create a RTOS task (in RTOS example)
  • Trigger a ISR and signal a semaphore from ISR to main task
  • Show usage of clock delay
  • Show usage of cache APIs
  • Show usage of heap APIs

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss0-0 freertos
m4fss0-0 nortos
m4fss0-0 freertos
Toolchain ti-arm-clang
Boards am243x-evm, am243x-lp
Example folder examples/kernel/dpl/dpl_demo/

Steps to Run the Example

See Also

Driver Porting Layer (DPL)

Sample Output

Shown below is a sample output when the application is run,

[DPL] Hwi post ...
[DPL] Hwi post ... DONE !!!
[DPL] Sleep for 100 msecs ...
[DPL] Sleep ... DONE (Measured time = 100000 usecs, CPU cycles = 80000055 ) !!!
[DPL] Running cache operations ...
[DPL] Running cache operations ... DONE !!!
[DPL] Heap free size = 1984 bytes
[DPL] Allocated 1023 bytes @ 0x80010440, heap free size = 896 bytes
[DPL] Free'ed 1023 bytes @ 0x80010440, heap free size = 1984 bytes
All tests have passed!