AM243x MCU+ SDK  08.05.00
SA2UL AES CBC-128 Test

Introduction

This example demonstrates the AES CBC-128 Encryption and Decryptions using SA2UL module.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am243x-evm
Example folder examples/security/crypto/sa2ul_aes/crypto_aes_cbc_128/crypto_aes_cbc_128.c

Steps to Run the Example

See Also

SA2UL

Sample Output

Shown below is a sample output when the application is run.

CCS Console:

[CRYPTO] AES CBC-128 example started ...
[CRYPTO] AES CBC-128 example completed!!
All tests have passed!!