EtherNet/IP™ Adapter  1.04.10
User Reference Manual
Attribute Functions (Setter)

Overview

A description of an externally visible characteristic or feature of an object. Attributes may provide status information or govern the operation of an object. For example: the ASCII name of an object, the repetition rate of a cyclic object.

Functions

uint32_t EI_API_CIP_setAttr_bool (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_bool attrValue_p)
 Set attribute of type BOOL. More...
 
uint32_t EI_API_CIP_setAttr_sint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_sint attrValue_p)
 Set attribute of type SINT. More...
 
uint32_t EI_API_CIP_setAttr_int (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_int attrValue_p)
 Set attribute of type INT. More...
 
uint32_t EI_API_CIP_setAttr_dint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_dint attrValue_p)
 Set attribute of type DINT. More...
 
uint32_t EI_API_CIP_setAttr_lint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_lint attrValue_p)
 Set attribute of type LINT. More...
 
uint32_t EI_API_CIP_setAttr_usint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_usint attrValue_p)
 Set attribute of type USINT. More...
 
uint32_t EI_API_CIP_setAttr_uint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_uint attrValue_p)
 Set attribute of type UINT. More...
 
uint32_t EI_API_CIP_setAttr_udint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_udint attrValue_p)
 Set attribute of type UDINT. More...
 
uint32_t EI_API_CIP_setAttr_ulint (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_ulint attrValue_p)
 Set attribute of type ULINT. More...
 
uint32_t EI_API_CIP_setAttr_real (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_real attrValue_p)
 Set attribute of type REAL. More...
 
uint32_t EI_API_CIP_setAttr_lreal (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_lreal attrValue_p)
 Set attribute of type LREAL. More...
 
uint32_t EI_API_CIP_setAttr_shortstring (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_shortstring *pAttrValue_p)
 Set attribute of type SHORT_STRING. More...
 
uint32_t EI_API_CIP_setAttr_byte (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_byte attrValue_p)
 Set attribute of type BYTE. More...
 
uint32_t EI_API_CIP_setAttr_word (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_word attrValue_p)
 Set attribute of type WORD. More...
 
uint32_t EI_API_CIP_setAttr_dword (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_dword attrValue_p)
 Set attribute of type DWORD. More...
 
uint32_t EI_API_CIP_setAttr_lword (T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p, ei_api_cip_edt_lword attrValue_p)
 Set attribute of type LWORD. More...