Macros | |
#define | ACCESS_READWRITE 0x003F |
Read/write in all states. More... | |
#define | ACCESS_READ 0x0007 |
Read only in all states. More... | |
#define | ACCESS_READ_PREOP 0x0001 |
Read only in PreOP. More... | |
#define | ACCESS_READ_SAFEOP 0x0002 |
Read only in SafeOP. More... | |
#define | ACCESS_READ_OP 0x0004 |
Read only in OP. More... | |
#define | ACCESS_WRITE 0x0038 |
Write only in all states. More... | |
#define | ACCESS_WRITE_PREOP 0x0008 |
Write only in PreOP. More... | |
#define | ACCESS_WRITE_SAFEOP 0x0010 |
Write only in SafeOP. More... | |
#define | ACCESS_WRITE_OP 0x0020 |
Write only in OP. More... | |
#define | OBJACCESS_NOPDOMAPPING 0x0000 |
Not PDO mappable. More... | |
#define | OBJACCESS_RXPDOMAPPING 0x0040 |
Mappable in RxPDOs. More... | |
#define | OBJACCESS_TXPDOMAPPING 0x0080 |
Mappable in TxPDOs. More... | |
#define | OBJACCESS_BACKUP 0x0100 |
Backup entry. More... | |
#define | OBJACCESS_SETTINGS 0x0200 |
Setting Entry. More... | |
#define | OBJACCESS_SAFEINPUTS 0x0400 |
Safe input. More... | |
#define | OBJACCESS_SAFEOUTPUTS 0x0800 |
Safe output. More... | |
#define | OBJACCESS_SAFEPARAMETER 0x1000 |
Safe parameter. More... | |