bool EC_SLV_APP_EoE_settingIndHandler | ( | void * | pContext_p, |
uint16_t * | pMac_p, | ||
uint16_t * | pIp_p, | ||
uint16_t * | pSubNet_p, | ||
uint16_t * | pDefaultGateway_p, | ||
uint16_t * | pDnsIp_p | ||
) |
EoE Settings Indication callback.
[in] | pContext_p | The pointer to the application instance. |
[in] | pMac_p | Virtual Net MAC address |
[in] | pIp_p | Virtual Net IP address |
[in] | pSubNet_p | Virtual Net Subnet |
[in] | pDefaultGateway_p | Virtual Net Default Gateway |
[in] | pDnsIp_p | Virtual Net DNS server address |