EtherCAT Slave  1.10.00
EEPROM Configuration

The EtherCAT slave information is generated on the fly and by default is not stored anywhere, it’s simply emulated. However, the SDK provides a set of functions to store the EtherCAT slave information content in a physical storage. Therefore, after a hardware reset the SDK will use the content from the non-volatile memory instead of the content generated on the fly.

Function Description
EC_API_SLV_cbRegisterFlashInit Register non-volatile memory initialization function
EC_API_SLV_EEPROM_cbRegisterLoad Register non-volatile memory read function
EC_API_SLV_EEPROM_cbRegisterWrite Register non-volatile memory write function